Data Fields

RcmClient_Struct Struct Reference
[RcmClient]

Opaque client structure large enough to hold an instance object. More...

#include <RcmClient.h>

Data Fields

xdc_runtime_knl_GateThread_Struct _f1
Ptr _f2
Ptr _f3
UInt16 _f4
Ptr _f5
UInt32 _f6
Bool _f7
UInt16 _f8
Ptr _f9
Ptr _f10
Ptr _f11
Ptr _f12

Detailed Description

Opaque client structure large enough to hold an instance object.

Use this structure to define an embedded RcmClient object.

See also:
RcmClient_construct

Field Documentation

xdc_runtime_knl_GateThread_Struct RcmClient_Struct::_f1

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated