Data Fields

IRES_HDVICP_Obj Struct Reference
[IRES HDVICP Protocol]

IRES_HDVICP_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. More...

#include <ires_hdvicp.h>

Collaboration diagram for IRES_HDVICP_Obj:
Collaboration graph
[legend]

Data Fields

IRES_Obj ires
Void * info
Int id
Void * registerBaseAddress
Void * memoryBaseAddress
unsigned int pscRegisterSpace

Detailed Description

IRES_HDVICP_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource.


Field Documentation

RSVD for future use

ID of the HDVICP being , granted, could be IRES_HDVICP_ID_0 or IRES_HDVICP_ID_1

Base address of reg space

Mem address of mem space

Base address of the PSC and system module register space


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated