Data Fields

IRES_EDMA3CHAN_Properties Struct Reference
[IRES EDMA3 Protocol]

Static Resource Properties. More...

#include <ires_edma3Chan.h>

Collaboration diagram for IRES_EDMA3CHAN_Properties:
Collaboration graph
[legend]

Data Fields

unsigned int numDmaChannels
unsigned int numQdmaChannels
unsigned int numTccs
unsigned int numPaRAMSets
unsigned int numEvtQueue
unsigned int numTcs
unsigned int numRegions
unsigned short dmaChPaRAMMapExists
 Channel mapping existence.
unsigned short memProtectionExists
IRES_EDMA3CHAN_EDMA3RegisterLayerglobalRegs

Detailed Description

Static Resource Properties.


Field Documentation

Total number of DMA Channel supported by the EDMA3

Total number of QDMA Channels supported by the EDMA3 Controller.

Total number of Tccs supported by the EDMA3.

Total number of PaRAM Sets supported by the EDMA3.

Total number of Event Queues in the EDMA3.

Total number of Transfer Controllers (TCs) in the EDMA3 Controller.

Number of Regions on the EDMA3 controller.

Channel mapping existence.

A value of 0 (No channel mapping) implies that there is fixed association for a channel number to a parameter entry number or, in other words, PaRAM entry n corresponds to channel n.

Existence of memory protection feature.

Pointer to Global Register region of CC Registers.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated