Functions | Defines | Data Structures | Typedefs

SCPY - Functional library for SDMA resources

Functions

void SCPY_init ()
 SCPY initialization API.
void SCPY_exit ()
 SCPY finalization API.
void SCPY_configure (IRES_SDMA_Handle logicalChannel, SCPY_Params *params)
 Configures transfer on a particular logical handle.
void SCPY_start (IRES_SDMA_Handle logicalChannel)
 Starts a transfer previously configured on a channel.
void SCPY_wait (IRES_SDMA_Handle logicalChannel)
 Wait for the transfer to complete.
Bool SCPY_complete (IRES_SDMA_Handle logicalChannel)
 Returns status of transfer on the logical channel.

Defines

#define OMAP_DMA_DATA_TYPE_S8   0x00
#define OMAP_DMA_DATA_TYPE_S16   0x01
#define OMAP_DMA_DATA_TYPE_S32   0x02
#define OMAP_DMA_PORT_EMIFF   0x00
#define OMAP_DMA_AMODE_POST_CONST   0x00
#define OMAP_DMA_AMODE_POST_INC   0x01
#define OMAP_DMA_AMODE_POST_SINGLE_INDEX   0x02
#define OMAP_DMA_AMODE_POST_DOUBLE_INDEX   0x03
#define OMAP_DMA_SYNC_MODE_ELEMENT   0x00
 To identify mode of sychronization of transfer.
#define OMAP_DMA_SYNC_MODE_FRAME   0x01
#define OMAP_DMA_SYNC_MODE_BLOCK   0x02
#define OMAP_DMA_SYNC_TYPE_DEST   0x00
#define OMAP_DMA_SYNC_TYPE_SRC   0x01

Data Structures

struct  SCPY_AddrParams
 Parameters of Address (source or destination) of transfer. More...
struct  SCPY_TransferParams
 Details of Transfer. More...
struct  SCPY_Params

Typedefs

typedef struct SCPY_AddrParams SCPY_AddrParams
 Parameters of Address (source or destination) of transfer.
typedef struct SCPY_TransferParams SCPY_TransferParams
 Details of Transfer.
typedef struct SCPY_Params SCPY_Params

Detailed Description

The SCPY module provides a list of SDMA operations an algorithm can perform on logical SDMA channels it acquires through the IRES_SDMA protocol. Examples of SCPY operations include channel configuration, SDMA transfer scheduling, and SDMA transfer synchronization.


Function Documentation

void SCPY_init (  )

SCPY initialization API.

void SCPY_exit (  )

SCPY finalization API.

void SCPY_configure ( IRES_SDMA_Handle  logicalChannel,
SCPY_Params params 
)

Configures transfer on a particular logical handle.

Parameters:
[in]logicalChannelHandle to the logical channel on which transfer will be configured
[in]paramsParams to describe the transfer, src/dst addresses, sychronization mode, transfer dimensions etc.
void SCPY_start ( IRES_SDMA_Handle  logicalChannel )

Starts a transfer previously configured on a channel.

Parameters:
[in]logicalChannelPreviously configured logical channel on which to start the transfer.
void SCPY_wait ( IRES_SDMA_Handle  logicalChannel )

Wait for the transfer to complete.

Parameters:
[in]logicalChannelLogical channel on which transfer is ongoing.
Bool SCPY_complete ( IRES_SDMA_Handle  logicalChannel )

Returns status of transfer on the logical channel.

Parameters:
[in]logicalChannelLogical channel on which transfer is ongoing.
Return values:
TRUETransfer completed
FALSETransfer in progress

Define Documentation

#define OMAP_DMA_DATA_TYPE_S8   0x00
#define OMAP_DMA_DATA_TYPE_S16   0x01
#define OMAP_DMA_DATA_TYPE_S32   0x02
#define OMAP_DMA_PORT_EMIFF   0x00
#define OMAP_DMA_AMODE_POST_CONST   0x00
#define OMAP_DMA_AMODE_POST_INC   0x01
#define OMAP_DMA_AMODE_POST_SINGLE_INDEX   0x02
#define OMAP_DMA_AMODE_POST_DOUBLE_INDEX   0x03
#define OMAP_DMA_SYNC_MODE_ELEMENT   0x00

To identify mode of sychronization of transfer.

#define OMAP_DMA_SYNC_MODE_FRAME   0x01
#define OMAP_DMA_SYNC_MODE_BLOCK   0x02
#define OMAP_DMA_SYNC_TYPE_DEST   0x00
#define OMAP_DMA_SYNC_TYPE_SRC   0x01

Typedef Documentation

Parameters of Address (source or destination) of transfer.

Details of Transfer.

typedef struct SCPY_Params SCPY_Params
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated