Data Fields

RcmServer_Struct Struct Reference
[RcmServer]

Opaque client structure large enough to hold an instance object. More...

#include <RcmServer.h>

Data Fields

GateThread_Struct _f1
Ptr _f2
Ptr _f3
Ptr _f4
struct {
   Int   _f1
   Ptr   _f2
_f5
Ptr _f6 [9]
UInt16 _f7
UInt16 _f8
Bool _f9
Int _f10
Ptr _f11 [4]
Ptr _f12

Detailed Description

Opaque client structure large enough to hold an instance object.

Use this structure to define an embedded RcmServer object.

See also:
RcmServer_construct

Field Documentation

GateThread_Struct RcmServer_Struct::_f1
struct { ... } RcmServer_Struct::_f5

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated