ECPY_Obj defines the structure of the dma channel handle that is used to manage state about the EDMA3 channel. More...
#include <ecpy.h>
Data Fields | |
IRES_EDMA3CHAN2_Obj * | iresHandle |
unsigned int | iprRegisterAddr |
unsigned int | iprBitMask |
unsigned int | esrRegisterAddr |
unsigned int | esrBitMask |
short | transferMode |
short | transferPending |
short | finalTransferNo |
IRES_EDMA3CHAN_PaRamStruct * | firstPARAMShadow |
ECPY_Obj defines the structure of the dma channel handle that is used to manage state about the EDMA3 channel.
unsigned int ECPY_Obj::iprRegisterAddr |
unsigned int ECPY_Obj::iprBitMask |
unsigned int ECPY_Obj::esrRegisterAddr |
unsigned int ECPY_Obj::esrBitMask |
short ECPY_Obj::transferMode |