Functions | Defines | Data Structures | Typedefs | Enumerations | Variables

VICPSYNC

Functions

VICPSYNC_Status VICPSYNC_start (IALG_Handle handle, VICPSYNC_ResourceType res, VICPSYNC_InterruptType intType, VICPSYNC_InterruptLine intLine, IRES_VICP2_Handle vicpHandle)
 This is the top level function that allows ARM-side algorithms to mark beginning of the usage of individual functional units of VICP.
VICPSYNC_Status VICPSYNC_wait (IRES_VICP2_Handle vicpHandle, VICPSYNC_ResourceType res)
 This is the top level function that allows the ARM-side algorithms to wait for interrupt corresponding to the functional unit of the VICP to fire.
Bool VICPSYNC_done (IRES_VICP2_Handle vicpHandle, VICPSYNC_ResourceType res)
 This is the top level function that allows the ARM-side algorithms to query the status of the interrupt corresponding to the functional unit that was configured using VICPSYNC_start call.
VICPSYNC_Status VICPSYNC_unregister (IRES_VICP2_Handle vicpHandle, VICPSYNC_ResourceType res)
 This is the top level function that allows the ARM-side algorithms to unregister the ISR associated with the VICP resource that may have been previously registered via a call to VICPSYNC_start.

Defines

#define VICPSYNC_GTNAME   "ti.sdo.fc.vicpsync"

Data Structures

struct  VICPSYNC_Params
 The module configuration structure for VICPSYNC implementation. More...

Typedefs

typedef struct VICPSYNC_Params VICPSYNC_Params
 The module configuration structure for VICPSYNC implementation.
typedef enum VICPSYNC_ResourceType VICPSYNC_ResourceType
 Resource types for which the API can be called.
typedef enum VICPSYNC_InterruptLine VICPSYNC_InterruptLine
 Interrupt line that can be specified for each Resource type.
typedef enum VICPSYNC_InterruptType VICPSYNC_InterruptType
 Interrupt type that can be specified for each Resource type.
typedef enum VICPSYNC_Status VICPSYNC_Status

Enumerations

enum  VICPSYNC_ResourceType {
  VICPSYNC_IMX0,
  VICPSYNC_IMX1,
  VICPSYNC_MJCP,
  VICPSYNC_NSF
}
 

Resource types for which the API can be called.

More...
enum  VICPSYNC_InterruptLine {
  VICPSYNC_FIXED,
  VICPSYNC_FLEXIBLE
}
 

Interrupt line that can be specified for each Resource type.

More...
enum  VICPSYNC_InterruptType {
  VICPSYNC_IRQ,
  VICPSYNC_FIQ
}
 

Interrupt type that can be specified for each Resource type.

More...
enum  VICPSYNC_Status {
  VICPSYNC_OK,
  VICPSYNC_EFAIL,
  VICPSYNC_ENORESOURCE
}

Variables

VICPSYNC_Params VICPSYNC_PARAMS
 Default module configuration structure (defined in vicpsync.c)

Detailed Description

This module is used by frameworks or applications which have xDAIS algorithms that use VICP hardware accelerators.


Function Documentation

VICPSYNC_Status VICPSYNC_start ( IALG_Handle  handle,
VICPSYNC_ResourceType  res,
VICPSYNC_InterruptType  intType,
VICPSYNC_InterruptLine  intLine,
IRES_VICP2_Handle  vicpHandle 
)

This is the top level function that allows ARM-side algorithms to mark beginning of the usage of individual functional units of VICP.

Parameters:
handleAlgorithm handle
resParticular function unit of the VICP to configure
intTypeType of interrupt (FIQ/IRQ) to configure
intLineInterrupt line to use (Fixed/Flexible)
vicpHandlevoid pointer to the vicp handle.
Returns:
VICPSYNC_Status Returns status of this call.
Note:
This function will be called from the algorithm but the implementation will lie in the application.
VICPSYNC_Status VICPSYNC_wait ( IRES_VICP2_Handle  vicpHandle,
VICPSYNC_ResourceType  res 
)

This is the top level function that allows the ARM-side algorithms to wait for interrupt corresponding to the functional unit of the VICP to fire.

Parameters:
vicpHandlevoid pointer to the vicp handle.
resParticular function unit of the VICP that has been configured to respond to interrupt.
Returns:
VICPSYNC_Status Returns status of this call
Note:
As per XDM, this function will be called from the algorithm but the implementation will lie in the application.
Bool VICPSYNC_done ( IRES_VICP2_Handle  vicpHandle,
VICPSYNC_ResourceType  res 
)

This is the top level function that allows the ARM-side algorithms to query the status of the interrupt corresponding to the functional unit that was configured using VICPSYNC_start call.

Parameters:
vicpHandlevoid pointer to the vicp handle.
resParticular functional unit of the VICP to query for status of interrupt.
Returns:
Bool value indicating if the interrupt has fired yet.
Note:
As per XDM, this function will be called from the algorithm but the implementation will lie in the application.
VICPSYNC_Status VICPSYNC_unregister ( IRES_VICP2_Handle  vicpHandle,
VICPSYNC_ResourceType  res 
)

This is the top level function that allows the ARM-side algorithms to unregister the ISR associated with the VICP resource that may have been previously registered via a call to VICPSYNC_start.

Parameters:
vicpHandlevoid pointer to the vicp handle.
resParticular functional unit of the VICP to query for status of interrupt.
Returns:
VICPSYNC_Status Returns status of this call.

Define Documentation

#define VICPSYNC_GTNAME   "ti.sdo.fc.vicpsync"

Name to identify the GT module


Typedef Documentation

The module configuration structure for VICPSYNC implementation.

Resource types for which the API can be called.

Interrupt line that can be specified for each Resource type.

Interrupt type that can be specified for each Resource type.


Enumeration Type Documentation

Resource types for which the API can be called.

Enumerator:
VICPSYNC_IMX0 
VICPSYNC_IMX1 
VICPSYNC_MJCP 
VICPSYNC_NSF 

Interrupt line that can be specified for each Resource type.

Enumerator:
VICPSYNC_FIXED 

Use dedicated line for this resource

VICPSYNC_FLEXIBLE 

Use generic interrupt line for this resource

Interrupt type that can be specified for each Resource type.

Enumerator:
VICPSYNC_IRQ 

Regular Interrupt Request

VICPSYNC_FIQ 

Fast Interrupt Request

Enumerator:
VICPSYNC_OK 

Success

VICPSYNC_EFAIL 

general failure

VICPSYNC_ENORESOURCE 

resources not owned to be able to configure this interrupt


Variable Documentation

Default module configuration structure (defined in vicpsync.c)

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated