Defines | Data Structures | Typedefs | Enumerations | Variables

IRES HDVICP2 Protocol (Beta)

Defines

#define IRES_HDVICP2_PROTOCOLNAME   "ti.sdo.fc.ires.hdvicp.hdvicp2"
 Name used to describe this protocol.
#define HDVICP2_MODNAME   "ti.sdo.fc.ires.hdvicp2"
 Name to pass to Diags_setMask() to enable logging for HDVICP2 functions. For example, Diags_setMask(HDVICP2_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect.
#define IRES_HDVICP2_ID_ANY   -2
 Used to specify the resource required in the protocol args, resource manager will return an HDVICP2 resource that is available to the scratch group.
#define IRES_HDVICP2_ID_LATE_ACQUIRE   -1
 Used to specify the resource required for protocol args, late acquire implies that no resource is to be returned right now, resource will be acquired later in the process call, using the acquire fxn returned via the IRES_HDVICP2_Handle.
#define IRES_HDVICP2_INVALID_ADDR   0xFFFFFFFF
 Used to indicate that the address returned in the IRES_HDVICP2_Handle is not yet valid, and should not be used.
#define IRES_HDVICP2_TIMEOUTFOREVER   ((UInt)(-1))
 Used to indicate to IRES_HDVICP2_Obj::wait() that the call should never timeout.
#define IRES_HDVICP2_UNKNOWNLATEACQUIREARG   (-1)
 Unknown late acquire argument.

Data Structures

struct  IRES_HDVICP2_ProtocolArgs
 HDVICP2 Protocol Arguments definition. More...
struct  IRES_HDVICP2_Obj
 IRES_HDVICP2_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. More...
struct  IRES_HDVICP2_RegisterLayer
 HDVICP2 Register Layout. More...
struct  IRES_HDVICP2_Properties
 Static Resource Properties. More...

Typedefs

typedef struct IRES_HDVICP2_ObjIRES_HDVICP2_Handle
 Handle to "logical" resource.
typedef struct
IRES_HDVICP2_ProtocolArgs 
IRES_HDVICP2_ProtocolArgs
 HDVICP2 Protocol Arguments definition.
typedef void(* IRES_HDVICP2_CallbackFxn )(IALG_Handle handle, Void *args)
 Callback function signature, used by the IRES_HDVICP2_ Handle's configure function.
typedef enum IRES_HDVICP2_Status IRES_HDVICP2_Status
 Describes the status/history of the HDVICP2 unit that is returned by the acquire call. This information can be used by the codec to avoid reloading the data memory or the program memory in the HDVICP2.
typedef struct IRES_HDVICP2_Obj IRES_HDVICP2_Obj
 IRES_HDVICP2_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource.
typedef struct
IRES_HDVICP2_RegisterLayer 
IRES_HDVICP2_RegisterLayer
 HDVICP2 Register Layout.
typedef struct
IRES_HDVICP2_Properties 
IRES_HDVICP2_Properties
 Static Resource Properties.
typedef IRES_Status(* ti_sdo_fc_ires_hdvicp_HDVICP2_GetHdvicp2Fxn )(XDAS_Int32 *Id, IALG_Handle alg, IRES_HDVICP2_Handle handle)
typedef IRES_Status(* ti_sdo_fc_ires_hdvicp_HDVICP2_FreeHdvicp2Fxn )(XDAS_Int32 Id, IALG_Handle alg, IRES_HDVICP2_Handle handle)

Enumerations

enum  IRES_HDVICP2_Status {
  SAMECODEC = 0,
  SAMECODECTYPE = 1,
  DIFFERENTCODEC = 2
}
 

Describes the status/history of the HDVICP2 unit that is returned by the acquire call. This information can be used by the codec to avoid reloading the data memory or the program memory in the HDVICP2.

More...

Variables

unsigned int ti_sdo_fc_ires_hdvicp_HDVICP2_timeoutVal
 Timeout value to be used by implementation of IRES_HDVICP2_Handle:wait function.

Detailed Description

Allows algorithms to request and receive handles representing HDVICP2 resources.


Define Documentation

#define IRES_HDVICP2_PROTOCOLNAME   "ti.sdo.fc.ires.hdvicp.hdvicp2"

Name used to describe this protocol.

#define HDVICP2_MODNAME   "ti.sdo.fc.ires.hdvicp2"

Name to pass to Diags_setMask() to enable logging for HDVICP2 functions. For example, Diags_setMask(HDVICP2_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect.

#define IRES_HDVICP2_ID_ANY   -2

Used to specify the resource required in the protocol args, resource manager will return an HDVICP2 resource that is available to the scratch group.

#define IRES_HDVICP2_ID_LATE_ACQUIRE   -1

Used to specify the resource required for protocol args, late acquire implies that no resource is to be returned right now, resource will be acquired later in the process call, using the acquire fxn returned via the IRES_HDVICP2_Handle.

#define IRES_HDVICP2_INVALID_ADDR   0xFFFFFFFF

Used to indicate that the address returned in the IRES_HDVICP2_Handle is not yet valid, and should not be used.

#define IRES_HDVICP2_TIMEOUTFOREVER   ((UInt)(-1))

Used to indicate to IRES_HDVICP2_Obj::wait() that the call should never timeout.

#define IRES_HDVICP2_UNKNOWNLATEACQUIREARG   (-1)

Unknown late acquire argument.

Remarks:
This definition should be used when a particular algorithm doesn't have an application-provided late acquire argument. The codec should supply IRES_HDVICP2_UNKNOWNLATEACQUIREARG as the argument to acquire() in this case.
See also:
XDM_CmdId::XDM_SETLATEACQUIREARG

Typedef Documentation

Handle to "logical" resource.

HDVICP2 Protocol Arguments definition.

typedef void(* IRES_HDVICP2_CallbackFxn)(IALG_Handle handle, Void *args)

Callback function signature, used by the IRES_HDVICP2_ Handle's configure function.

Describes the status/history of the HDVICP2 unit that is returned by the acquire call. This information can be used by the codec to avoid reloading the data memory or the program memory in the HDVICP2.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.

IRES_HDVICP2_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource.

HDVICP2 Register Layout.

Static Resource Properties.


Enumeration Type Documentation

Describes the status/history of the HDVICP2 unit that is returned by the acquire call. This information can be used by the codec to avoid reloading the data memory or the program memory in the HDVICP2.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
Enumerator:
SAMECODEC 

Same codec was granted this unit, last time

SAMECODECTYPE 

Different codec, but of the same codec class was granted this unit last time

DIFFERENTCODEC 

Completely different codec ran last time


Variable Documentation

Timeout value to be used by implementation of IRES_HDVICP2_Handle:wait function.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated