Functions | Defines | Data Structures | Typedefs | Enumerations | Variables

HDVICPSYNC

Functions

HDVICPSYNC_Status HDVICPSYNC_start (IALG_Handle handle, HDVICPSYNC_InterruptType intType, IRES_HDVICP_Handle hdvicpHandle)
 This function is used to mark the beginning of HDVICP coprocessor usage by the algorithm.
HDVICPSYNC_Status HDVICPSYNC_wait (IRES_HDVICP_Handle hdvicpHandle)
 This is the top level function that allows the ARM-side algorithm to wait for the Kaleido (frame) interrupt to fire.
HDVICPSYNC_Status HDVICPSYNC_unregister (IRES_HDVICP_Handle hdvicpHandle)
 This is the top level function that allows the ARM-side algorithms to explicitly unregister a particular interrupt handler for ISRS registerd via a call to HDVICPSYNC_start API.
Bool HDVICPSYNC_done (IRES_HDVICP_Handle hdvicpHandle)
 This is the top level function that allows the ARM-side algorithm to return a status indicating if a Kaleido interrupt has fired (frame has been processed) since HDVICPSYNC_start was called.

Defines

#define HDVICPSYNC_GTNAME   "ti.sdo.fc.hdvicpsync"
 Name to identify the GT module.

Data Structures

struct  HDVICPSYNC_Params
 The module configuration structure for HDVICPSYNC implementation. More...

Typedefs

typedef struct HDVICPSYNC_Params HDVICPSYNC_Params
 The module configuration structure for HDVICPSYNC implementation.
typedef enum
HDVICPSYNC_InterruptType 
HDVICPSYNC_InterruptType
 Interrupt type that can be specified for each Resource type.
typedef enum HDVICPSYNC_Status HDVICPSYNC_Status

Enumerations

enum  HDVICPSYNC_InterruptType {
  HDVICPSYNC_IRQ,
  HDVICPSYNC_FIQ
}
 

Interrupt type that can be specified for each Resource type.

More...
enum  HDVICPSYNC_Status {
  HDVICPSYNC_OK,
  HDVICPSYNC_EFAIL,
  HDVICPSYNC_ENORESOURCE
}

Variables

HDVICPSYNC_Params HDVICPSYNC_PARAMS
 Default module configuration structure (defined in hdvicpsync.c)

Detailed Description

HDVICPSYNC provides framework support for synchronization between codec and HDVICP coprocessor usage. This module is used by frameworks or applications which have xDAIS algorithms that use HDVICP hardware accelerators.


Function Documentation

HDVICPSYNC_Status HDVICPSYNC_start ( IALG_Handle  handle,
HDVICPSYNC_InterruptType  intType,
IRES_HDVICP_Handle  hdvicpHandle 
)

This function is used to mark the beginning of HDVICP coprocessor usage by the algorithm.

Parameters:
handleAlgorithm handle
intTypeInterrupt Type
hdvicpHandlePointer to the hdvicp handle.
Returns:
none
Note:
This function will be called from the algorithm but the implementation will lie in the application.
HDVICPSYNC_Status HDVICPSYNC_wait ( IRES_HDVICP_Handle  hdvicpHandle )

This is the top level function that allows the ARM-side algorithm to wait for the Kaleido (frame) interrupt to fire.

Parameters:
hdvicpHandlevoid pointer to the hdvicp handle.
Returns:
none
Note:
As per XDM, this function will be called from the algorithm but the implementation will lie in the application.
HDVICPSYNC_Status HDVICPSYNC_unregister ( IRES_HDVICP_Handle  hdvicpHandle )

This is the top level function that allows the ARM-side algorithms to explicitly unregister a particular interrupt handler for ISRS registerd via a call to HDVICPSYNC_start API.

Parameters:
hdvicpHandlevoid pointer to the hdvicp handle.
Returns:
HDVICPSYNC_Status Returns status of this call
Note:
As per XDM, this function will be called from the algorithm but the implementation will lie in the application.
Bool HDVICPSYNC_done ( IRES_HDVICP_Handle  hdvicpHandle )

This is the top level function that allows the ARM-side algorithm to return a status indicating if a Kaleido interrupt has fired (frame has been processed) since HDVICPSYNC_start was called.

Parameters:
hdvicpHandlevoid pointer to the hdvicp handle.
Returns:
none
Note:
As per XDM, this function will be called from the algorithm but the implementation will lie in the application.

Define Documentation

#define HDVICPSYNC_GTNAME   "ti.sdo.fc.hdvicpsync"

Name to identify the GT module.


Typedef Documentation

The module configuration structure for HDVICPSYNC implementation.

Interrupt type that can be specified for each Resource type.


Enumeration Type Documentation

Interrupt type that can be specified for each Resource type.

Enumerator:
HDVICPSYNC_IRQ 

Regular Interrupt Request

HDVICPSYNC_FIQ 

Fast Interrupt Request

Enumerator:
HDVICPSYNC_OK 

Success

HDVICPSYNC_EFAIL 

general failure

HDVICPSYNC_ENORESOURCE 

resources not owned to be able to configure the interrupt


Variable Documentation

Default module configuration structure (defined in hdvicpsync.c)

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated