Functions | Defines | Data Structures | Typedefs

RcmServer.h File Reference


Detailed Description

Remote Command Message Server Module. An RcmServer processes inbound messages received from an RcmClient.

The RcmServer processes inbound messages received from an RcmClient. After processing a message, the server will return the message to the client.

See also:
RcmClient.h
RCM Overview
#include <xdc/runtime/knl/GateThread.h>
#include <xdc/runtime/knl/Thread.h>
Include dependency graph for RcmServer.h:

Go to the source code of this file.

Functions

Int RcmServer_addSymbol (RcmServer_Handle handle, String name, RcmServer_MsgFxn addr, UInt32 *index)
 Add a symbol to the server's function table.
Int RcmServer_construct (RcmServer_Struct *structPtr, String name, const RcmServer_Params *params)
 Initialize a new instance object inside the provided structure.
Int RcmServer_create (String name, RcmServer_Params *params, RcmServer_Handle *handle)
 Create an RcmServer instance.
Int RcmServer_delete (RcmServer_Handle *handlePtr)
 Delete an RcmServer instance.
Int RcmServer_destruct (RcmServer_Struct *structPtr)
 Finalize the instance object inside the provided structure.
Void RcmServer_exit (Void)
 Finalize the RcmServer module.
Void RcmServer_init (Void)
 Initialize the RcmServer module.
Void RcmServer_Params_init (RcmServer_Params *params)
 Initialize the instance create params structure.
Int RcmServer_removeSymbol (RcmServer_Handle handle, String name)
 Remove a symbol and from the server's function table.
Int RcmServer_start (RcmServer_Handle handle)
 Start the server.

Defines

#define RcmServer_S_SUCCESS   (0)
 Success return code.
#define RcmServer_E_FAIL   (-1)
 General failure return code.
#define RcmServer_E_NOMEMORY   (-2)
 The was insufficient memory left on the heap.
#define RcmServer_E_SYMBOLNOTFOUND   (-3)
 The given symbol was not found in the server's symbol table.
#define RcmServer_E_SYMBOLSTATIC   (-4)
 The given symbols is in the static table, it cannot be removed.
#define RcmServer_E_SYMBOLTABLEFULL   (-5)
 The server's symbol table is full.

Data Structures

struct  RcmServer_FxnDesc
 Function descriptor. More...
struct  RcmServer_FxnDescAry
 Function descriptor array. More...
struct  RcmServer_ThreadPoolDesc
 Worker pool descriptor. More...
struct  RcmServer_ThreadPoolDescAry
 Worker pool descriptor array. More...
struct  RcmServer_Params
 RcmServer Instance create parameters. More...
struct  RcmServer_Struct
 Opaque client structure large enough to hold an instance object. More...

Typedefs

typedef Int32(* RcmServer_MsgFxn )(UInt32, UInt32 *)
 Remote function type.
typedef struct
RcmServer_Object_tag * 
RcmServer_Handle
 RcmServer instance object handle.
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated