IRESMAN_Fxns Struct Reference
[Resource manager interface]

#include <iresman.h>

Collaboration diagram for IRESMAN_Fxns:
Collaboration graph
[legend]

Data Fields

String(* getProtocolName )()
 Function to query the name of the protocol.
IRES_ProtocolRevision *(* getProtocolRevision )()
 Function to query the revision of hte protocol.
IRES_Status(* init )(IRESMAN_Params *initArgs)
 Function to create and initialize the device specific resource manager implementation.
IRES_Status(* exit )()
 Function called when RESMAN is no longer needed. Use it to free memory allocated etc.
IRES_Handle(* getHandle )(IALG_Handle algHandle, IRES_ProtocolArgs *protocolArgs, Int scratchGroupId, IRES_Status *status)
 Function that returns the IRES_Handle to resource requested using the IRES_ProtocolArgs.
IRES_Status(* freeHandle )(IALG_Handle algHandle, IRES_Handle resourceHandle, IRES_ProtocolArgs *protocolArgs, Int scratchGroupId)
 Frees handles back to the resource pool.

Field Documentation

Function to query the name of the protocol.

Function to query the revision of hte protocol.

Return values:
Pointer to the protocol revision structure

Function to create and initialize the device specific resource manager implementation.

Parameters:
[in] initArgs Initialization arguments maybe interpreted by device specific implementation
Return values:
IRESMAN_EOK Success IRESMAN_EEXISTS RESMAN already initialized IRESMAN_EERROR RESMAN could not be initialized

Function called when RESMAN is no longer needed. Use it to free memory allocated etc.

Return values:
IRESMAN_EOK Success IRESMAN_ENOINIT RESMAN not initialized IRESMAN_EERROR RESMAN could not be reset
IRES_Handle(* IRESMAN_Fxns::getHandle)(IALG_Handle algHandle, IRES_ProtocolArgs *protocolArgs, Int scratchGroupId, IRES_Status *status)

Function that returns the IRES_Handle to resource requested using the IRES_ProtocolArgs.

Parameters:
[in] algHandle Handle of the algorithm that is requesting the resources
[in] protocolArgs Arguments to be interpreted by IRES_Manager implementation to determine actual physical resources to obtain
[in] scratchGroupId Scratch Group Id where resources should be allocated
[out] status IRESMAN_EOK Success IRESMAN_ENORESOURCE Resource unavailable IRESMAN_EERROR Error obtaining handles
IRES_Status(* IRESMAN_Fxns::freeHandle)(IALG_Handle algHandle, IRES_Handle resourceHandle, IRES_ProtocolArgs *protocolArgs, Int scratchGroupId)

Frees handles back to the resource pool.

Parameters:
[in] algHandle Handle of the algorithm that is releasing the resources
[in] resourceHandle Handle that is to be released
[in] protocolArgs Arguments that help determine which resources to free
Return values:
IRESMAN_EOK Success IRESMAN_EERROR Handle could not be freed

The documentation for this struct was generated from the following file:

Copyright 2010, Texas Instruments Incorporated