Generic Trace Support

The "Generic Tracing" module. Provides producers of content the ability to, in a runtime-independant way, add tracing. Also provides consumers of trace-enabled content the mechanisms necessary to enable/disable the various trace statements. More...

Data Structures

struct  GT_Mask
 Object representing a GT module instance. More...

Defines

#define GT_ENTER   ((UInt8)0x01)
 Mask for tracing entry and exit points within functions.
#define GT_1CLASS   ((UInt8)0x02)
#define GT_2CLASS   ((UInt8)0x04)
#define GT_3CLASS   ((UInt8)0x08)
#define GT_4CLASS   ((UInt8)0x10)
#define GT_5CLASS   ((UInt8)0x20)
 User mask 5. By convention, used for benchmarking related tracing.
#define GT_6CLASS   ((UInt8)0x40)
 User mask 6. By convention, used for internal warning related tracing.
#define GT_7CLASS   ((UInt8)0x80)
 User mask 7. By convention, used for internal error related tracing.
#define GT_create(mask, modName)   _GT_create((mask), (modName))
#define GT_set(str)   _GT_set(str)
#define GT_0trace(mask, classId, format)
#define GT_1trace(mask, classId, format, arg1)
#define GT_2trace(mask, classId, format, arg1, arg2)
#define GT_3trace(mask, classId, format, arg1, arg2, arg3)
#define GT_4trace(mask, classId, format, arg1, arg2, arg3, arg4)
#define GT_5trace(mask, classId, format, arg1, arg2, arg3, arg4, arg5)
#define GT_6trace(mask, classId, format, arg1, arg2, arg3, arg4, arg5, arg6)

Functions

Void _GT_create (GT_Mask *mask, String modName)
 Initialize a GT mask.
Void GT_init (Void)
 Initialize the GT module.
Void _GT_set (String str)
 Modify the current trace mask settings.
Int _GT_trace (GT_Mask *mask, Int classId, String format,...)
 Conditionally emit a trace statement.

Detailed Description

The "Generic Tracing" module. Provides producers of content the ability to, in a runtime-independant way, add tracing. Also provides consumers of trace-enabled content the mechanisms necessary to enable/disable the various trace statements.

Remarks:
Note that the public APIs (e.g. GT_create()) are implemented as macros around private services of a similar name, but prefixed with an underscore (e.g. _GT_create()). This enables GT tracing to be conditionally compiled out of code bases. Users of the GT APIs should never call the private services (indicated by convention with a leading underscore '_'). Rather, they should restrict usage to the public APIs (i.e., call GT_1trace(), not _GT_trace()).

Define Documentation

#define GT_ENTER   ((UInt8)0x01)

Mask for tracing entry and exit points within functions.

#define GT_1CLASS   ((UInt8)0x02)

User mask 1.

#define GT_2CLASS   ((UInt8)0x04)

User mask 2.

#define GT_3CLASS   ((UInt8)0x08)

User mask 3.

#define GT_4CLASS   ((UInt8)0x10)

User mask 4.

#define GT_5CLASS   ((UInt8)0x20)

User mask 5. By convention, used for benchmarking related tracing.

#define GT_6CLASS   ((UInt8)0x40)

User mask 6. By convention, used for internal warning related tracing.

#define GT_7CLASS   ((UInt8)0x80)

User mask 7. By convention, used for internal error related tracing.

#define GT_create ( mask,
modName   )     _GT_create((mask), (modName))

Initialize a GT mask.

Parameters:
[in] mask Address of an existing GT_Mask structure.
[in] modName Module name to be associated with this mask.
Precondition:
mask must point to a pre-allocated GT_Mask structure. Typically this memory is set aside as a static global variable for simplicity, althought that need not be the case.
Remarks:
This function should not be called directly. Users should use the GT_create() macro wrapping this function instead, to enable conditional removal of tracing from the client binaries.
modName must be unique within the entire system. To that end, it typically contains the client package's name.

#define GT_set ( str   )     _GT_set(str)

Modify the current trace mask settings.

Parameters:
[in] str New trace format string.
Remarks:
_GT_set() should not be called directly. Users should use the GT_set() macro which wraps _GT_set() instead, to enable conditional removal of tracing from the client binaries.

#define GT_0trace ( mask,
classId,
format   ) 
Value:
((*(mask).flags & (classId)) ? \
    _GT_trace(&(mask), (classId), (format)) : 0)
See also:
_GT_trace()
#define GT_1trace ( mask,
classId,
format,
arg1   ) 
Value:
((*(mask).flags & (classId)) ? \
    _GT_trace(&(mask), (classId), (format), (arg1)) : 0)
See also:
_GT_trace()
#define GT_2trace ( mask,
classId,
format,
arg1,
arg2   ) 
Value:
((*(mask).flags & (classId)) ? \
    _GT_trace(&(mask), (classId), (format), (arg1), (arg2)) : 0)
See also:
_GT_trace()
#define GT_3trace ( mask,
classId,
format,
arg1,
arg2,
arg3   ) 
Value:
((*(mask).flags & (classId)) ? \
    _GT_trace(&(mask), (classId), (format), (arg1), (arg2), (arg3)) : 0)
See also:
_GT_trace()
#define GT_4trace ( mask,
classId,
format,
arg1,
arg2,
arg3,
arg4   ) 
Value:
((*(mask).flags & (classId)) ? \
    _GT_trace(&(mask), (classId), (format), (arg1), (arg2), (arg3), (arg4)) : 0)
See also:
_GT_trace()
#define GT_5trace ( mask,
classId,
format,
arg1,
arg2,
arg3,
arg4,
arg5   ) 
Value:
((*(mask).flags & (classId)) ? \
    _GT_trace(&(mask), (classId), (format), (arg1), (arg2), (arg3), (arg4), (arg5)) : 0)
See also:
_GT_trace()
#define GT_6trace ( mask,
classId,
format,
arg1,
arg2,
arg3,
arg4,
arg5,
arg6   ) 
Value:
((*(mask).flags & (classId)) ? \
    _GT_trace(&(mask), (classId), (format), (arg1), (arg2), (arg3), (arg4), \
        (arg5), (arg6)) : 0)
See also:
_GT_trace()

Function Documentation

Void _GT_create ( GT_Mask mask,
String  modName 
)

Initialize a GT mask.

Parameters:
[in] mask Address of an existing GT_Mask structure.
[in] modName Module name to be associated with this mask.
Precondition:
mask must point to a pre-allocated GT_Mask structure. Typically this memory is set aside as a static global variable for simplicity, althought that need not be the case.
Remarks:
This function should not be called directly. Users should use the GT_create() macro wrapping this function instead, to enable conditional removal of tracing from the client binaries.
modName must be unique within the entire system. To that end, it typically contains the client package's name.
Void GT_init ( Void   ) 

Initialize the GT module.

Remarks:
GT_init() can be called multiple times, and should be called by all explicit users of GT.
Void _GT_set ( String  str  ) 

Modify the current trace mask settings.

Parameters:
[in] str New trace format string.
Remarks:
_GT_set() should not be called directly. Users should use the GT_set() macro which wraps _GT_set() instead, to enable conditional removal of tracing from the client binaries.
Int _GT_trace ( GT_Mask mask,
Int  classId,
String  format,
  ... 
)

Conditionally emit a trace statement.

Parameters:
[in] mask Mask associated with this trace statement.
[in] classId class of this trace statement.
[in] format printf-style format string.
Remarks:
This function should not be called directly. Users should use the macros wrapping this function instead (e.g. GT_1trace()) to enable conditional removal of tracing from the client binaries.
classId can be a logically OR'd set of classes. Doing so will cause the trace to be emitted if any of the classId classes are enabled in the current settings of the mask.
Most, but not all printf format strings are supported.
Precondition:
mask must have been initialized with GT_create().
See also:
GT_create()

Copyright 2010, Texas Instruments Incorporated