VICPSYNC

Data Structures

struct  VICPSYNC_Params
 The module configuration structure for VICPSYNC implementation. More...

Defines

#define VICPSYNC_GTNAME   "ti.sdo.fc.vicpsync"

Enumerations

enum  VICPSYNC_ResourceType {
  VICPSYNC_IMX0,
  VICPSYNC_IMX1,
  VICPSYNC_MJCP,
  VICPSYNC_NSF
}
 

Resource types for which the API can be called.

More...
enum  VICPSYNC_InterruptLine {
  VICPSYNC_FIXED,
  VICPSYNC_FLEXIBLE
}
 

Interrupt line that can be specified for each Resource type.

More...
enum  VICPSYNC_InterruptType {
  VICPSYNC_IRQ,
  VICPSYNC_FIQ
}
 

Interrupt type that can be specified for each Resource type.

More...
enum  VICPSYNC_Status {
  VICPSYNC_OK,
  VICPSYNC_EFAIL,
  VICPSYNC_ENORESOURCE
}

Functions

VICPSYNC_Status VICPSYNC_start (IALG_Handle handle, VICPSYNC_ResourceType res, VICPSYNC_InterruptType intType, VICPSYNC_InterruptLine intLine, IRES_VICP2_Handle vicpHandle)
 This is the top level function that allows ARM-side algorithms to mark beginning of the usage of individual functional units of VICP.
VICPSYNC_Status VICPSYNC_wait (IRES_VICP2_Handle vicpHandle, VICPSYNC_ResourceType res)
 This is the top level function that allows the ARM-side algorithms to wait for interrupt corresponding to the functional unit of the VICP to fire.
Bool VICPSYNC_done (IRES_VICP2_Handle vicpHandle, VICPSYNC_ResourceType res)
 This is the top level function that allows the ARM-side algorithms to query the status of the interrupt corresponding to the functional unit that was configured using VICPSYNC_start call.
VICPSYNC_Status VICPSYNC_unregister (IRES_VICP2_Handle vicpHandle, VICPSYNC_ResourceType res)
 This is the top level function that allows the ARM-side algorithms to unregister the ISR associated with the VICP resource that may have been previously registered via a call to VICPSYNC_start.

Variables

VICPSYNC_Params VICPSYNC_PARAMS
 Default module configuration structure (defined in vicpsync.c).

Detailed Description

This module is used by frameworks or applications which have xDAIS algorithms that use VICP hardware accelerators.


Define Documentation

#define VICPSYNC_GTNAME   "ti.sdo.fc.vicpsync"

Name to identify the GT module


Enumeration Type Documentation

Resource types for which the API can be called.

Enumerator:
VICPSYNC_IMX0 
VICPSYNC_IMX1 
VICPSYNC_MJCP 
VICPSYNC_NSF 

Interrupt line that can be specified for each Resource type.

Enumerator:
VICPSYNC_FIXED 

Use dedicated line for this resource

VICPSYNC_FLEXIBLE 

Use generic interrupt line for this resource

Interrupt type that can be specified for each Resource type.

Enumerator:
VICPSYNC_IRQ 

Regular Interrupt Request

VICPSYNC_FIQ 

Fast Interrupt Request

Enumerator:
VICPSYNC_OK 

Success

VICPSYNC_EFAIL 

general failure

VICPSYNC_ENORESOURCE 

resources not owned to be able to configure this interrupt


Function Documentation

VICPSYNC_Status VICPSYNC_start ( IALG_Handle  handle,
VICPSYNC_ResourceType  res,
VICPSYNC_InterruptType  intType,
VICPSYNC_InterruptLine  intLine,
IRES_VICP2_Handle  vicpHandle 
)

This is the top level function that allows ARM-side algorithms to mark beginning of the usage of individual functional units of VICP.

Parameters:
handle Algorithm handle
res Particular function unit of the VICP to configure
intType Type of interrupt (FIQ/IRQ) to configure
intLine Interrupt line to use (Fixed/Flexible)
vicpHandle void pointer to the vicp handle.
Returns:
VICPSYNC_Status Returns status of this call.
Note:
This function will be called from the algorithm but the implementation will lie in the application.
VICPSYNC_Status VICPSYNC_wait ( IRES_VICP2_Handle  vicpHandle,
VICPSYNC_ResourceType  res 
)

This is the top level function that allows the ARM-side algorithms to wait for interrupt corresponding to the functional unit of the VICP to fire.

Parameters:
vicpHandle void pointer to the vicp handle.
res Particular function unit of the VICP that has been configured to respond to interrupt.
Returns:
VICPSYNC_Status Returns status of this call
Note:
As per XDM, this function will be called from the algorithm but the implementation will lie in the application.
Bool VICPSYNC_done ( IRES_VICP2_Handle  vicpHandle,
VICPSYNC_ResourceType  res 
)

This is the top level function that allows the ARM-side algorithms to query the status of the interrupt corresponding to the functional unit that was configured using VICPSYNC_start call.

Parameters:
vicpHandle void pointer to the vicp handle.
res Particular functional unit of the VICP to query for status of interrupt.
Returns:
Bool value indicating if the interrupt has fired yet.
Note:
As per XDM, this function will be called from the algorithm but the implementation will lie in the application.
VICPSYNC_Status VICPSYNC_unregister ( IRES_VICP2_Handle  vicpHandle,
VICPSYNC_ResourceType  res 
)

This is the top level function that allows the ARM-side algorithms to unregister the ISR associated with the VICP resource that may have been previously registered via a call to VICPSYNC_start.

Parameters:
vicpHandle void pointer to the vicp handle.
res Particular functional unit of the VICP to query for status of interrupt.
Returns:
VICPSYNC_Status Returns status of this call.

Variable Documentation

Default module configuration structure (defined in vicpsync.c).


Copyright 2010, Texas Instruments Incorporated