HDVICPSYNC

Data Structures

struct  HDVICPSYNC_Params
 The module configuration structure for HDVICPSYNC implementation. More...

Defines

#define HDVICPSYNC_GTNAME   "ti.sdo.fc.hdvicpsync"
 Name to identify the GT module.

Enumerations

enum  HDVICPSYNC_InterruptType {
  HDVICPSYNC_IRQ,
  HDVICPSYNC_FIQ
}
 

Interrupt type that can be specified for each Resource type.

More...
enum  HDVICPSYNC_Status {
  HDVICPSYNC_OK,
  HDVICPSYNC_EFAIL,
  HDVICPSYNC_ENORESOURCE
}

Functions

HDVICPSYNC_Status HDVICPSYNC_start (IALG_Handle handle, HDVICPSYNC_InterruptType intType, IRES_HDVICP_Handle hdvicpHandle)
 This function is used to mark the beginning of HDVICP coprocessor usage by the algorithm.
HDVICPSYNC_Status HDVICPSYNC_wait (IRES_HDVICP_Handle hdvicpHandle)
 This is the top level function that allows the ARM-side algorithm to wait for the Kaleido (frame) interrupt to fire.
HDVICPSYNC_Status HDVICPSYNC_unregister (IRES_HDVICP_Handle hdvicpHandle)
 This is the top level function that allows the ARM-side algorithms to explicitly unregister a particular interrupt handler for ISRS registerd via a call to HDVICPSYNC_start API.
Bool HDVICPSYNC_done (IRES_HDVICP_Handle hdvicpHandle)
 This is the top level function that allows the ARM-side algorithm to return a status indicating if a Kaleido interrupt has fired (frame has been processed) since HDVICPSYNC_start was called.

Variables

HDVICPSYNC_Params HDVICPSYNC_PARAMS
 Default module configuration structure (defined in hdvicpsync.c).

Detailed Description

HDVICPSYNC provides framework support for synchronization between codec and HDVICP coprocessor usage. This module is used by frameworks or applications which have xDAIS algorithms that use HDVICP hardware accelerators.


Define Documentation

#define HDVICPSYNC_GTNAME   "ti.sdo.fc.hdvicpsync"

Name to identify the GT module.


Enumeration Type Documentation

Interrupt type that can be specified for each Resource type.

Enumerator:
HDVICPSYNC_IRQ 

Regular Interrupt Request

HDVICPSYNC_FIQ 

Fast Interrupt Request

Enumerator:
HDVICPSYNC_OK 

Success

HDVICPSYNC_EFAIL 

general failure

HDVICPSYNC_ENORESOURCE 

resources not owned to be able to configure the interrupt


Function Documentation

HDVICPSYNC_Status HDVICPSYNC_start ( IALG_Handle  handle,
HDVICPSYNC_InterruptType  intType,
IRES_HDVICP_Handle  hdvicpHandle 
)

This function is used to mark the beginning of HDVICP coprocessor usage by the algorithm.

Parameters:
handle Algorithm handle
intType Interrupt Type
hdvicpHandle Pointer to the hdvicp handle.
Returns:
none
Note:
This function will be called from the algorithm but the implementation will lie in the application.
HDVICPSYNC_Status HDVICPSYNC_wait ( IRES_HDVICP_Handle  hdvicpHandle  ) 

This is the top level function that allows the ARM-side algorithm to wait for the Kaleido (frame) interrupt to fire.

Parameters:
hdvicpHandle void pointer to the hdvicp handle.
Returns:
none
Note:
As per XDM, this function will be called from the algorithm but the implementation will lie in the application.
HDVICPSYNC_Status HDVICPSYNC_unregister ( IRES_HDVICP_Handle  hdvicpHandle  ) 

This is the top level function that allows the ARM-side algorithms to explicitly unregister a particular interrupt handler for ISRS registerd via a call to HDVICPSYNC_start API.

Parameters:
hdvicpHandle void pointer to the hdvicp handle.
Returns:
HDVICPSYNC_Status Returns status of this call
Note:
As per XDM, this function will be called from the algorithm but the implementation will lie in the application.
Bool HDVICPSYNC_done ( IRES_HDVICP_Handle  hdvicpHandle  ) 

This is the top level function that allows the ARM-side algorithm to return a status indicating if a Kaleido interrupt has fired (frame has been processed) since HDVICPSYNC_start was called.

Parameters:
hdvicpHandle void pointer to the hdvicp handle.
Returns:
none
Note:
As per XDM, this function will be called from the algorithm but the implementation will lie in the application.

Variable Documentation

Default module configuration structure (defined in hdvicpsync.c).


Copyright 2010, Texas Instruments Incorporated