Main Page
Modules
Data Structures
Files
Directories
Related Pages
Data Structures
Data Structure Index
Data Fields
SHMBUF_Params Struct Reference
[
Shared Memory Buffer Protocol
]
SHMBUF specific params.
More...
#include <
shmbuf.h
>
Collaboration diagram for SHMBUF_Params:
[
legend
]
Data Fields
IRESMAN_Params
iresConfig
Int
bufsize
UInt32
key
UInt32
isScratch
Detailed Description
SHMBUF specific params.
Remarks:
This struct extends
IRESMAN_Params
. These params are used to initialize the resource.
Field Documentation
IRESMAN_Params
SHMBUF_Params::iresConfig
Int
SHMBUF_Params::bufsize
UInt32
SHMBUF_Params::key
UInt32
SHMBUF_Params::isScratch
The documentation for this struct was generated from the following file:
shmbuf.h
Copyright 2009, Texas Instruments Incorporated