IRES_ADDRSPACE_Obj Struct Reference

IRES_ADDRSPACE_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource. More...

#include <ires_addrspace.h>

Collaboration diagram for IRES_ADDRSPACE_Obj:
Collaboration graph
[legend]

Data Fields

IRES_Obj ires
Void * addr
unsigned int len

Detailed Description

IRES_ADDRSPACE_Obj extends the generic IRES_Obj structure that is returned back to the algorithm requesting the resource.


Field Documentation


The documentation for this struct was generated from the following file:

Copyright 2009, Texas Instruments Incorporated