Defines |
#define | DSKT2_GTNAME "ti.sdo.fc.dskt2" |
#define | DSKT2_NUM_SCRATCH_GROUPS 20 |
#define | DSKT2_MAX_MEM_ALLOCATION_SIZE 0xFFFF |
#define | DSKT2_NUM_SHAREDHEAPS 2 |
Typedefs |
typedef Void(* | DSKT2_CacheWBInvFxn )(Ptr blockPtr, size_t byteCnt, Bool wait) |
| Function prototype of cache writeback function: Writes back the memory within the range of blockPtr and blockPtr + byteCnt.
|
Functions |
Void | DSKT2_activateAlg (Int scratchMutexId, IALG_Handle alg) |
| Prepares a xDAIS algorithm instance object to start using its scratch memory.
|
Int | DSKT2_controlAlg (IALG_Handle alg, IALG_Cmd cmd, IALG_Status *status) |
| This is a convenience API to call a xDAIS algorithm instance's algControl function.
|
IALG_Handle | DSKT2_createAlg (Int scratchMutexId, IALG_Fxns *fxns, IALG_Handle parent, IALG_Params *params) |
| Creates and initializes a xDAIS algorithm instance object.
|
IALG_Handle | DSKT2_createAlg2 (Int scratchMutexId, IALG_Fxns *fxns, IALG_Handle parent, IALG_Params *params, Int extHeapId) |
| Creates and initializes a xDAIS algorithm instance object.
|
IALG_Handle | DSKT2_createAlgExt (Int scratchId, IALG_Fxns *fxns, IALG_Handle parent, IALG_Params *params) |
| Creates and initializes a xDAIS algorithm instance object, allocating all algorithm memory in external memory.
|
Void | DSKT2_deactivateAlg (Int scratchMutexId, IALG_Handle alg) |
| Prepares a xDAIS algorithm instance object to give up using its scratch memory.
|
Int | DSKT2_deactivateAll () |
| All algorithms that have been deactivated lazily are now really deactivate. Any algorithms that are still currently active will be left as is. The number of algorithms that are still active will be returned from this call.
|
Bool | DSKT2_freeAlg (Int scratchMutexId, IALG_Handle alg) |
| Deletes a xDAIS algorithm instance object and frees all persistent memory allocated for the instance object.
|
Bool | DSKT2_allocScratch (IALG_Handle alg, Int mutexId, IALG_MemRec *memTab, Int numRecs) |
| Alocates memory from a DSKT2 shared scratch group buffer.
|
Void | DSKT2_freeScratch (Int mutexId, Void *addr, Uns size) |
| Alocates memory from a DSKT2 shared scratch group buffer.
|
Bool | DSKT2_allocPersistent (IALG_MemRec *memTab, Int numRecs) |
| Alocates persistent memory to the requesting algorithm.
|
Void | DSKT2_freePersistent (IALG_MemRec *memTab, Int numRecs) |
| Frees persistent memory from the requesting algorithm.
|
The xDAIS Socket Library provides services to support the creation, initialization, control, and deletion of xDAIS algorithm instance objects.
Void DSKT2_activateAlg |
( |
Int |
scratchMutexId, |
|
|
IALG_Handle |
alg | |
|
) |
| | |
Prepares a xDAIS algorithm instance object to start using its scratch memory.
DSKT2_activateAlg() performs all scratch memory initialization for an algorithm's instance object. After a successful return from DSKT2_activateAlg(), the algorithm's instance object is ready to be used to process data.
Unless the instance is already active, DSKT2_activateAlg() uses the algorithm's IALG interface function algActivate to initialize the algorithm instance's scratch buffers from persistent data memory.
DSKT2_activateAlg() must be called before any processing or control methods of the algorithm instance can be called.
DSKT2 maintains state information about current "active" algorithm instances at run-time, so that it does not perform unnecessary IALG "activation" calls when alg is already active. As part of this optimization it may call the algDeactivate method of the currently active algorithm instance in order to activate this algorithm instance (alg).
- Parameters:
-
[in] | scratchMutexId | scratch-group Id used to associate the instance with a scratch group. The value must be the same id used when creating this algorithm instance. |
[in] | alg | IALG_Handle of the algorithm instance to be activated. |
- Return values:
-
- Precondition:
- alg must be a valid handle for the algorithm's instance object returned by an earlier call to DSKT2_createAlg()
-
If alg uses DMA (IDMA2) dmaInit must be called before calling this methed, ensuring that all of the instance's persistent memory is initialized and the object is ready to be used
-
No other algorithm method is currently being run on this instance. This method never preempts any other method on the same instance.
- Postcondition:
- All of the instance's persistent and scratch memory is initialized and the object is ready to be used.
- See also:
- DSKT2_deactivateAlg()
-
DMAN_addAlg()
Creates and initializes a xDAIS algorithm instance object.
It uses the algorithm's IALG interface functions to query the algorithm for its memory needs then allocates the memory for the algorithm and calls the algorithm's algInit function to let the new algorithm instance object initialize itself using the allocated memory.
DSKT2_createAlg() performs initialization necessary to complete the run-time creation of an algorithm's instance object. After a successful return from DSKT2_createAlg(), the algorithm's instance object can be activated via a DSKT2_activateAlg() before it can be used to process data.
DSKT2_createAlg() tries to dynamically allocate instance memory based on the IALG_MemSpace attribute of the requested memory. Global DSKT2 configuration settings allow OEM to designate a memory heap for each IALG_MemSpace. DSKT2_createAlg() attempts to allocate memory in the requested space, but may search for alternative heaps when preferred heap is not large enough.
- Parameters:
-
[in] | scratchMutexId | Scratch-group Id for determining the shared scratch memory buffer. Value -1 is used to disable scratch sharing for this algorithm instance. A value between 0 and (DSKT2_NUM_SCRATCH_GROUPS-1) indicates a valid scratch group |
[in] | fxns | Pointer to the algorithm's IALG_Fxns table. |
[in] | parent | Handle of parent algorithm (optional). |
[in] | params | Pointer to an IALG_Params structure. |
- Return values:
-
| non-NULL | IALG_Handle for the new instance object. |
| NULL | Failure. |
- Precondition:
- fxns is a valid pointer to an IALG_Fxns structure (containing the vtable for a XDAIS compliant algorithm)
- Postcondition:
- If scratchMutexId is -1, all instance scratch memory is allocated as persistent (i.e. not shared) and instance operation does not require mutual exclusion
-
With the exception of any initialization performed by algActivate and (IDMA2) dmaInit all of the instance's persistent memory is initialized and the object is ready to be used
- Note:
- The parent argument is a handle to another algorithm instance object. This parameter is often NULL, indicating that no parent object exists. This parameter allows clients to create a shared algorithm instance object and pass it to other algorithm instances. For example, a parent instance object might contain global read-only tables that are used by several instances of a vocoder.
- Note:
- The params argument is a pointer to algorithm-specific parameters that are necessary for the creation and initialization of the instance object. This pointer points to the same parameters passed to the algorithm's IALG algAlloc function. However, this pointer may be NULL. In this case, algorithm's IALG function algInit, must assume default creation parameters.
- See also:
- DSKT2_activateAlg(), DSKT2_deactivateAlg(), DSKT2_freeAlg()
Creates and initializes a xDAIS algorithm instance object.
It uses the algorithm's IALG interface functions to query the algorithm for its memory needs then allocates the memory for the algorithm and calls the algorithm's algInit function to let the new algorithm instance object initialize itself using the allocated memory.
DSKT2_createAlg2() performs initialization necessary to complete the run-time creation of an algorithm's instance object. After a successful return from DSKT2_createAlg2(), the algorithm's instance object can be activated via a DSKT2_activateAlg() before it can be used to process data.
DSKT2_createAlg2() tries to dynamically allocate instance memory based on the IALG_MemSpace attribute of the requested memory. Global DSKT2 configuration settings allow OEM to designate a memory heap for each IALG_MemSpace. DSKT2_createAlg2() attempts to allocate memory in the requested space, but may search for alternative heaps when preferred heap is not large enough.
DSKT2_createAlg2() will attempt to use the heap specified by the input parameter, extHeapId, for all allocations in the IALG_MemSpace, IALG_ESDATA. Furthermore, this holds for any IALG_MemSpace that has been configured with the same memory segment as IALG_ESDATA. e.g., if IALG_ESDATA and IALG_SARAM3 have both been configured to use the heap in the memory segment EXTMEM, then DSKT2_createAlg2() will attempt to allocate memory requested in the spaces IALG_SARAM3 and IALG_ESDATA, from the heap, extHeapId.
- Parameters:
-
[in] | scratchMutexId | Scratch-group Id for determining the shared scratch memory buffer. Value -1 is used to disable scratch sharing for this algorithm instance. A value between 0 and (DSKT2_NUM_SCRATCH_GROUPS-1) indicates a valid scratch group |
[in] | fxns | Pointer to the algorithm's IALG_Fxns table. |
[in] | parent | Handle of parent algorithm (optional). |
[in] | params | Pointer to an IALG_Params structure. |
[in] | extHeapId | Segment Id of memory heap to be used for all allocations in memory space IALG_ESDATA. This segment will be used instead of the default external memory segment. |
- Return values:
-
| non-NULL | IALG_Handle for the new instance object. |
| NULL | Failure. |
- Precondition:
- fxns is a valid pointer to an IALG_Fxns structure (containing the vtable for a XDAIS compliant algorithm)
-
extHeapId >= 0
- Postcondition:
- If scratchMutexId is -1, all instance scratch memory is allocated as persistent (i.e. not shared) and instance operation does not require mutual exclusion
-
With the exception of any initialization performed by algActivate and (IDMA2) dmaInit all of the instance's persistent memory is initialized and the object is ready to be used
- Note:
- The parent argument is a handle to another algorithm instance object. This parameter is often NULL, indicating that no parent object exists. This parameter allows clients to create a shared algorithm instance object and pass it to other algorithm instances. For example, a parent instance object might contain global read-only tables that are used by several instances of a vocoder.
- Note:
- The params argument is a pointer to algorithm-specific parameters that are necessary for the creation and initialization of the instance object. This pointer points to the same parameters passed to the algorithm's IALG algAlloc function. However, this pointer may be NULL. In this case, algorithm's IALG function algInit, must assume default creation parameters.
- See also:
- DSKT2_activateAlg(), DSKT2_deactivateAlg(), DSKT2_freeAlg()
Creates and initializes a xDAIS algorithm instance object, allocating all algorithm memory in external memory.
This API is very similar to DSKT2_createAlg(), in that it uses the algorithm's IALG interface functions to query the algorithm for its memory needs, allocates the memory for the algorithm and calls the algorithm's algInit function to let the new algorithm instance object initialize itself using the allocated memory. Unlike DSKT2_createAlg(), however, DSKT2_createAlgExt() will ignore the space
field of the IALG_MemRec
table entries filled in by the algorithm's algAlloc() function, and allocate all of the memory in the memory segment that is mapped to DSKT2.ESDATA.
After a successful return from DSKT2_createAlgExt(), the algorithm's instance object can be activated via a DSKT2_activateAlg() before it can be used to process data.
- Parameters:
-
[in] | scratchId | Scratch-group Id for determining the shared scratch memory buffer. Value -1 is used to disable scratch sharing for this algorithm instance. A value between 0 and (DSKT2_NUM_SCRATCH_GROUPS-1) indicates a valid scratch group |
[in] | fxns | Pointer to the algorithm's IALG_Fxns table. |
[in] | parent | Handle of parent algorithm (optional). |
[in] | params | Pointer to an IALG_Params structure. |
- Return values:
-
| non-NULL | IALG_Handle for the new instance object. |
| NULL | Failure. |
- Precondition:
- fxns is a valid pointer to an IALG_Fxns structure (containing the vtable for a XDAIS compliant algorithm)
- Postcondition:
- If scratchMutexId is -1, all instance scratch memory is allocated as persistent (i.e. not shared) and instance operation does not require mutual exclusion
-
With the exception of any initialization performed by algActivate and (IDMA2 or IDMA3) dmaInit all of the instance's persistent memory is initialized and the object is ready to be used
- Note:
- The parent argument is a handle to another algorithm instance object. This parameter is often NULL, indicating that no parent object exists. This parameter allows clients to create a shared algorithm instance object and pass it to other algorithm instances. For example, a parent instance object might contain global read-only tables that are used by several instances of a vocoder.
- Note:
- The params argument is a pointer to algorithm-specific parameters that are necessary for the creation and initialization of the instance object. This pointer points to the same parameters passed to the algorithm's IALG algAlloc function. However, this pointer may be NULL. In this case, algorithm's IALG function algInit, must assume default creation parameters.
- See also:
- DSKT2_activateAlg(), DSKT2_deactivateAlg(), DSKT2_freeAlg()
Void DSKT2_deactivateAlg |
( |
Int |
scratchMutexId, |
|
|
IALG_Handle |
alg | |
|
) |
| | |
Prepares a xDAIS algorithm instance object to give up using its scratch memory.
DSKT2_deactivateAlg() marks an algorithm's shared scratch memory as available to other instances activation. After a successful return from DSKT2_deactivateAlg(), the algorithm's processing or control functions cannot be called to process data.
Object's deactivation logic involves calling the algorithm's IALG interface function algDeactivate to save necessary data from the algorithm instance's scratch buffers to its persistent data memory.
DSKT2_deactivateAlg() must be called after the last processing or control methods of the algorithm instance, alg, during each execute stage of its socket operation.
DSKT2 maintains state information about current "active" algorithm instances at run-time, so that it does not perform unnecessary IALG "deactivation" calls. As part of this optimization it may defer the deactivation of this algorithm instance (alg) to a later stage, i.e. when DSKT2_activateAlg() is called to activate another algorithm instance.
- Parameters:
-
[in] | scratchMutexId | scratch-group Id used for determining the shared scratch memory. |
[in] | alg | IALG_Handle of the algorithm instance to be deactivated. |
- Return values:
-
- Precondition:
- alg must be a valid handle for the algorithm's instance object returned by an earlier call to DSKT2_createAlg()
-
No other algorithm method is currently being run on this instance. This method never preempts any other method on the same instance.
-
DSKT2_activateAlg() must be called before calling this method
- Note:
- The implementation of the IALG algDeactivate is optional by XDAIS standard. So, the instance deactivation makes sense only when the method is implemented by the algorithm. DSKT2_deactivateAlg() makes proper checks to ensure correct operation even if the algorithm does not implement the algDeactivate methods.
- See also:
- DSKT2_activateAlg()