This structure defines the codec parameters that can be modified after creation via control() calls. More...
#include <ividdec2.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | decodeHeader |
XDAS_Int32 | displayWidth |
XDAS_Int32 | frameSkipMode |
XDAS_Int32 | frameOrder |
XDAS_Int32 | newFrameFlag |
XDAS_Int32 | mbDataFlag |
This structure defines the codec parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Decode entire access unit or only header.
Pitch. If set to zero, use the decoded image width. Else, use given display width in pixels.
Video frame skip features for video decoder.
Video decoder output frame order.
Flag to indicate that the algorithm should start a new frame.
Flag to indicate that the algorithm should generate MB Data in addition to decoding the data.