Defines the run time output arguments for all ISPHENC instance objects. More...
#include <isphenc.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | rate |
XDAS_Int32 | frameType |
XDAS_Int32 | outbufferSize |
Defines the run time output arguments for all ISPHENC instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Current frame bit rate.
Current frame type.
Output buffer size in bytes.