Defines the creation time parameters for all ISPHDEC instance objects. More...
#include <isphdec.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | dataEnable |
XDAS_Int32 | compandingLaw |
XDAS_Int32 | packingType |
Defines the creation time parameters for all ISPHDEC instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
TTY/DTMF enabled flag. Set to 1 to enable, 0 to disable.
Companding Law.
Packing Format Option (for codecs that support multiple packing formats - used for selection, 0, 1, 2...)