This structure defines the codec parameters that can be modified after creation via ISPHDEC1_Fxns.control(). More...
#include <isphdec1.h>
Data Fields | |
XDAS_Int16 | size |
XDAS_Int16 | postFilter |
This structure defines the codec parameters that can be modified after creation via ISPHDEC1_Fxns.control().
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Assign the postFilter setting.