Data Structures | |
struct | IVIDENC2_CodecClassConfig |
Definition of IVIDENC2 codec class configurable parameters. More... | |
Defines | |
#define | VIDENC2_EOK IVIDENC2_EOK |
#define | VIDENC2_EFAIL IVIDENC2_EFAIL |
#define | VIDENC2_EUNSUPPORTED IVIDENC2_EUNSUPPORTED |
#define | VIDENC2_ETIMEOUT VISA_ETIMEOUT |
#define | VIDENC2_FOREVER VISA_FOREVER |
#define | VIDENC2_VISATYPE "ti.sdo.ce.video2.IVIDENC2" |
The VISA type. | |
#define | VIDENC2_STUBSNAME "VIDENC2_STUBS" |
Name of stub functions. Use this name when registering the VIDENC2_STUBS functions with Engine_addStubFxns. | |
Typedefs | |
typedef VISA_Handle | VIDENC2_Handle |
Opaque handle to a VIDENC2 codec. | |
typedef struct IVIDENC2_Params | VIDENC2_Params |
typedef IVIDENC2_InArgs | VIDENC2_InArgs |
typedef IVIDENC2_OutArgs | VIDENC2_OutArgs |
typedef IVIDENC2_Cmd | VIDENC2_Cmd |
typedef IVIDENC2_DynamicParams | VIDENC2_DynamicParams |
typedef IVIDENC2_Status | VIDENC2_Status |
typedef struct IVIDENC2_CodecClassConfig | IVIDENC2_CodecClassConfig |
Definition of IVIDENC2 codec class configurable parameters. | |
Functions | |
Int32 | VIDENC2_control (VIDENC2_Handle handle, VIDENC2_Cmd id, VIDENC2_DynamicParams *params, VIDENC2_Status *status) |
Execute the control() method in this instance of a video encoder algorithm. | |
VIDENC2_Handle | VIDENC2_create (Engine_Handle e, String name, VIDENC2_Params *params) |
Create an instance of a video encoder algorithm. | |
Void | VIDENC2_delete (VIDENC2_Handle handle) |
Delete the instance of a video encoder algorithm. | |
Int32 | VIDENC2_process (VIDENC2_Handle handle, IVIDEO2_BufDesc *inBufs, XDM2_BufDesc *outBufs, VIDENC2_InArgs *inArgs, VIDENC2_OutArgs *outArgs) |
Execute the process() method in this instance of a video encoder algorithm. | |
XDAS_Int32 | VIDENC2_processAsync (VIDENC2_Handle handle, IVIDEO2_BufDesc *inBufs, XDM2_BufDesc *outBufs, IVIDENC2_InArgs *inArgs, IVIDENC2_OutArgs *outArgs) |
Perform asynchronous submission to this instance of a video decoder algorithm. | |
XDAS_Int32 | VIDENC2_processWait (VIDENC2_Handle handle, IVIDEO2_BufDesc *inBufs, XDM2_BufDesc *outBufs, IVIDENC2_InArgs *inArgs, IVIDENC2_OutArgs *outArgs, UInt timeout) |
Wait for a return message from a previous invocation of VIDENC2_processAsync() in this instance of an video decoder algorithm. |
This is the VIDENC2 video encoder interface. Several of the data types in this API are specified by the XDM IVIDENC2 interface; please see the XDM documentation for those details.
#define VIDENC2_EOK IVIDENC2_EOK |
Success.
#define VIDENC2_EFAIL IVIDENC2_EFAIL |
General failure.
#define VIDENC2_EUNSUPPORTED IVIDENC2_EUNSUPPORTED |
Request is unsupported.
#define VIDENC2_ETIMEOUT VISA_ETIMEOUT |
Timeout occurred.
#define VIDENC2_FOREVER VISA_FOREVER |
Special value for timeout parameter indicating never timeout.
#define VIDENC2_VISATYPE "ti.sdo.ce.video2.IVIDENC2" |
The VISA type.
#define VIDENC2_STUBSNAME "VIDENC2_STUBS" |
Name of stub functions. Use this name when registering the VIDENC2_STUBS functions with Engine_addStubFxns.
typedef VISA_Handle VIDENC2_Handle |
Opaque handle to a VIDENC2 codec.
typedef struct IVIDENC2_Params VIDENC2_Params |
Defines the creation time parameters for all IVIDENC2 instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details. typedef IVIDENC2_InArgs VIDENC2_InArgs |
Defines the input arguments for all IVIDENC2 instance process function.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.typedef IVIDENC2_OutArgs VIDENC2_OutArgs |
Defines the run time output arguments for all IVIDENC2 instance objects.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.typedef IVIDENC2_Cmd VIDENC2_Cmd |
Defines the control commands for the IVIDENC2 module.
This structure defines the algorithm parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.typedef IVIDENC2_Status VIDENC2_Status |
Defines instance status parameters.
size
parameter. size
field must be correctly set by the caller. See https://processors.wiki.ti.com/index.php/Extending_data_structures_in_XDM for more details.typedef struct IVIDENC2_CodecClassConfig IVIDENC2_CodecClassConfig |
Definition of IVIDENC2 codec class configurable parameters.
Int32 VIDENC2_control | ( | VIDENC2_Handle | handle, |
VIDENC2_Cmd | id, | ||
VIDENC2_DynamicParams * | params, | ||
VIDENC2_Status * | status | ||
) |
Execute the control() method in this instance of a video encoder algorithm.
[in] | handle | Handle to a created video encoder instance. |
[in] | id | Command id for XDM control operation. |
[in] | params | Runtime control parameters used for encoding. |
[out] | status | Status info upon completion of encode operation. |
handle
is a valid (non-NULL) video encoder handle and the video encoder is in the created state.VIDENC2_EOK | Success. |
VIDENC2_EFAIL | Failure. |
VIDENC2_EUNSUPPORTED | The requested operation is not supported. |
status->extendedError
may indicate further details about the error. See VIDENC2_Status::extendedError for details.VIDENC2_Handle VIDENC2_create | ( | Engine_Handle | e, |
String | name, | ||
VIDENC2_Params * | params | ||
) |
Create an instance of a video encoder algorithm.
Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via VIDENC2_create()) or explicitly serialize access to a shared handle.
[in] | e | Handle to an opened engine. |
[in] | name | String identifier of the type of video encoder to create. |
[in] | params | Creation parameters. |
NULL | An error has occurred. |
non-NULL | The handle to the newly created video encoder instance. |
params
is optional. If it's not supplied, codec-specific default params will be used.name
is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated, to be overridden. This optional argument string is of the form ":priority", ":priority:flag", or "::flag". IALG_EXTERNAL
. If flag is 0, the memory for the codec will be allocated from the heaps it has requested. For example, if a codec named "mp3" has been configured into the system, setting name to "mp3:4" would cause the codec to be created at priority 4, instead of whatever priority was configured. This feature is useful if more than one instance of the codec are to be created at different priorities. Void VIDENC2_delete | ( | VIDENC2_Handle | handle ) |
Delete the instance of a video encoder algorithm.
[in] | handle | Handle to a created video encoder instance. |
handle
is a valid (non-NULL) handle which is in the created state.Int32 VIDENC2_process | ( | VIDENC2_Handle | handle, |
IVIDEO2_BufDesc * | inBufs, | ||
XDM2_BufDesc * | outBufs, | ||
VIDENC2_InArgs * | inArgs, | ||
VIDENC2_OutArgs * | outArgs | ||
) |
Execute the process() method in this instance of a video encoder algorithm.
[in] | handle | Handle to a created video encoder instance. |
[in] | inBufs | A buffer descriptor containing input buffers. |
[out] | outBufs | A buffer descriptor containing output buffers. |
[in] | inArgs | Input Arguments. |
[out] | outArgs | Output Arguments. |
handle
is a valid (non-NULL) video encoder handle and the video encoder is in the created state.VIDENC2_EOK | Success. |
VIDENC2_EFAIL | Failure. |
VIDENC2_EUNSUPPORTED | The requested operation is not supported. |
outArgs->extendedError
may indicate further details about the error. See VIDENC2_OutArgs::extendedError for details.XDAS_Int32 VIDENC2_processAsync | ( | VIDENC2_Handle | handle, |
IVIDEO2_BufDesc * | inBufs, | ||
XDM2_BufDesc * | outBufs, | ||
IVIDENC2_InArgs * | inArgs, | ||
IVIDENC2_OutArgs * | outArgs | ||
) |
Perform asynchronous submission to this instance of a video decoder algorithm.
[in] | handle | Handle to a created video decoder instance. |
[in] | inBufs | A buffer descriptor containing input buffers. |
[out] | outBufs | A buffer descriptor containing output buffers. |
[in] | inArgs | Input Arguments. |
[out] | outArgs | Output Arguments. |
handle
is a valid (non-NULL) video decoder handle and the video decoder is in the created state.VIDENC2_EOK | Success. |
VIDENC2_EFAIL | Failure. |
VIDENC2_EUNSUPPORTED | Unsupported request. |
XDAS_Int32 VIDENC2_processWait | ( | VIDENC2_Handle | handle, |
IVIDEO2_BufDesc * | inBufs, | ||
XDM2_BufDesc * | outBufs, | ||
IVIDENC2_InArgs * | inArgs, | ||
IVIDENC2_OutArgs * | outArgs, | ||
UInt | timeout | ||
) |
Wait for a return message from a previous invocation of VIDENC2_processAsync() in this instance of an video decoder algorithm.
[in] | handle | Handle to a created video decoder instance. |
[in] | inBufs | A buffer descriptor containing input buffers. |
[out] | outBufs | A buffer descriptor containing output buffers. |
[in] | inArgs | Input Arguments. |
[out] | outArgs | Output Arguments. |
[in] | timeout | Amount of "time" to wait (from 0 -> VIDENC2_FOREVER) |
handle
is a valid (non-NULL) video decoder handle and the video decoder is in the created state.VIDENC2_EOK | Success. |
VIDENC2_EFAIL | Failure. |
VIDENC2_EUNSUPPORTED | Unsupported request. |
VIDENC2_ETIMEOUT | Operation timed out. |