Data Structures | Typedefs

split/ividdec2.h File Reference


Detailed Description

This header defines all types, constants, enums, and functions that are common across all split IVIDDEC2-based codecs.

#include <ti/xdais/ialg.h>
#include <ti/xdais/xdas.h>
#include "../xdm.h"
#include "../ividdec2.h"
Include dependency graph for split/ividdec2.h:
This graph shows which files directly or indirectly include this file:

Go to the source code of this file.

Data Structures

struct  IVIDDEC2FRONT_Obj
 This must be the first field of all IVIDDEC2FRONT instance objects. More...
struct  IVIDDEC2BACK_Obj
 This must be the first field of all IVIDDEC2BACK instance objects. More...
struct  IVIDDEC2FRONT_Status
 Defines instance status parameters. More...
struct  IVIDDEC2FRONT_OutArgs
 Defines the run time output arguments for all IVIDDEC2FRONT instance objects. More...
struct  IVIDDEC2FRONT_Fxns
 Defines all of the operations on IVIDDEC2FRONT objects. More...
struct  IVIDDEC2BACK_Fxns
 Defines all of the operations on IVIDDEC2BACK objects. More...

Typedefs

typedef struct IVIDDEC2FRONT_Obj IVIDDEC2FRONT_Obj
 This must be the first field of all IVIDDEC2FRONT instance objects.
typedef struct IVIDDEC2FRONT_ObjIVIDDEC2FRONT_Handle
 Opaque handle to an IVIDDEC2FRONT objects.
typedef struct IVIDDEC2BACK_Obj IVIDDEC2BACK_Obj
 This must be the first field of all IVIDDEC2BACK instance objects.
typedef struct IVIDDEC2BACK_ObjIVIDDEC2BACK_Handle
 Opaque handle to an IVIDDEC2BACK objects.
typedef struct IVIDDEC2FRONT_Status IVIDDEC2FRONT_Status
 Defines instance status parameters.
typedef struct
IVIDDEC2FRONT_OutArgs 
IVIDDEC2FRONT_OutArgs
 Defines the run time output arguments for all IVIDDEC2FRONT instance objects.
typedef struct IVIDDEC2FRONT_Fxns IVIDDEC2FRONT_Fxns
 Defines all of the operations on IVIDDEC2FRONT objects.
typedef struct IVIDDEC2BACK_Fxns IVIDDEC2BACK_Fxns
 Defines all of the operations on IVIDDEC2BACK objects.
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2012, Texas Instruments Incorporated