![]() |
![]() |
This structure defines the algorithm parameters that can be modified after creation via control() calls. More...
#include <ividenc2.h>
This structure defines the algorithm parameters that can be modified after creation via control() calls.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Input frame height.
Input frame width.
Reference, or input, frame rate in fps * 1000.
Target frame rate in fps * 1000.
Target bit rate in bits per second.
The number of frames between two I frames. For example, 30.
Encode entire access unit or only header.
DEFAULT(0): use imagewidth as pitch else use given capture width for pitch provided it is greater than image width.
Force the current (immediate) frame to be encoded as a specific frame type.
Number of B frames between two reference frames; that is, the number of B frames between two P frames or I/P frames. DEFAULT(0).
Pixel Accuracy of the motion vector
Sample aspect ratio: Height
Sample aspect ratio: Width
Flag to indicate that the application has ignored the output buffer size requirement.
ignoreOutbufSizeFlag
field to XDAS_TRUE. When this flag is set to XDAS_TRUE, the encoder shouldn't return an error even if the output buffer size is less than requested by the codec.Optional datasync "put data" function.
Datasync "put data" handle
Datasync "get data" function.
Datasync "get data" handle
getDataFxn
.Datasync "get buffer" function.
Datasync "get buffer" handle
Argument used during late acquire.
lateAcquireArg
value when requesting resources (i.e. during their call to acquire() when requesting the resource).