Data Structures | Defines | Typedefs | Functions

VIDDEC - Video Decoder Interface

Data Structures

struct  IVIDDEC_CodecClassConfig
 Definition of VIDDEC codec class configurable parameters. More...

Defines

#define VIDDEC_EOK   IVIDDEC_EOK
#define VIDDEC_EFAIL   IVIDDEC_EFAIL
#define VIDDEC_ERUNTIME   IVIDDEC_ERUNTIME
#define VIDDEC_ETIMEOUT   VISA_ETIMEOUT
#define VIDDEC_FOREVER   VISA_FOREVER
#define VIDDEC_VISATYPE   "ti.sdo.ce.video.IVIDDEC"
 The VISA type.

Typedefs

typedef IVIDDEC_Status VIDDEC_Status
typedef VISA_Handle VIDDEC_Handle
 Opaque handle to a VIDDEC codec.
typedef struct IVIDDEC_Params VIDDEC_Params
 This structure defines the parameters necessary to create an instance of a video decoder object.
typedef IVIDDEC_InArgs VIDDEC_InArgs
typedef IVIDDEC_OutArgs VIDDEC_OutArgs
typedef IVIDDEC_Cmd VIDDEC_Cmd
typedef IVIDDEC_DynamicParams VIDDEC_DynamicParams
typedef struct
IVIDDEC_CodecClassConfig 
IVIDDEC_CodecClassConfig
 Definition of VIDDEC codec class configurable parameters.

Functions

VIDDEC_Handle VIDDEC_create (Engine_Handle e, String name, VIDDEC_Params *params)
 Create an instance of a video decoder algorithm.
Int32 VIDDEC_process (VIDDEC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, VIDDEC_InArgs *inArgs, VIDDEC_OutArgs *outArgs)
 Execute the process() method in this instance of a video decoder algorithm.
Int32 VIDDEC_control (VIDDEC_Handle handle, VIDDEC_Cmd id, VIDDEC_DynamicParams *params, VIDDEC_Status *status)
 Execute the "control" method in this instance of a video decoder algorithm.
Void VIDDEC_delete (VIDDEC_Handle handle)
 Delete the instance of a video decoder algorithm.
XDAS_Int32 VIDDEC_processAsync (VIDDEC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, VIDDEC_InArgs *inArgs, VIDDEC_OutArgs *outArgs)
 Perform asynchronous submission to this instance of a video decoder algorithm.
XDAS_Int32 VIDDEC_processWait (VIDDEC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, VIDDEC_InArgs *inArgs, VIDDEC_OutArgs *outArgs, UInt timeout)
 Wait for a return message from a previous invocation of VIDDEC_processAsync() in this instance of an video decoder algorithm.

Detailed Description

This is the VIDDEC video decoder interface. Several of the data types in this API are specified by the XDM interface; please see the XDM documentation for those details.


Define Documentation

#define VIDDEC_EOK   IVIDDEC_EOK

Success.

#define VIDDEC_EFAIL   IVIDDEC_EFAIL

General failure.

#define VIDDEC_ERUNTIME   IVIDDEC_ERUNTIME

General runtime failure.

#define VIDDEC_ETIMEOUT   VISA_ETIMEOUT

Timeout occurred.

#define VIDDEC_FOREVER   VISA_FOREVER

Special value for timeout parameter indicating never timeout.

#define VIDDEC_VISATYPE   "ti.sdo.ce.video.IVIDDEC"

The VISA type.


Typedef Documentation

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC_Fxns::control()

Opaque handle to a VIDDEC codec.

typedef struct IVIDDEC_Params VIDDEC_Params

This structure defines the parameters necessary to create an instance of a video decoder object.

Defines the input arguments for all IVIDDEC instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC_Fxns::process()

Defines the run time output arguments for all IVIDDEC instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC_Fxns::process()

Defines the control commands for the IVIDDEC module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IVIDDEC_Fxns::control()

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC_Fxns::control()

Definition of VIDDEC codec class configurable parameters.

See also:
VISA_getCodecClassConfig()

Function Documentation

VIDDEC_Handle VIDDEC_create ( Engine_Handle  e,
String  name,
VIDDEC_Params params 
)

Create an instance of a video decoder algorithm.

Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via VIDDEC_create()) or explicitly serialize access to a shared handle.

Parameters:
[in]eHandle to an opened engine.
[in]nameString identifier of the type of video decoder. to create.
[in]paramsCreation parameters.
Return values:
NULLAn error has occurred.
non-NULLThe handle to the newly created video decoder instance.
Remarks:
params is optional. If it's not supplied, codec-specific default params will be used.
Depending on the configuration of the engine opened, this call may create a local or remote instance of the video decoder.
In general, name is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated, to be overridden. This optional argument string is of the form ":priority", ":priority:flag", or "::flag".
priority is the new priority to create the codec with.
The flag must be either 0 or 1, and if 1, all memory allocated for the codec will be in the heap that corresponds to IALG_EXTERNAL. If flag is 0, the memory for the codec will be allocated from the heaps it has requested. For example, if a codec named "mp3" has been configured into the system, setting name to "mp3:4" would cause the codec to be created at priority 4, instead of whatever priority was configured. This feature is useful if more than one instance of the codec are to be created at different priorities.
The flag can be used to prevent the codec from using any internal memory, for example, if it is to be run at the same time as another codec that must use internal memory, and there is insufficient internal memory for both.
See also:
Engine_open()
VIDDEC_delete()
Int32 VIDDEC_process ( VIDDEC_Handle  handle,
XDM_BufDesc inBufs,
XDM_BufDesc outBufs,
VIDDEC_InArgs inArgs,
VIDDEC_OutArgs outArgs 
)

Execute the process() method in this instance of a video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
[in]inBufsA buffer descriptor containing input buffers.
[out]outBufsA buffer descriptor containing output buffers.
[in]inArgsInput Arguments.
[out]outArgsOutput Arguments.
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC_EOKSuccess.
VIDDEC_EFAILFailure.
VIDDEC_ERUNTIMEInternal Runtime Error.
Remarks:
Since the VIDDEC decoder contains support for asynchronous buffer submission and retrieval, this API becomes known as synchronous in nature.
This is a blocking call, and will return after the data has been decoded.
The buffers supplied to VIDDEC_process() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDDEC_create()
VIDDEC_delete()
VIDDEC_control()
VIDDEC_processAsync()
VIDDEC_processWait()
IVIDDEC_Fxns::process()
Int32 VIDDEC_control ( VIDDEC_Handle  handle,
VIDDEC_Cmd  id,
VIDDEC_DynamicParams params,
VIDDEC_Status status 
)

Execute the "control" method in this instance of a video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
[in]idCommand id for XDM control operation.
[in]paramsRuntime control parameters used for decoding.
[out]statusStatus info upon completion of decode operation.
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC_EOKSuccess.
VIDDEC_EFAILFailure.
VIDDEC_ERUNTIMEInternal Runtime Error.
Remarks:
This is a blocking call, and will return after the control command has been executed.
See also:
VIDDEC_create()
VIDDEC_delete()
IVIDDEC_Fxns::control()
Void VIDDEC_delete ( VIDDEC_Handle  handle )

Delete the instance of a video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
Remarks:
Depending on the configuration of the engine opened, this call may delete a local or remote instance of the video decoder.
Precondition:
handle is a valid (non-NULL) handle which is in the created state.
Postcondition:
All resources allocated as part of the VIDDEC_create() operation (memory, DMA channels, etc.) are freed.
See also:
VIDDEC_create()
XDAS_Int32 VIDDEC_processAsync ( VIDDEC_Handle  handle,
XDM_BufDesc inBufs,
XDM_BufDesc outBufs,
VIDDEC_InArgs inArgs,
VIDDEC_OutArgs outArgs 
)

Perform asynchronous submission to this instance of a video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
[in]inBufsA buffer descriptor containing input buffers.
[out]outBufsA buffer descriptor containing output buffers.
[in]inArgsInput Arguments.
[out]outArgsOutput Arguments.
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC_EOKSuccess.
VIDDEC_EFAILFailure.
VIDDEC_ERUNTIMEInternal Runtime Error.
Remarks:
This API is the asynchronous counterpart to the process() method. It allows for buffer and argument submission without waiting for retrieval. A response is retrieved using the VIDDEC_processWait() API.
The buffers supplied to VIDDEC_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDDEC_create()
VIDDEC_delete()
VIDDEC_control()
VIDDEC_process()
VIDDEC_processWait()
IVIDDEC_Fxns::process()
XDAS_Int32 VIDDEC_processWait ( VIDDEC_Handle  handle,
XDM_BufDesc inBufs,
XDM_BufDesc outBufs,
VIDDEC_InArgs inArgs,
VIDDEC_OutArgs outArgs,
UInt  timeout 
)

Wait for a return message from a previous invocation of VIDDEC_processAsync() in this instance of an video decoder algorithm.

Parameters:
[in]handleHandle to a created video decoder instance.
[in]inBufsA buffer descriptor containing input buffers.
[out]outBufsA buffer descriptor containing output buffers.
[in]inArgsInput Arguments.
[out]outArgsOutput Arguments.
[in]timeoutAmount of "time" to wait (from 0 -> VIDDEC_FOREVER)
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC_EOKSuccess.
VIDDEC_EFAILFailure.
VIDDEC_ERUNTIMEInternal Runtime Error.
VIDDEC_ETIMEOUTOperation timed out.
Remarks:
This is a blocking call, and will return after the data has been decoded.
"Polling" is supported by using a timeout of 0. Waiting forever is supported by using a timeout of VIDDEC_EFOREVER.
There must have previously been an invocation of the VIDDEC_processAsync() API.
The buffers supplied to VIDDEC_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDDEC_create()
VIDDEC_delete()
VIDDEC_control()
VIDDEC_process()
VIDDEC_processAsync()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated