Defines | Typedefs | Functions

VIDANALYTICS - Video Analytics Interface

Defines

#define VIDANALYTICS_EOK   IVIDANALYTICS_EOK
#define VIDANALYTICS_EFAIL   IVIDANALYTICS_EFAIL
#define VIDANALYTICS_EUNSUPPORTED   IVIDANALYTICS_EUNSUPPORTED
#define VIDANALYTICS_ETIMEOUT   VISA_ETIMEOUT
#define VIDANALYTICS_FOREVER   VISA_FOREVER
#define VIDANALYTICS_VISATYPE   "ti.sdo.ce.vidanalytics.IVIDANALYTICS"
 The VISA type.

Typedefs

typedef VISA_Handle VIDANALYTICS_Handle
 Opaque handle to a VIDANALYTICS codec.
typedef IVIDANALYTICS_Params VIDANALYTICS_Params
typedef IVIDANALYTICS_InArgs VIDANALYTICS_InArgs
typedef IVIDANALYTICS_OutArgs VIDANALYTICS_OutArgs
typedef IVIDANALYTICS_Cmd VIDANALYTICS_Cmd
typedef IVIDANALYTICS_DynamicParams VIDANALYTICS_DynamicParams
typedef IVIDANALYTICS_Status VIDANALYTICS_Status

Functions

Int32 VIDANALYTICS_control (VIDANALYTICS_Handle handle, VIDANALYTICS_Cmd id, VIDANALYTICS_DynamicParams *params, VIDANALYTICS_Status *status)
 Execute the control() method in this instance of a video analytics algorithm.
VIDANALYTICS_Handle VIDANALYTICS_create (Engine_Handle e, String name, VIDANALYTICS_Params *params)
 Create an instance of a video analytics algorithm.
Void VIDANALYTICS_delete (VIDANALYTICS_Handle handle)
 Delete the instance of a video analytics algorithm.
Int32 VIDANALYTICS_process (VIDANALYTICS_Handle handle, XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs, VIDANALYTICS_InArgs *inArgs, VIDANALYTICS_OutArgs *outArgs)
 Execute the process() method in this instance of a video analytics algorithm.
XDAS_Int32 VIDANALYTICS_processAsync (VIDANALYTICS_Handle handle, XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs, IVIDANALYTICS_InArgs *inArgs, IVIDANALYTICS_OutArgs *outArgs)
 Perform asynchronous submission to this instance of a video analytics algorithm.
XDAS_Int32 VIDANALYTICS_processWait (VIDANALYTICS_Handle handle, XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs, IVIDANALYTICS_InArgs *inArgs, IVIDANALYTICS_OutArgs *outArgs, UInt timeout)
 Wait for a return message from a previous invocation of VIDANALYTICS_processAsync() in this instance of an video analytics algorithm.

Detailed Description

This is the VIDANALYTICS video analytics interface. Several of the data types in this API are specified by the XDM IVIDANALYTICS interface; please see the XDM documentation for those details.


Define Documentation

#define VIDANALYTICS_EOK   IVIDANALYTICS_EOK

Success.

#define VIDANALYTICS_EFAIL   IVIDANALYTICS_EFAIL

General failure.

#define VIDANALYTICS_EUNSUPPORTED   IVIDANALYTICS_EUNSUPPORTED

Request is unsupported.

#define VIDANALYTICS_ETIMEOUT   VISA_ETIMEOUT

Timeout occurred.

#define VIDANALYTICS_FOREVER   VISA_FOREVER

Special value for timeout parameter indicating never timeout.

#define VIDANALYTICS_VISATYPE   "ti.sdo.ce.vidanalytics.IVIDANALYTICS"

The VISA type.


Typedef Documentation

Opaque handle to a VIDANALYTICS codec.

Defines the creation time parameters for all IVIDANALYTICS instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

Defines the input arguments for all IVIDANALYTICS instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDANALYTICS_Fxns::process()

Defines the run time output arguments for all IVIDANALYTICS instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC1_Fxns::process()

Defines the control commands for the IVIDANALYTICS module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IVIDANALYTICS_Fxns::control()

This structure defines the algorithm parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDANALYTICS_Fxns::control()

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDANALYTICS_Fxns::control()

Function Documentation

Int32 VIDANALYTICS_control ( VIDANALYTICS_Handle  handle,
VIDANALYTICS_Cmd  id,
VIDANALYTICS_DynamicParams params,
VIDANALYTICS_Status status 
)

Execute the control() method in this instance of a video analytics algorithm.

Parameters:
[in]handleHandle to a created video analytics instance.
[in]idCommand id for XDM control operation.
[in]paramsRuntime control parameters used for the video analytics instance.
[out]statusStatus info returned by the video analytics instance.
Precondition:
handle is a valid (non-NULL) video analytics handle and the video analytics instance is in the created state.
Return values:
VIDANALYTICS_EOKSuccess.
VIDANALYTICS_EFAILFailure.
VIDANALYTICS_EUNSUPPORTEDUnsupported request.
Remarks:
This is a blocking call, and will return after the control command has been executed.
See also:
VIDANALYTICS_create()
VIDANALYTICS_delete()
IVIDANALYTICS_Fxns::control()
VIDANALYTICS_Handle VIDANALYTICS_create ( Engine_Handle  e,
String  name,
VIDANALYTICS_Params params 
)

Create an instance of a video analytics algorithm.

Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via VIDANALYTICS_create()) or explicitly serialize access to a shared handle.

Parameters:
[in]eHandle to an opened engine.
[in]nameString identifier of the type of video analytics algorithm to create.
[in]paramsCreation parameters.
Return values:
NULLAn error has occurred.
non-NULLThe handle to the newly created video analytics instance.
Remarks:
params is optional. If it's not supplied, codec-specific default params will be used.
Depending on the configuration of the engine opened, this call may create a local or remote instance of the video analytics algorithm.
In general, name is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated, to be overridden. This optional argument string is of the form ":priority", ":priority:flag", or "::flag".
priority is the new priority to create the codec with.
The flag must be either 0 or 1, and if 1, all memory allocated for the codec will be in the heap that corresponds to IALG_EXTERNAL. If flag is 0, the memory for the codec will be allocated from the heaps it has requested. For example, if a codec named "mp3" has been configured into the system, setting name to "mp3:4" would cause the codec to be created at priority 4, instead of whatever priority was configured. This feature is useful if more than one instance of the codec are to be created at different priorities.
The flag can be used to prevent the codec from using any internal memory, for example, if it is to be run at the same time as another codec that must use internal memory, and there is insufficient internal memory for both.
See also:
Engine_open()
VIDANALYTICS_delete()
Void VIDANALYTICS_delete ( VIDANALYTICS_Handle  handle )

Delete the instance of a video analytics algorithm.

Parameters:
[in]handleHandle to a created video analytics instance.
Remarks:
Depending on the configuration of the engine opened, this call may delete a local or remote instance of the video analytics algorithm.
Precondition:
handle is a valid (non-NULL) handle which is in the created state.
Postcondition:
All resources allocated as part of the VIDANALYTICS_create() operation (memory, DMA channels, etc.) are freed.
See also:
VIDANALYTICS_create()
Int32 VIDANALYTICS_process ( VIDANALYTICS_Handle  handle,
XDM1_BufDesc inBufs,
XDM1_BufDesc outBufs,
VIDANALYTICS_InArgs inArgs,
VIDANALYTICS_OutArgs outArgs 
)

Execute the process() method in this instance of a video analytics algorithm.

Parameters:
[in]handleHandle to a created video analytics instance.
[in]inBufsA buffer descriptor containing input buffers.
[out]outBufsA buffer descriptor containing output buffers.
[in]inArgsInput Arguments.
[out]outArgsOutput Arguments.
Precondition:
handle is a valid (non-NULL) video analytics handle and the video analytics algorithm instance is in the created state.
Return values:
VIDANALYTICS_EOKSuccess.
VIDANALYTICS_EFAILFailure.
VIDANALYTICS_EUNSUPPORTEDUnsupported request.
Remarks:
Since the VIDANALYTICS algorithm contains support for asynchronous buffer submission and retrieval, this API becomes known as synchronous in nature.
This is a blocking call, and will return after the data has been encoded.
The buffers supplied to VIDANALYTICS_process() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDANALYTICS_create()
VIDANALYTICS_delete()
VIDANALYTICS_control()
VIDANALYTICS_processAsync()
VIDANALYTICS_processWait()
IVIDANALYTICS_Fxns::process()
XDAS_Int32 VIDANALYTICS_processAsync ( VIDANALYTICS_Handle  handle,
XDM1_BufDesc inBufs,
XDM1_BufDesc outBufs,
IVIDANALYTICS_InArgs inArgs,
IVIDANALYTICS_OutArgs outArgs 
)

Perform asynchronous submission to this instance of a video analytics algorithm.

Parameters:
[in]handleHandle to a created video analytics instance.
[in]inBufsA buffer descriptor containing input buffers.
[out]outBufsA buffer descriptor containing output buffers.
[in]inArgsInput Arguments.
[out]outArgsOutput Arguments.
Precondition:
handle is a valid (non-NULL) video analytics handle and the video analytics algorithm instance is in the created state.
Return values:
VIDANALYTICS_EOKSuccess.
VIDANALYTICS_EFAILFailure.
VIDANALYTICS_EUNSUPPORTEDUnsupported request.
Remarks:
This API is the asynchronous counterpart to the process() method. It allows for buffer and argument submission without waiting for retrieval. A response is retrieved using the VIDANALYTICS_processWait() API.
The buffers supplied to VIDANALYTICS_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDANALYTICS_create()
VIDANALYTICS_delete()
VIDANALYTICS_control()
VIDANALYTICS_process()
VIDANALYTICS_processWait()
IVIDANALYTICS_Fxns::process()
XDAS_Int32 VIDANALYTICS_processWait ( VIDANALYTICS_Handle  handle,
XDM1_BufDesc inBufs,
XDM1_BufDesc outBufs,
IVIDANALYTICS_InArgs inArgs,
IVIDANALYTICS_OutArgs outArgs,
UInt  timeout 
)

Wait for a return message from a previous invocation of VIDANALYTICS_processAsync() in this instance of an video analytics algorithm.

Parameters:
[in]handleHandle to a created video analytics instance.
[in]inBufsA buffer descriptor containing input buffers.
[out]outBufsA buffer descriptor containing output buffers.
[in]inArgsInput Arguments.
[out]outArgsOutput Arguments.
[in]timeoutAmount of "time" to wait (from 0 -> VIDANALYTICS_FOREVER)
Precondition:
handle is a valid (non-NULL) video analytics handle and the video analytics algorithm instance is in the created state.
Return values:
VIDANALYTICS_EOKSuccess.
VIDANALYTICS_EFAILFailure.
VIDANALYTICS_EUNSUPPORTEDUnsupported request.
VIDANALYTICS_ETIMEOUTOperation timed out.
Remarks:
This is a blocking call, and will return after the data has been decoded.
"Polling" is supported by using a timeout of 0. Waiting forever is supported by using a timeout of VIDANALYTICS_FOREVER.
There must have previously been an invocation of the VIDANALYTICS_processAsync() API.
The buffers supplied to VIDANALYTICS_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDANALYTICS_create()
VIDANALYTICS_delete()
VIDANALYTICS_control()
VIDANALYTICS_process()
VIDANALYTICS_processAsync()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated