Data Structures | Defines | Typedefs | Functions | Variables

Codec Engine Runtime

Data Structures

struct  Engine_Attrs
 Attributes of an Engine. More...
struct  Engine_AlgInfo
 Properties of an Engine algorithm. More...
struct  Engine_DllAlgDesc
 Discriptor for a dynamically loaded codec. A dynamic library for a codec must export a function that fills in a structure of this type. More...
struct  Engine_DllAlgParams
 This structure is passed to Engine_addAlg(), and contains parameters to create a dynamic codec with. More...

Defines

#define Engine_MODNAME   "ti.sdo.ce.Engine"
 Name to pass to Diags_setMask() to enable logging for Engine functions. For example, Diags_setMask(Engine_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect.
#define Engine_EOK   0
#define Engine_EEXIST   1
#define Engine_ENOMEM   2
#define Engine_EDSPLOAD   3
#define Engine_ENOCOMM   4
#define Engine_ENOSERVER   5
#define Engine_ECOMALLOC   6
#define Engine_ERUNTIME   7
#define Engine_ECODECCREATE   8
#define Engine_ECODECSTART   9
#define Engine_EINVAL   10
#define Engine_EBADSERVER   11
#define Engine_ENOTAVAIL   12
#define Engine_EWRONGSTATE   13
#define Engine_EINUSE   14
#define Engine_ENOTFOUND   15
#define Engine_ETIMEOUT   16
#define Engine_GETALGDESCFXN   "GetEngineAlgDesc"
 Name of function that a dynamically loaded codec must supply.

Typedefs

typedef struct Engine_Obj * Engine_Handle
 Opaque handle to an engine.
typedef Int Engine_Error
 Engine error code.
typedef struct Engine_Attrs Engine_Attrs
 Attributes of an Engine.
typedef struct Engine_AlgInfo Engine_AlgInfo
 Properties of an Engine algorithm.
typedef struct Engine_DllAlgDesc Engine_DllAlgDesc
 Discriptor for a dynamically loaded codec. A dynamic library for a codec must export a function that fills in a structure of this type.
typedef Int(* Engine_GetAlgDescFxn )(Engine_DllAlgDesc *dllAlgDesc)
 Prototype of function that must be supplied by a dynamic codec library to fill in a Engine_DllAlgDesc structure.
typedef struct Engine_DllAlgParams Engine_DllAlgParams
 This structure is passed to Engine_addAlg(), and contains parameters to create a dynamic codec with.

Functions

Void CERuntime_exit (Void)
 Exit the Codec Engine Runtime.
Void CERuntime_init (Void)
 Initialize the Codec Engine Runtime.
Engine_Error Engine_add (String engineName, String remoteName)
 Add an Engine to the database of engines that can be opened with Engine_open()
Engine_Error Engine_addAlg (Engine_Handle engine, String location, Engine_DllAlgParams *pAlgParams)
 Dynamically add an algorithm to an Engine instance.
Engine_Error Engine_removeAlg (Engine_Handle engine, String name)
 Dynamically remove an algorithm from an Engine instance.
Void Engine_close (Engine_Handle engine)
 Close an Engine.
Engine_Handle Engine_open (String name, Engine_Attrs *attrs, Engine_Error *ec)
 Open an Engine.
Int Engine_fwriteTrace (Engine_Handle engine, String prefix, FILE *out)
 Write Server's trace buffer to specifed file stream.
Engine_Error Engine_getAlgInfo (String name, Engine_AlgInfo *algInfo, Int index)
 Get details of an algorithm configured into an engine.
Int Engine_getCpuLoad (Engine_Handle engine)
 Get Server's cpu usage in percent.
Engine_Error Engine_getLastError (Engine_Handle engine)
 Get error code of the last failed operation.
String Engine_getName (Engine_Handle engine)
 Get the name of an opened engine.
Engine_Error Engine_getNumAlgs (String name, Int *numAlgs)
 Get the number of algorithms configured into an Engine.
Server_Handle Engine_getServer (Engine_Handle engine)
 Get handle to an Engine's Server.
UInt32 Engine_getUsedMem (Engine_Handle engine)
 Get Server's total memory usage.
Engine_Error Engine_remove (String engineName)
 Remove an engine from the list of engines that can be opened.
Int Engine_setTrace (Engine_Handle engine, String mask)
 Set Server's trace mask.

Variables

Engine_Attrs Engine_ATTRS
 Default engine attributes.

Define Documentation

#define Engine_MODNAME   "ti.sdo.ce.Engine"

Name to pass to Diags_setMask() to enable logging for Engine functions. For example, Diags_setMask(Engine_MODNAME"+EX1234567"); turns on all Log statements in this module. Diags_setMask() must be called after initialization to take effect.

#define Engine_EOK   0

Success.

#define Engine_EEXIST   1

Name does not exist.

#define Engine_ENOMEM   2

Unable to allocate memory.

#define Engine_EDSPLOAD   3

Unable to load the DSP.

#define Engine_ENOCOMM   4

Unable to create a comm connection to the DSP.

#define Engine_ENOSERVER   5

Unable to locate the server on the DSP.

#define Engine_ECOMALLOC   6

Unable to allocate communication buffer.

#define Engine_ERUNTIME   7

Internal engine runtime failure.

#define Engine_ECODECCREATE   8

Creation of the Codec failed.

#define Engine_ECODECSTART   9

Start of the Codec failed. For codecs which are implemented as a thread, this implies that the codec thread of execution failed to start.

#define Engine_EINVAL   10

Bad paramater passed to method.

#define Engine_EBADSERVER   11

Incompatible server specified.

#define Engine_ENOTAVAIL   12

Service not available.

#define Engine_EWRONGSTATE   13

Call can not be made at this time.

#define Engine_EINUSE   14

Call can't be made at this time because a required name/resource is in use.

#define Engine_ENOTFOUND   15

Entity was not found.

#define Engine_ETIMEOUT   16

Timeout-based operation timed out.

#define Engine_GETALGDESCFXN   "GetEngineAlgDesc"

Name of function that a dynamically loaded codec must supply.


Typedef Documentation

typedef struct Engine_Obj* Engine_Handle

Opaque handle to an engine.

typedef Int Engine_Error

Engine error code.

typedef struct Engine_Attrs Engine_Attrs

Attributes of an Engine.

See also:
Engine_open() and Engine_ATTRS.

Properties of an Engine algorithm.

See also:
Engine_getAlgInfo()

Discriptor for a dynamically loaded codec. A dynamic library for a codec must export a function that fills in a structure of this type.

See also:
Engine_GetAlgDescFxn
typedef Int(* Engine_GetAlgDescFxn)(Engine_DllAlgDesc *dllAlgDesc)

Prototype of function that must be supplied by a dynamic codec library to fill in a Engine_DllAlgDesc structure.

Remarks:
This function will be called by Engine_addAlg() to fill in the dynamic codec's descriptor.
See also:
Engine_DllAlgDesc

This structure is passed to Engine_addAlg(), and contains parameters to create a dynamic codec with.

See also:
Engine_addAlg().

Function Documentation

Void CERuntime_exit ( Void   )

Exit the Codec Engine Runtime.

Remarks:
This function finalizes the Codec Engine modules used in the current configuration.
See also:
CERuntime_init()
Void CERuntime_init ( Void   )

Initialize the Codec Engine Runtime.

Remarks:
This function must be called prior to using any Codec Engine APIs; it initializes all Codec Engine modules used in the the current configuration.
See also:
CERuntime_exit()
Engine_Error Engine_add ( String  engineName,
String  remoteName 
)

Add an Engine to the database of engines that can be opened with Engine_open()

Parameters:
[in]engineNameThe name of the engine to create. This must not be NULL.
[in]remoteNameThe name of the remote server to load (if any).
Return values:
Engine_EINVALBad parameter passed.
Engine_EINUSEAn engine with the given name already exists.
Engine_ENOMEMA memory allocation failed.
Engine_EOKSuccess.
Precondition:
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Postcondition:
If the return value is Engine_EOK, Engine_open() can be called with engineName.
See also:
Engine_remove()
Engine_Error Engine_addAlg ( Engine_Handle  engine,
String  location,
Engine_DllAlgParams pAlgParams 
)

Dynamically add an algorithm to an Engine instance.

Parameters:
[in]engineThe handle to an engine, previously acquired by a call to Engine_open().
[in]locationString identifying the location of the algorithm. Often this is a file name, but for systems without a file system, it may be a system-specific string identifier.
[in]pAlgParamsParameters describing the algorithm being added.
Precondition:
engine is a valid (non-NULL) engine handle which is in the open state.
Remarks:
This API is not yet supported.
If there is an existing algorithm in the engine already named name, an error will be returned.
Return values:
Engine_EOKSuccess.
Engine_EINUSEattrs.name is in use.
See also:
Engine_open()
Engine_removeAlg()
Engine_Error Engine_removeAlg ( Engine_Handle  engine,
String  name 
)

Dynamically remove an algorithm from an Engine instance.

Parameters:
[in]engineThe handle to an engine, previously acquired by a call to Engine_open().
[in]nameName of the algorithm to remove.
Remarks:
This API is not yet supported.
Return values:
Engine_EOKSuccess.
Engine_ENOTFOUNDname could not be found in engine.
See also:
Engine_open()
Engine_addAlg()
Void Engine_close ( Engine_Handle  engine )

Close an Engine.

Parameters:
[in]engineThe handle to an engine, previously acquired by a call to Engine_open().
Precondition:
engine must not be referenced by any algorithm instance objects; i.e., you must first delete all algorithm instances associated with engine before closing it.
engine is a valid (non-NULL) engine handle which is in the open state.
Engine_Handle Engine_open ( String  name,
Engine_Attrs attrs,
Engine_Error ec 
)

Open an Engine.

The handle returned may be used to create one or more instances of an algorithm contained in the specified Engine.

An Engine may be opened more than once; each open returns a unique handle that can be used to create algorithm instances or get status of the Engine.

Engine handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via Engine_open()) or explicitly serialize access to a shared handle.

Parameters:
[in]nameThe name of the engine to open. name is specified in the engine configuration.
[in]attrsAttributes for the open engine.
[out]ecOptional output error code
Return values:
NULLAn error has occurred.
non-NULLThe handle to the opened engine.
Precondition:
name is a non-NULL string.
name is a valid, pre-configured name of an engine.
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Postcondition:
If the return handle is NULL and ec is non-NULL, *ec is set to a non-zero value indicating the cause of the failure.
If ec is non-NULL, the Engine_Error value is set to one of the following values:
Int Engine_fwriteTrace ( Engine_Handle  engine,
String  prefix,
FILE *  out 
)

Write Server's trace buffer to specifed file stream.

Parameters:
[in]engineThe handle to the opened engine.
[in]prefixA string to prepend to each line output; this allows one to easily identify trace from the server from the application's trace, for example.
[in]outA open FILE stream used to output the Server's trace characters.
Return values:
Integernumber of characters copied to the specified FILE stream.
Precondition:
engine is a valid (non-NULL) engine handle and the engine is in the open state.
Postcondition:
In the event a negative value is returned, Engine_getLastError() will return one of the following values:
  • Engine_ERUNTIME Either an internal runtime error occured or the underlying server error occured.
  • Engine_EINUSE Server trace resource is already in use.
Engine_Error Engine_getAlgInfo ( String  name,
Engine_AlgInfo algInfo,
Int  index 
)

Get details of an algorithm configured into an engine.

Parameters:
[in]nameThe name of the engine. name is specified in the engine configuration.
[out]algInfoStructure to store algorithm details. The algInfoSize field of this structure must be set to sizeof(Engine_AlgInfo) by the application.
[out]indexThe index of the algorithm to get the information.
Return values:
Engine_EOKSuccess.
Engine_EEXISTThere is no engine with the given name.
Engine_ENOTFOUNDindex is greater than or equal to the total number of algorithms configured for the engine, or index < 0.
Engine_EINVALThe value of algInfoSize passed to this function does not match the CE library's sizeof(Engine_AlgInfo).
Precondition:
name is a non-NULL string.
algInfo is non-NULL.
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Postcondition:
If name is a valid engine name and 0 <= index < the total number of algorithms configured for the engine, then algInfo will contain the information for the engine's ith (i = index) algorithm.
See also:
Engine_getNumAlgs()
Int Engine_getCpuLoad ( Engine_Handle  engine )

Get Server's cpu usage in percent.

Deprecated:
This service has been replaced by Server_getCpuLoad() to better indicate that this API is not intended for obtaining the current processor's CPU load, rather it obtains the CPU load of a remote Server.
Parameters:
[in]engineThe handle to the opened engine.
Return values:
integerbetween 0-100 indicating percentage of time the Server is processing measured over a period of approximately 1 second. If the load is unavailable, a negative value is returned.
Precondition:
engine is a valid (non-NULL) engine handle and the engine is in the open state.
Postcondition:
In the event a negative value is returned, Engine_getLastError() will return one of the following values:
See also:
Server_getCpuLoad()
Engine_Error Engine_getLastError ( Engine_Handle  engine )

Get error code of the last failed operation.

Parameters:
[in]engineThe handle to the opened engine.
Return values:
errorcode (Engine_Error) of the last failed engine operation.
Precondition:
engine is a valid (non-NULL) engine handle and the engine is in the open state.
String Engine_getName ( Engine_Handle  engine )

Get the name of an opened engine.

Parameters:
[in]engineThe handle to the opened engine.
Return values:
NULLAn error has occurred.
non-NULLThe name of the opened engine.
Engine_Error Engine_getNumAlgs ( String  name,
Int *  numAlgs 
)

Get the number of algorithms configured into an Engine.

Parameters:
[in]nameThe name of the Engine. name is specified in the engine configuration.
[out]numAlgsThe number of algorithms that are configured in the given engine.
Return values:
Engine_EOKSuccess.
Engine_EEXISTThere is no engine with the given name.
Precondition:
name is a non-NULL string.
numAlgs is non-NULL.
As with all Codec Engine API's, CERuntime_init() must have previously been called.
Postcondition:
If name is a valid engine name, then numAlgs will contain the number of algorithms configured for the given engine.
See also:
Engine_getAlgs()
Server_Handle Engine_getServer ( Engine_Handle  engine )

Get handle to an Engine's Server.

This function returns the handle to an Engines server, that can be used with Server APIs to obtain information from and control the remote DSP server.

Parameters:
[in]engineThe handle to the opened engine.
Return values:
Handleto engine's server.
Precondition:
engine is a valid (non-NULL) engine handle and the engine is in the open state.
UInt32 Engine_getUsedMem ( Engine_Handle  engine )

Get Server's total memory usage.

Deprecated:
This service has been replaced by Server_getMemStat() to better indicate that this API is not intended for obtaining the current processor's memory statistics, rather it obtains the memory statistics of a remote Server. Also, Server_getMemStat() provides more granularity than Engine_getUsedMem().
Parameters:
[in]engineThe handle to the opened engine.
Return values:
Totalamount of used memory (in MAUs). If the amount is not available, 0 is returned and the reason can be retrieved via Engine_getLastError().
Precondition:
engine is a valid (non-NULL) engine handle and the engine is in the open state.
Postcondition:
in the event that 0 is returned, Engine_getLastError() will return one of the following values:
Engine_Error Engine_remove ( String  engineName )

Remove an engine from the list of engines that can be opened.

Parameters:
[in]engineNameThe name of the engine to be removed.
Precondition:
engineName is non-NULL.
Return values:
Engine_EINUSEThe engine cannot be removed because an instance of it is still opened.
Engine_EEXISTNo engine by this name exists.
Engine_EOKSuccess.
See also:
Engine_add()
Int Engine_setTrace ( Engine_Handle  engine,
String  mask 
)

Set Server's trace mask.

Parameters:
[in]engineThe handle to the opened engine.
[in]maskTrace mask, e.g. "*=01234567"
Return values:
Engine_ENOSERVERNo server for this engine.
Engine_EINUSETrace resource is already in use.
Engine_ERUNTIMEInternal runtime error has occurred.
Precondition:
engine is a valid (non-NULL) engine handle and the engine is in the open state.
Remarks:
This only sets the trace for a remote server. To change the trace mask for the application-side of the framework, use Diags_setMask(), or Diags_setMaskMeta().
See also:
xdc.runtime.Diags

Variable Documentation

Default engine attributes.

Default attrs.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2011, Texas Instruments Incorporated