![]() |
![]() |
Defines the run time output arguments for all IVIDANALYTICS instance objects. More...
#include <ividanalytics.h>
Data Fields | |
XDAS_Int32 | size |
XDAS_Int32 | numTargets |
XDM_Rect | targets [128] |
XDAS_Int32 | numEvents |
XDAS_Int32 | eventId [128] |
XDAS_Int32 | extendedError |
XDM_Date | date |
Defines the run time output arguments for all IVIDANALYTICS instance objects.
size
parameter. size
field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.
Number of targets detected
target locations.
numTargets
is zero, the values in this array are undefined. Number of events detected
Zero-terminated array containing the ids of rules fired during the process() call.
numEvents
is zero, the values in this array are undefined. Extended error information.
Current time.