Data Fields

ISPHDEC1_DynamicParams Struct Reference
[ISPHDEC1 - XDM Speech Decoder Interface]

This structure defines the codec parameters that can be modified after creation via ISPHDEC1_Fxns.control(). More...

#include <isphdec1.h>

Data Fields

XDAS_Int16 size
XDAS_Int16 postFilter

Detailed Description

This structure defines the codec parameters that can be modified after creation via ISPHDEC1_Fxns.control().

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
ISPHDEC1_Fxns::control()

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

Assign the postFilter setting.

See also:
ISPEECH1_PostFilter
ISPHDEC1_Status.postFilter

The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated