Data Fields

Engine_DllAlgParams Struct Reference
[Codec Engine Runtime]

This structure is passed to Engine_addAlg(), and contains parameters to create a dynamic codec with. More...

#include <Engine.h>

Data Fields

String name
Bool isLocal
Int groupId

Detailed Description

This structure is passed to Engine_addAlg(), and contains parameters to create a dynamic codec with.

See also:
Engine_addAlg().

Field Documentation

Name of algorithm.

if TRUE, run locally.

Resource sharing group Id.


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated