Data Structures | Defines | Typedefs | Enumerations

ISPHENC1 - XDM Speech Encoder Interface

Data Structures

struct  ISPHENC1_Obj
 This must be the first field of all ISPHENC1 instance objects. More...
struct  ISPHENC1_Params
 Defines the creation time parameters for all ISPHENC1 instance objects. More...
struct  ISPHENC1_DynamicParams
 This structure defines the codec parameters that can be modified after creation via ISPHENC1_Fxns.control(). More...
struct  ISPHENC1_InArgs
 Defines the input arguments for all ISPHENC1 instance process function. More...
struct  ISPHENC1_Status
 Defines instance status parameters. More...
struct  ISPHENC1_OutArgs
 Defines the run time output arguments for all ISPHENC1 instance objects. More...
struct  ISPHENC1_Fxns
 Defines all of the operations on ISPHENC1 objects. More...

Defines

#define ISPHENC1_EOK   XDM_EOK
#define ISPHENC1_EFAIL   XDM_EFAIL
#define ISPHENC1_EUNSUPPORTED   XDM_EUNSUPPORTED
#define ISPHENC1_ENOOUTPUT   1
 This value signifies no output being available at encoder, for example in the case of intermediate calls in 10msec frame size execution.

Typedefs

typedef struct ISPHENC1_Obj ISPHENC1_Obj
 This must be the first field of all ISPHENC1 instance objects.
typedef struct ISPHENC1_ObjISPHENC1_Handle
 Opaque handle to an ISPHENC1 objects.
typedef struct ISPHENC1_Params ISPHENC1_Params
 Defines the creation time parameters for all ISPHENC1 instance objects.
typedef struct
ISPHENC1_DynamicParams 
ISPHENC1_DynamicParams
 This structure defines the codec parameters that can be modified after creation via ISPHENC1_Fxns.control().
typedef struct ISPHENC1_InArgs ISPHENC1_InArgs
 Defines the input arguments for all ISPHENC1 instance process function.
typedef struct ISPHENC1_Status ISPHENC1_Status
 Defines instance status parameters.
typedef struct ISPHENC1_OutArgs ISPHENC1_OutArgs
 Defines the run time output arguments for all ISPHENC1 instance objects.
typedef IALG_Cmd ISPHENC1_Cmd
 Defines the control commands for the ISPHENC1 module.
typedef struct ISPHENC1_Fxns ISPHENC1_Fxns
 Defines all of the operations on ISPHENC1 objects.

Enumerations

enum  ISPHENC1_FrameType {
  ISPHENC1_FTYPE_SPEECH = 0,
  ISPHENC1_FTYPE_SIDFRAME = 1,
  ISPHENC1_FTYPE_NODATA = 2
}
 

Encoder frame types.

More...

Detailed Description

This is the XDM ISPHENC1 Speech Encoder Interface.


Define Documentation

#define ISPHENC1_EOK   XDM_EOK

Success.

#define ISPHENC1_EFAIL   XDM_EFAIL

General failure.

#define ISPHENC1_EUNSUPPORTED   XDM_EUNSUPPORTED

Request is unsupported.

#define ISPHENC1_ENOOUTPUT   1

This value signifies no output being available at encoder, for example in the case of intermediate calls in 10msec frame size execution.


Typedef Documentation

typedef struct ISPHENC1_Obj ISPHENC1_Obj

This must be the first field of all ISPHENC1 instance objects.

typedef struct ISPHENC1_Obj* ISPHENC1_Handle

Opaque handle to an ISPHENC1 objects.

Defines the creation time parameters for all ISPHENC1 instance objects.

Remarks:
Some of the fields in this structure are optional and depend on the class of speech encoder you're creating.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

This structure defines the codec parameters that can be modified after creation via ISPHENC1_Fxns.control().

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

Defines the input arguments for all ISPHENC1 instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

Defines the run time output arguments for all ISPHENC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
ISPHENC1_Fxns::process()

Defines the control commands for the ISPHENC1 module.

Remarks:
This ID can be extended in IMOD interface for additional control commands.
See also:
XDM_CmdId
ISPHENC1_Fxns::control()
typedef struct ISPHENC1_Fxns ISPHENC1_Fxns

Defines all of the operations on ISPHENC1 objects.


Enumeration Type Documentation

Encoder frame types.

Remarks:
This enumeration data type should not be used for storage, but rather only for its constant values.
Enumerator:
ISPHENC1_FTYPE_SPEECH 

Speech frame

ISPHENC1_FTYPE_SIDFRAME 

SID frames for codecs which support DTX.

ISPHENC1_FTYPE_NODATA 

Untransmitted frame for codecs which support DTX.

 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated