Video 1.0 decoder codec interface

Data Structures

struct  IVIDDEC1_CodecClassConfig
 Definition of IVIDDEC1 codec class configurable parameters. More...

Defines

#define VIDDEC1_EOK   IVIDDEC1_EOK
#define VIDDEC1_EFAIL   IVIDDEC1_EFAIL
#define VIDDEC1_EUNSUPPORTED   IVIDDEC1_EUNSUPPORTED
#define VIDDEC1_ETIMEOUT   VISA_ETIMEOUT
#define VIDDEC1_FOREVER   VISA_FOREVER

Typedefs

typedef IVIDDEC1_Status VIDDEC1_Status
typedef VISA_Handle VIDDEC1_Handle
 Opaque handle to a VIDDEC1 codec.
typedef struct IVIDDEC1_Params VIDDEC1_Params
 This structure defines the parameters necessary to create an instance of a Video Decoder object.
typedef IVIDDEC1_InArgs VIDDEC1_InArgs
typedef IVIDDEC1_OutArgs VIDDEC1_OutArgs
typedef IVIDDEC1_Cmd VIDDEC1_Cmd
typedef IVIDDEC1_DynamicParams VIDDEC1_DynamicParams

Functions

VIDDEC1_Handle VIDDEC1_create (Engine_Handle e, String name, VIDDEC1_Params *params)
 Create an instance of a video decoder algorithm.
Int32 VIDDEC1_process (VIDDEC1_Handle handle, XDM1_BufDesc *inBufs, XDM_BufDesc *outBufs, VIDDEC1_InArgs *inArgs, VIDDEC1_OutArgs *outArgs)
 Execute the process() method in this instance of a video decoder algorithm.
Int32 VIDDEC1_control (VIDDEC1_Handle handle, VIDDEC1_Cmd id, VIDDEC1_DynamicParams *params, VIDDEC1_Status *status)
 Execute the control() method in this instance of a video decoder algorithm.
Void VIDDEC1_delete (VIDDEC1_Handle handle)
 Delete the instance of a video decoder algorithm.
XDAS_Int32 VIDDEC1_processAsync (VIDDEC1_Handle handle, XDM1_BufDesc *inBufs, XDM_BufDesc *outBufs, VIDDEC1_InArgs *inArgs, VIDDEC1_OutArgs *outArgs)
 Perform asynchronous submission to this instance of a video decoder algorithm.
XDAS_Int32 VIDDEC1_processWait (VIDDEC1_Handle handle, XDM1_BufDesc *inBufs, XDM_BufDesc *outBufs, VIDDEC1_InArgs *inArgs, VIDDEC1_OutArgs *outArgs, UInt timeout)
 Wait for a return message from a previous invocation of VIDDEC1_processAsync() in this instance of an video decoder algorithm.

Detailed Description

This is the 1.0 video decoder codec interface. Several of the data types in this API are specified by the xDM 1.0 interface; please see the xDM documentation for those details.


Define Documentation

#define VIDDEC1_EOK   IVIDDEC1_EOK

Success.

#define VIDDEC1_EFAIL   IVIDDEC1_EFAIL

General failure. Request is unsupported.

#define VIDDEC1_EUNSUPPORTED   IVIDDEC1_EUNSUPPORTED
#define VIDDEC1_ETIMEOUT   VISA_ETIMEOUT

Timeout occurred.

#define VIDDEC1_FOREVER   VISA_FOREVER

Special value for timeout parameter indicating never timeout.


Typedef Documentation

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
All fields correspond to latest IVIDDEC1_Fxns::process() call on the particular instance of the decoder.
See also:
IVIDDEC1_Fxns::control()

Opaque handle to a VIDDEC1 codec.

This structure defines the parameters necessary to create an instance of a Video Decoder object.

Defines the input arguments for all IVIDDEC1 instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC1_Fxns::process()

Defines the run time output arguments for all IVIDDEC1 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC1_Fxns::process()

Defines the control commands for the IVIDDEC1 module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IVIDDEC1_Fxns::control()

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC1_Fxns::control()


Function Documentation

VIDDEC1_Handle VIDDEC1_create ( Engine_Handle  e,
String  name,
VIDDEC1_Params params 
)

Create an instance of a video decoder algorithm.

Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via VIDDEC1_create) or explicitly serialize access to a shared handle.

Parameters:
[in] e Handle to an opened engine.
[in] name String identifier of the type of video decoder to create.
[in] params Creation parameters.
Return values:
NULL An error has occurred.
non-NULL The handle to the newly created video decoder instance.
Remarks:
Depending on the configuration of the engine opened, this call may create a local or remote instance of the video decoder.
In general, name is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated and/or the number of VISA messages to allocate, to be overridden. This optional argument string is of the form ":priority:flag:number-of-messages", and can be specified with an empty field for any element that you don't want to be overridden, e.g. "mp3:::3" to cause 3 messages to be allocated while using the default values for priority and the heap flag.
priority is the new priority to create the codec with.
The flag must be either 0 or 1, and if 1, all memory allocated for the codec will be in the heap that corresponds to IALG_EXTERNAL. If flag is 0, the memory for the codec will be allocated from the heaps it has requested. For example, if a codec named "mp3" has been configured into the system, setting name to "mp3:4" would cause the codec to be created at priority 4, instead of whatever priority was configured. This feature is useful if more than one instance of the codec are to be created at different priorities.
The flag can be used to prevent the codec from using any internal memory, for example, if it is to be run at the same time as another codec that must use internal memory, and there is insufficient internal memory for both.
The number-of-messages overrides the default of 1 message, and is useful (or required, practically speaking) for when the "asynchronous" process method is used, i.e. "AUDENC1_processAsync()"
See also:
Engine_open()
Int32 VIDDEC1_process ( VIDDEC1_Handle  handle,
XDM1_BufDesc inBufs,
XDM_BufDesc outBufs,
VIDDEC1_InArgs inArgs,
VIDDEC1_OutArgs outArgs 
)

Execute the process() method in this instance of a video decoder algorithm.

Parameters:
[in] handle Handle to a created video decoder instance.
[in] inBufs A buffer describer containing input buffers.
[out] outBufs A buffer describer containing output buffers.
[in] inArgs Input Arguments.
[out] outArgs Output Arguments.
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC1_EOK Success.
VIDDEC1_EFAIL Failure.
Remarks:
Since the VIDDEC1 decoder contains support for asynchronous buffer submission and retrieval, this API becomes known as synchronous in nature.
This is a blocking call, and will return after the data has been decoded.
The buffers supplied to VIDDEC1_process() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDDEC1_create()
VIDDEC1_delete()
VIDDEC1_control()
VIDDEC1_processAsync()
VIDDEC1_processWait()
IVIDDEC1_Fxns::process()
Int32 VIDDEC1_control ( VIDDEC1_Handle  handle,
VIDDEC1_Cmd  id,
VIDDEC1_DynamicParams params,
VIDDEC1_Status status 
)

Execute the control() method in this instance of a video decoder algorithm.

Parameters:
[in] handle Handle to a created video decoder instance.
[in] id Command id for xDM control operation.
[in] params Runtime control parameters used for decoding.
[out] status Status info upon completion of decode operation.
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC1_EOK Success.
VIDDEC1_EFAIL Failure.
Remarks:
This is a blocking call, and will return after the control command has been executed.
See also:
VIDDEC1_create()
VIDDEC1_delete()
IVIDDEC1_Fxns::process()
Void VIDDEC1_delete ( VIDDEC1_Handle  handle  ) 

Delete the instance of a video decoder algorithm.

Parameters:
[in] handle Handle to a created video decoder instance.
Remarks:
Depending on the configuration of the engine opened, this call may delete a local or remote instance of the video decoder.
Precondition:
handle is a valid (non-NULL) handle which is in the created state.
Postcondition:
All resources allocated as part of the VIDDEC1_create() operation (memory, DMA channels, etc.) are freed.
See also:
VIDDEC1_create()
XDAS_Int32 VIDDEC1_processAsync ( VIDDEC1_Handle  handle,
XDM1_BufDesc inBufs,
XDM_BufDesc outBufs,
VIDDEC1_InArgs inArgs,
VIDDEC1_OutArgs outArgs 
)

Perform asynchronous submission to this instance of a video decoder algorithm.

Parameters:
[in] handle Handle to a created video decoder instance.
[in] inBufs A buffer descriptor containing input buffers.
[out] outBufs A buffer descriptor containing output buffers.
[in] inArgs Input Arguments.
[out] outArgs Output Arguments.
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC1_EOK Success.
VIDDEC1_EFAIL Failure.
VIDDEC1_EUNSUPPORTED Unsupported request.
Remarks:
This API is the asynchronous counterpart to the process() method. It allows for buffer and argument submission without waiting for retrieval. A response is retrieved using the VIDDEC1_processWait() API.
The buffers supplied to VIDDEC1_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDDEC1_create()
VIDDEC1_delete()
VIDDEC1_control()
VIDDEC1_process()
VIDDEC1_processWait()
IVIDDEC1_Fxns::process()
XDAS_Int32 VIDDEC1_processWait ( VIDDEC1_Handle  handle,
XDM1_BufDesc inBufs,
XDM_BufDesc outBufs,
VIDDEC1_InArgs inArgs,
VIDDEC1_OutArgs outArgs,
UInt  timeout 
)

Wait for a return message from a previous invocation of VIDDEC1_processAsync() in this instance of an video decoder algorithm.

Parameters:
[in] handle Handle to a created video decoder instance.
[in] inBufs A buffer descriptor containing input buffers.
[out] outBufs A buffer descriptor containing output buffers.
[in] inArgs Input Arguments.
[out] outArgs Output Arguments.
[in] timeout Amount of "time" to wait (from 0 -> VIDDEC1_FOREVER)
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC1_EOK Success.
VIDDEC1_EFAIL Failure.
VIDDEC1_EUNSUPPORTED Unsupported request.
VIDDEC1_ETIMEOUT Operation timed out.
Remarks:
This is a blocking call, and will return after the data has been decoded.
"Polling" is supported by using a timeout of 0. Waiting forever is supported by using a timeout of VIDDEC1_EFOREVER.
There must have previously been an invocation of the VIDDEC1_processAsync() API.
The buffers supplied to VIDDEC1_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDDEC1_create()
VIDDEC1_delete()
VIDDEC1_control()
VIDDEC1_process()
VIDDEC1_processAsync()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated