Codec Engine OSAL - Memory

Data Structures

struct  Memory_AllocParams
 Parameters for Memory_alloc() & Memory_free(). More...

Defines

#define Memory_DEFAULTALIGNMENT   ((UInt)(-1))
#define Memory_GTNAME   "OM"
#define Memory_CACHED   0x00000000
#define Memory_NONCACHED   0x00000001
#define Memory_CACHEDMASK   0x00000001

Enumerations

enum  Memory_type {
  Memory_MALLOC = 0,
  Memory_SEG = 1,
  Memory_CONTIGPOOL = 2,
  Memory_CONTIGHEAP = 3
}
 

Enum values for Memory_AllocParams.type.

More...

Functions

Ptr Memory_alloc (UInt size, Memory_AllocParams *params)
 General memory allocation.
Void Memory_cacheInv (Ptr addr, Int sizeInBytes)
 Invalidate a range of cache.
Void Memory_cacheWb (Ptr addr, Int sizeInBytes)
 Write back cache.
Void Memory_cacheWbInv (Ptr addr, Int sizeInBytes)
 Write back and invalidate cache.
Ptr Memory_contigAlloc (UInt size, UInt align)
 Allocate physically contiguous blocks of memory.
Bool Memory_contigFree (Ptr addr, UInt size)
 Free memory allocated by Memory_contigAlloc().
Bool Memory_free (Ptr addr, UInt size, Memory_AllocParams *params)
 Free memory allocated with Memory_alloc().
Void Memory_dumpKnownContigBufsList (Void)
 Dumps the list of all translated/registered bufs.
UInt32 Memory_getBufferPhysicalAddress (Ptr virtualAddress, Int sizeInBytes, Bool *isContiguous)
 Converts application virtual address to a physical address.
Int Memory_getHeapId (String name)
 Get the heap heap ID corresponding to a heap name. This number will be between 0 and the value returned by Memory_getNumHeaps(). The heap Id can be passed to Memory_redefine(), Memory_restoreHeap(), and Memory_segStat().
Int Memory_getNumHeaps ()
 Get the number of memory heaps.
Ptr Memory_getBufferVirtualAddress (UInt32 physicalAddress, Int sizeInBytes)
 Obtains the virtual address of a physically contiguous buffer.
Void Memory_registerContigBuf (UInt32 virtualAddress, UInt32 sizeInBytes, UInt32 physicalAddress)
 Register a physical buffer allocated without Memory_contigAlloc().
Void Memory_unregisterContigBuf (UInt32 virtualAddress, UInt32 sizeInBytes)
 Unregisters a physical buffer allocated without Memory_contigAlloc().

Variables

Memory_AllocParams Memory_DEFAULTPARAMS
 Default parameters for Memory_alloc() & Memory_free().

Define Documentation

#define Memory_DEFAULTALIGNMENT   ((UInt)(-1))
#define Memory_GTNAME   "OM"
#define Memory_CACHED   0x00000000

Cached allocation.

See also:
Memory_AllocParams.flags
#define Memory_NONCACHED   0x00000001

Non-cached allocation.

See also:
Memory_AllocParams.flags
#define Memory_CACHEDMASK   0x00000001

Mask to isolate cache flag.

See also:
Memory_AllocParams.flags

Enumeration Type Documentation

Enum values for Memory_AllocParams.type.

See also:
Memory_AllocParams
Enumerator:
Memory_MALLOC 

malloc()-based allocation

Memory_SEG 

DSP/BIOS segment-based allocation

Memory_CONTIGPOOL 

Contiguous, pool-based allocation

Memory_CONTIGHEAP 

Contiguous, heap-based allocation


Function Documentation

Ptr Memory_alloc ( UInt  size,
Memory_AllocParams params 
)

General memory allocation.

Parameters:
[in] size Number of bytes to allocate.
[in] params Parameters controlling the allocation.
Return values:
NULL The memory request failed.
non-NULL The pointer to a buffer containing the requested memory.
See also:
Memory_free()
Memory_contigAlloc()
Void Memory_cacheInv ( Ptr  addr,
Int  sizeInBytes 
)

Invalidate a range of cache.

Parameters:
[in] addr Address of the beginning of the buffer to invalidate.
[in] sizeInBytes Size of the buffer to invalidate.
Remarks:
In addition to application usage, this is often called by a skeleton implementor after it has received a shared memory buffer from another processor, and before it invokes an algorithm's interface which will operate on that shared memory buffer.
See also:
Memory_cacheWb()
Memory_cacheWbInv()
Void Memory_cacheWb ( Ptr  addr,
Int  sizeInBytes 
)

Write back cache.

Parameters:
[in] addr Address of the beginning of the buffer to writeback.
[in] sizeInBytes Size of the buffer to writeback.
See also:
Memory_cacheInv()
Memory_cacheWbInv()
Void Memory_cacheWbInv ( Ptr  addr,
Int  sizeInBytes 
)

Write back and invalidate cache.

Parameters:
[in] addr Address of the beginning of the buffer to writeback and invalidate.
[in] sizeInBytes Size of the buffer to writeback invalidate.
See also:
Memory_cacheInv()
Memory_cacheWb()
Ptr Memory_contigAlloc ( UInt  size,
UInt  align 
)

Allocate physically contiguous blocks of memory.

Deprecated:
This function has been superceded by Memory_alloc() and will be removed in a future release. Users are recommended to modify their applications to use the new, more flexible Memory_alloc() instead.
Parameters:
[in] size Size of the buffer to allocate.
[in] align Alignment of the buffer; must be divisible by a power of two.
Precondition:
align must be divisible by a power of two.
Return values:
non-NULL Address of a physically contiguous buffer.
NULL Unable to obtain the requested buffer.
Remarks:
This is commonly called by an application wishing to obtain a physically contiguous buffer which it must share with another processor.
For portability reasons, applications commonly use this API even in environments which do not have virtual memory or an MMU (e.g. a single processor, DSP/BIOS based system). Doing so makes them portable to environments which do have to provide physically contiguous memory to remote processors.
See also:
Memory_alloc()
Memory_contigFree()
Bool Memory_contigFree ( Ptr  addr,
UInt  size 
)

Free memory allocated by Memory_contigAlloc().

Parameters:
[in] addr Address of a buffer allocated by Memory_contigAlloc()
[in] size Size of the buffer to free.
Return values:
TRUE The buffer was freed and the memory pointed to by addr is no longer valid.
FALSE The buffer couldn't be freed.
Precondition:
addr must be a valid address returned by Memory_contigAlloc()
size must be equivalent to the size passed in during the Memory_contigAlloc() allocation.
See also:
Memory_contigAlloc()
Bool Memory_free ( Ptr  addr,
UInt  size,
Memory_AllocParams params 
)

Free memory allocated with Memory_alloc().

Parameters:
[in] addr Address of a buffer allocated by Memory_alloc().
[in] size Size of the buffer to free.
[in] params Parameters controlling the free operation.
Return values:
TRUE The buffer was freed and the memory pointed to by addr is no longer valid.
FALSE The buffer couldn't be freed.
Precondition:
addr must be a valid address returned by Memory_alloc().
size must be equivalent to the size passed in during the Memory_alloc() allocation.
See also:
Memory_alloc()
Void Memory_dumpKnownContigBufsList ( Void   ) 

Dumps the list of all translated/registered bufs.

Remarks:
The list is printed using the tracing infrastructure at trace level 5 to tracemask Memory_GTNAME.
There are several mechanisms to enable this trace mask, one would be to do the following from your application:
See also:
Memory_registerContigBuf()
Memory_unregisterContigBuf()
UInt32 Memory_getBufferPhysicalAddress ( Ptr  virtualAddress,
Int  sizeInBytes,
Bool *  isContiguous 
)

Converts application virtual address to a physical address.

This API also checks verifies that the buffer is really contiguous.

Parameters:
[in] virtualAddress Address of a buffer.
[in] sizeInBytes Size of the buffer.
[out] isContiguous Optional flag indicating whether the buffer was physically contiguous or not.
Return values:
0 Failure, the physical address could not be obtained.
non-zero The physical address of the buffer.
Remarks:
sizeInBytes must be non-zero.
isContiguous is an optional parameter, and can be NULL if the caller doesn't want the results of this check. If isContiguous is NULL but the buffer is not contiguous, error trace will be generated.
If a physically discontiguous buffer is provided in virtualAddress, zero will be returned. And if isContiguous is non-null, it will be set to FALSE.
This is typically called by a stub implementation to translate an application-side virtual address into a physical address usable by a remote skeleton and algorithm.
To enable portable code, this is safe to call on systems without virtual memory. In those cases, the returned physical buffer will be the same as the provided "virtual" buffer.
See also:
Memory_getBufferVirtualAddress()
Int Memory_getHeapId ( String  name  ) 

Get the heap heap ID corresponding to a heap name. This number will be between 0 and the value returned by Memory_getNumHeaps(). The heap Id can be passed to Memory_redefine(), Memory_restoreHeap(), and Memory_segStat().

Remarks:
This is an unsupported, private function. There is no contract to provide compatibility between releases, and it may be deleted at any time.
Return values:
>= 0 The heap number.
< 0 No heap with the given name was found.
See also:
Memory_getNumHeaps()
Int Memory_getNumHeaps (  ) 

Get the number of memory heaps.

Remarks:
This is an unsupported, private function. There is no contract to provide compatibility between releases, and it may be deleted at any time.
Return values:
The number of memroy heaps.
See also:
Memory_getHeapId()
Ptr Memory_getBufferVirtualAddress ( UInt32  physicalAddress,
Int  sizeInBytes 
)

Obtains the virtual address of a physically contiguous buffer.

Parameters:
[in] physicalAddress Physical address of a buffer.
[in] sizeInBytes Size of the buffer.
Return values:
NULL Failure, the virtual address could not be obtained.
non-zero The virtual address of the buffer.
Remarks:
sizeInBytes must be non-zero.
If virtualAddress, was not acquired by Memory_getBufferPhysicalAddress(), no attempt is made to map the physically contiguous buffer into a the application's virtual memory space.
This is typically called by a stub implementation to translate a buffer provided by a remote skeleton and/or algorithm into an application-usable, virtual address.
To enable portable code, this is safe to call on systems without virtual memory. In those cases, the returned "virtual" buffer will be the same as the provided physical buffer.
See also:
Memory_getBufferPhysicalAddress()
Void Memory_registerContigBuf ( UInt32  virtualAddress,
UInt32  sizeInBytes,
UInt32  physicalAddress 
)

Register a physical buffer allocated without Memory_contigAlloc().

Parameters:
[in] virtualAddress Address of the buffer mapped into the process space
[in] sizeInBytes Size of the region
[in] physicalAddress Physical address of the buffer
Remarks:
A cache of "app-address to codec-address" mappings (e.g. virtual to physical address mappings in DM644x devices) is internally maintained in some environments (e.g. Linux). This is used, for example, by Memory_getBufferPhysicalAddress() and Memory_getBufferVirtualAddress(). This lookup map is automatically updated when using Memory_contigAlloc() and Memory_contigFree(). However, if the user acquires buffers independently, it must use Memory_registerContigBuf() and Memory_unregisterContigBuf() to ensure the lookup map is current.
Individual sub-blocks of a buffer need not be registered; registering the entire buffer once will suffice.
This API is typically only required for environments with virtual memory (e.g. Linux-based systems).
See also:
Memory_unregisterContigBuf()
Memory_dumpKnownContigBufsList()
Void Memory_unregisterContigBuf ( UInt32  virtualAddress,
UInt32  sizeInBytes 
)

Unregisters a physical buffer allocated without Memory_contigAlloc().

Parameters:
[in] virtualAddress beginning address of the buffer mapped into the process space
[in] sizeInBytes size of the region
Remarks:
This API must be used to unregister a buffer allocated outside of Memory_contigAlloc() if the buffer (or a portion of it) is passed on to VISA calls. Segments of the buffer need not be individually unregistered.
See also:
Memory_registerContigBuf()
Memory_dumpKnownContigBufsList()

Variable Documentation

Default parameters for Memory_alloc() & Memory_free().

Remarks:
Memory_DEFAULTPARAMS will be used when NULL is passed in the Memory_AllocParams parameter for Memory_alloc() & Memory_free(). When passing a non-NULL Memory_AllocParams parameter, you should first copy Memory_DEFAULTPARAMS to your structure and then modify individual elements as needed:
See also:
Memory_alloc()
Memory_free()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2010, Texas Instruments Incorporated