1.00 Audio Decoder Codec Interface
Defines |
#define | AUDDEC1_EOK IAUDDEC1_EOK |
#define | AUDDEC1_EFAIL IAUDDEC1_EFAIL |
#define | AUDDEC1_EUNSUPPORTED IAUDDEC1_EUNSUPPORTED |
#define | AUDDEC1_ETIMEOUT VISA_ETIMEOUT |
#define | AUDDEC1_FOREVER VISA_FOREVER |
Typedefs |
typedef VISA_Handle | AUDDEC1_Handle |
| Opaque handle to a AUDDEC1 codec.
|
typedef struct IAUDDEC1_Params | AUDDEC1_Params |
| This structure defines the parameters necessary to create an instance of a 1.0 audio decoder object.
|
typedef IAUDDEC1_InArgs | AUDDEC1_InArgs |
typedef IAUDDEC1_OutArgs | AUDDEC1_OutArgs |
typedef IAUDDEC1_Cmd | AUDDEC1_Cmd |
typedef IAUDDEC1_Status | AUDDEC1_Status |
typedef IAUDDEC1_DynamicParams | AUDDEC1_DynamicParams |
Functions |
Int32 | AUDDEC1_control (AUDDEC1_Handle handle, AUDDEC1_Cmd id, AUDDEC1_DynamicParams *params, AUDDEC1_Status *status) |
| Execute the control() method in this instance of an audio1 decoder algorithm.
|
AUDDEC1_Handle | AUDDEC1_create (Engine_Handle e, String name, AUDDEC1_Params *params) |
| Create an instance of an audio decoder algorithm.
|
Void | AUDDEC1_delete (AUDDEC1_Handle handle) |
| Delete the instance of an audio decoder algorithm.
|
Int32 | AUDDEC1_process (AUDDEC1_Handle handle, XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs, AUDDEC1_InArgs *inArgs, AUDDEC1_OutArgs *outArgs) |
| Execute the process() method in this instance of a audio decoder algorithm.
|
Int32 | AUDDEC1_processAsync (AUDDEC1_Handle handle, XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs, AUDDEC1_InArgs *inArgs, AUDDEC1_OutArgs *outArgs) |
| Perform asynchronous submission to this instance of a audio decoder algorithm.
|
Int32 | AUDDEC1_processWait (AUDDEC1_Handle handle, XDM1_BufDesc *inBufs, XDM1_BufDesc *outBufs, AUDDEC1_InArgs *inArgs, AUDDEC1_OutArgs *outArgs, UInt timeout) |
| Wait for a return message from a previous invocation of AUDDEC1_processAsync() in this instance of an audio decoder algorithm.
|
Detailed Description
This is the 1.00 audio decoder codec interface. Several of the data types in this API are specified by the xDM 1.00 interface; please see the xDM documentation for those details.
Define Documentation
#define AUDDEC1_EOK IAUDDEC1_EOK |
#define AUDDEC1_EFAIL IAUDDEC1_EFAIL |
#define AUDDEC1_EUNSUPPORTED IAUDDEC1_EUNSUPPORTED |
#define AUDDEC1_ETIMEOUT VISA_ETIMEOUT |
#define AUDDEC1_FOREVER VISA_FOREVER |
Special value for timeout parameter indicating never timeout.
Typedef Documentation
Opaque handle to a AUDDEC1 codec.
This structure defines the parameters necessary to create an instance of a 1.0 audio decoder object.
This structure defines the codec parameters that can be modified after creation via control() calls.
- See also:
- IAUDDEC1_Fxns::control()
Function Documentation
Execute the control() method in this instance of an audio1 decoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created audio decoder instance. |
[in] | id | Command id for xDM control operation. |
[in] | params | Runtime control parameters used for decoding. |
[out] | status | Status info upon completion of decode operation. |
- Precondition:
handle
is a valid (non-NULL) audio decoder handle and the audio decoder is in the created state.
- Return values:
-
- See also:
- AUDDEC1_create()
-
AUDDEC1_delete()
-
IAUDDEC1_Fxns()control()
Create an instance of an audio decoder algorithm.
Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via AUDDEC1_create()) or explicitly serialize access to a shared handle.
- Parameters:
-
[in] | e | Handle to an opened engine. |
[in] | name | String identifier of the type of audio decoder. to create. |
[in] | params | Creation parameters. |
- Return values:
-
| NULL | An error has occurred. |
| non-NULL | The handle to the newly created audio decoder instance. |
- See also:
- Engine_open()
-
AUDDEC1_delete()
Delete the instance of an audio decoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created audio decoder instance. |
- Precondition:
handle
is a valid (non-NULL) handle which is in the created state.
- Postcondition:
- All resources allocated as part of the AUDDEC1_create() operation (memory, DMA channels, etc.) are freed.
- See also:
- AUDDEC1_create()
Perform asynchronous submission to this instance of a audio decoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created audio decoder instance. |
[in] | inBufs | A buffer descriptor containing input buffers. |
[out] | outBufs | A buffer descriptor containing output buffers. |
[in] | inArgs | Input Arguments. |
[out] | outArgs | Output Arguments. |
- Precondition:
handle
is a valid (non-NULL) audio decoder handle and the audio decoder is in the created state.
- Return values:
-
- See also:
- AUDDEC1_create()
-
AUDDEC1_delete()
-
AUDDEC1_control()
-
AUDDEC1_process()
-
AUDDEC1_processWait()
-
IAUDDEC1_Fxns::process()
Wait for a return message from a previous invocation of AUDDEC1_processAsync() in this instance of an audio decoder algorithm.
- Parameters:
-
[in] | handle | Handle to a created audio decoder instance. |
[in] | inBufs | A buffer descriptor containing input buffers. |
[out] | outBufs | A buffer descriptor containing output buffers. |
[in] | inArgs | Input Arguments. |
[out] | outArgs | Output Arguments. |
[in] | timeout | Amount of "time" to wait (from 0 -> AUDDEC1_FOREVER) |
- Precondition:
handle
is a valid (non-NULL) audio decoder handle and the audio decoder is in the created state.
- Return values:
-
- See also:
- AUDDEC1_create()
-
AUDDEC1_delete()
-
AUDDEC1_control()
-
AUDDEC1_process()
-
AUDDEC1_processAsync()