ISPHDEC_Params Struct Reference
[XDM ISPHDEC Speech/Voice Decoder Interface]

Defines the creation time parameters for all ISPHDEC instance objects. More...

#include <isphdec.h>

Data Fields

XDAS_Int32 size
XDAS_Int32 dataEnable
XDAS_Int32 compandingLaw
XDAS_Int32 packingType

Detailed Description

Defines the creation time parameters for all ISPHDEC instance objects.

Remarks:
The application should set the parameters to 0 to use the algorithm's default values.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

Field Documentation

Size of this structure in bytes. Because this structure can be extended, this field must be correctly set by the caller.

TTY/DTMF enabled flag. Set to 1 to enable, 0 to disable.

Companding Law.

See also:
ISPEECH_CompoundLaw.

Packing Format Option (for codecs that support multiple packing formats - used for selection, 0, 1, 2...)


The documentation for this struct was generated from the following file:
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated