Video decoder codec interface

Data Structures

struct  IVIDDEC2_CodecClassConfig
 Definition of IVIDDEC2 codec class configurable parameters. More...

Defines

#define VIDDEC2_EOK   IVIDDEC2_EOK
#define VIDDEC2_EFAIL   IVIDDEC2_EFAIL
#define VIDDEC2_EUNSUPPORTED   IVIDDEC2_EUNSUPPORTED
#define VIDDEC2_ETIMEOUT   VISA_ETIMEOUT
#define VIDDEC2_FOREVER   VISA_FOREVER

Typedefs

typedef VISA_Handle VIDDEC2_Handle
 Opaque handle to a VIDDEC2 codec.
typedef IVIDDEC2_Params VIDDEC2_Params
typedef IVIDDEC2_InArgs VIDDEC2_InArgs
typedef IVIDDEC2_OutArgs VIDDEC2_OutArgs
typedef IVIDDEC2_Cmd VIDDEC2_Cmd
typedef IVIDDEC2_DynamicParams VIDDEC2_DynamicParams
typedef IVIDDEC2_Status VIDDEC2_Status

Functions

Int32 VIDDEC2_control (VIDDEC2_Handle handle, VIDDEC2_Cmd id, VIDDEC2_DynamicParams *params, VIDDEC2_Status *status)
 Execute the control() method in this instance of a video decoder algorithm.
VIDDEC2_Handle VIDDEC2_create (Engine_Handle e, String name, VIDDEC2_Params *params)
 Create an instance of a video decoder algorithm.
Void VIDDEC2_delete (VIDDEC2_Handle handle)
 Delete the instance of a video decoder algorithm.
Int32 VIDDEC2_process (VIDDEC2_Handle handle, XDM1_BufDesc *inBufs, XDM_BufDesc *outBufs, VIDDEC2_InArgs *inArgs, VIDDEC2_OutArgs *outArgs)
 Execute the process() method in this instance of a video decoder algorithm.
XDAS_Int32 VIDDEC2_processAsync (VIDDEC2_Handle handle, XDM1_BufDesc *inBufs, XDM_BufDesc *outBufs, VIDDEC2_InArgs *inArgs, VIDDEC2_OutArgs *outArgs)
 Perform asynchronous submission to this instance of a video decoder algorithm.
XDAS_Int32 VIDDEC2_processWait (VIDDEC2_Handle handle, XDM1_BufDesc *inBufs, XDM_BufDesc *outBufs, VIDDEC2_InArgs *inArgs, VIDDEC2_OutArgs *outArgs, UInt timeout)
 Wait for a return message from a previous invocation of VIDDEC2_processAsync() in this instance of an video decoder algorithm.

Detailed Description

This is the VIDDEC2 video decoder codec interface. Several of the data types in this API are specified by the XDM IVIDDEC2 interface; please see the XDM documentation for those details.


Define Documentation

#define VIDDEC2_EOK   IVIDDEC2_EOK

Success.

#define VIDDEC2_EFAIL   IVIDDEC2_EFAIL

General failure.

#define VIDDEC2_EUNSUPPORTED   IVIDDEC2_EUNSUPPORTED

Request is unsupported.

#define VIDDEC2_ETIMEOUT   VISA_ETIMEOUT

Timeout occurred.

#define VIDDEC2_FOREVER   VISA_FOREVER

Special value for timeout parameter indicating never timeout.


Typedef Documentation

Opaque handle to a VIDDEC2 codec.

Defines the creation time parameters for all IVIDDEC2 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.

Defines the input arguments for all IVIDDEC2 instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC2_Fxns::process()

Defines the run time output arguments for all IVIDDEC2 instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC2_Fxns::process()

Defines the control commands for the IVIDDEC2 module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IVIDDEC2_Fxns::control()

This structure defines the codec parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that a given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IVIDDEC2_Fxns::control()

Defines instance status parameters.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
All fields correspond to latest IVIDDEC2_Fxns::process() call on the particular instance of the decoder.
See also:
IVIDDEC2_Fxns::control()


Function Documentation

Int32 VIDDEC2_control ( VIDDEC2_Handle  handle,
VIDDEC2_Cmd  id,
VIDDEC2_DynamicParams params,
VIDDEC2_Status status 
)

Execute the control() method in this instance of a video decoder algorithm.

Parameters:
[in] handle Handle to a created video decoder instance.
[in] id Command id for XDM control operation.
[in] params Runtime control parameters used for decoding.
[out] status Status info upon completion of decode operation.
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC2_EOK Success.
VIDDEC2_EFAIL Failure.
VIDDEC2_EUNSUPPORTED Unsupported request.
Remarks:
This is a blocking call, and will return after the control command has been executed.
See also:
VIDDEC2_create()
VIDDEC2_delete()
IVIDDEC2_Fxns::process()
VIDDEC2_Handle VIDDEC2_create ( Engine_Handle  e,
String  name,
VIDDEC2_Params params 
)

Create an instance of a video decoder algorithm.

Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via VIDDEC2_create) or explicitly serialize access to a shared handle.

Parameters:
[in] e Handle to an opened engine.
[in] name String identifier of the type of video decoder to create.
[in] params Creation parameters.
Return values:
NULL An error has occurred.
non-NULL The handle to the newly created video decoder instance.
Remarks:
params is optional. If it's not supplied, codec-specific default params will be used.
Depending on the configuration of the engine opened, this call may create a local or remote instance of the video decoder.
In general, name is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated, to be overridden. This optional argument string is of the form ":priority", ":priority:flag", or "::flag".
priority is the new priority to create the codec with.
The flag must be either 0 or 1, and if 1, all memory allocated for the codec will be in the heap that corresponds to IALG_EXTERNAL. If flag is 0, the memory for the codec will be allocated from the heaps it has requested. For example, if a codec named "mp3" has been configured into the system, setting name to "mp3:4" would cause the codec to be created at priority 4, instead of whatever priority was configured. This feature is useful if more than one instance of the codec are to be created at different priorities.
The flag can be used to prevent the codec from using any internal memory, for example, if it is to be run at the same time as another codec that must use internal memory, and there is insufficient internal memory for both.
See also:
Engine_open()
VIDDEC2_delete()
Void VIDDEC2_delete ( VIDDEC2_Handle  handle  ) 

Delete the instance of a video decoder algorithm.

Parameters:
[in] handle Handle to a created video decoder instance.
Remarks:
Depending on the configuration of the engine opened, this call may delete a local or remote instance of the video decoder.
Precondition:
handle is a valid (non-NULL) handle which is in the created state.
Postcondition:
All resources allocated as part of the VIDDEC2_create() operation (memory, DMA channels, etc.) are freed.
See also:
VIDDEC2_create()
Int32 VIDDEC2_process ( VIDDEC2_Handle  handle,
XDM1_BufDesc inBufs,
XDM_BufDesc outBufs,
VIDDEC2_InArgs inArgs,
VIDDEC2_OutArgs outArgs 
)

Execute the process() method in this instance of a video decoder algorithm.

Parameters:
[in] handle Handle to a created video decoder instance.
[in] inBufs A buffer descriptor containing input buffers.
[out] outBufs A buffer descriptor containing output buffers.
[in] inArgs Input Arguments.
[out] outArgs Output Arguments.
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC2_EOK Success.
VIDDEC2_EFAIL Failure.
VIDDEC2_EUNSUPPORTED Unsupported request.
Remarks:
Since the VIDDEC2 decoder contains support for asynchronous buffer submission and retrieval, this API becomes known as synchronous in nature.
This is a blocking call, and will return after the data has been decoded.
The buffers supplied to VIDDEC2_process() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDDEC2_create()
VIDDEC2_delete()
VIDDEC2_control()
VIDDEC2_processAsync()
VIDDEC2_processWait()
IVIDDEC2_Fxns::process()
XDAS_Int32 VIDDEC2_processAsync ( VIDDEC2_Handle  handle,
XDM1_BufDesc inBufs,
XDM_BufDesc outBufs,
VIDDEC2_InArgs inArgs,
VIDDEC2_OutArgs outArgs 
)

Perform asynchronous submission to this instance of a video decoder algorithm.

Parameters:
[in] handle Handle to a created video decoder instance.
[in] inBufs A buffer descriptor containing input buffers.
[out] outBufs A buffer descriptor containing output buffers.
[in] inArgs Input Arguments.
[out] outArgs Output Arguments.
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC2_EOK Success.
VIDDEC2_EFAIL Failure.
VIDDEC2_EUNSUPPORTED Unsupported request.
Remarks:
This API is the asynchronous counterpart to the process() method. It allows for buffer and argument submission without waiting for retrieval. A response is retrieved using the VIDDEC2_processWait() API.
The buffers supplied to VIDDEC2_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDDEC2_create()
VIDDEC2_delete()
VIDDEC2_control()
VIDDEC2_process()
VIDDEC2_processWait()
IVIDDEC2_Fxns::process()
XDAS_Int32 VIDDEC2_processWait ( VIDDEC2_Handle  handle,
XDM1_BufDesc inBufs,
XDM_BufDesc outBufs,
VIDDEC2_InArgs inArgs,
VIDDEC2_OutArgs outArgs,
UInt  timeout 
)

Wait for a return message from a previous invocation of VIDDEC2_processAsync() in this instance of an video decoder algorithm.

Parameters:
[in] handle Handle to a created video decoder instance.
[in] inBufs A buffer descriptor containing input buffers.
[out] outBufs A buffer descriptor containing output buffers.
[in] inArgs Input Arguments.
[out] outArgs Output Arguments.
[in] timeout Amount of "time" to wait (from 0 -> VIDDEC2_FOREVER)
Precondition:
handle is a valid (non-NULL) video decoder handle and the video decoder is in the created state.
Return values:
VIDDEC2_EOK Success.
VIDDEC2_EFAIL Failure.
VIDDEC2_EUNSUPPORTED Unsupported request.
VIDDEC2_ETIMEOUT Operation timed out.
Remarks:
This is a blocking call, and will return after the data has been decoded.
"Polling" is supported by using a timeout of 0. Waiting forever is supported by using a timeout of VIDDEC2_EFOREVER.
There must have previously been an invocation of the VIDDEC2_processAsync() API.
The buffers supplied to VIDDEC2_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
VIDDEC2_create()
VIDDEC2_delete()
VIDDEC2_control()
VIDDEC2_process()
VIDDEC2_processAsync()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated