AUDENC Audio Encoder Interface

Defines

#define AUDENC_EOK   IAUDENC_EOK
#define AUDENC_EFAIL   IAUDENC_EFAIL
#define AUDENC_ERUNTIME   IAUDENC_ERUNTIME
#define AUDENC_ETIMEOUT   VISA_ETIMEOUT
#define AUDENC_FOREVER   VISA_FOREVER

Typedefs

typedef IAUDENC_Status AUDENC_Status
typedef VISA_Handle AUDENC_Handle
 Opaque handle to a AUDENC codec.
typedef struct IAUDENC_Params AUDENC_Params
 This structure defines the parameters necessary to create an instance of a Audio Encoder object.
typedef IAUDENC_InArgs AUDENC_InArgs
typedef IAUDENC_OutArgs AUDENC_OutArgs
typedef IAUDENC_Cmd AUDENC_Cmd
typedef IAUDENC_DynamicParams AUDENC_DynamicParams

Functions

AUDENC_Handle AUDENC_create (Engine_Handle e, String name, AUDENC_Params *params)
 Create an instance of an audio encoder algorithm.
Int32 AUDENC_process (AUDENC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, AUDENC_InArgs *inArgs, AUDENC_OutArgs *outArgs)
 Execute the process() method in this instance of an audio encoder algorithm.
Int32 AUDENC_control (AUDENC_Handle handle, AUDENC_Cmd id, AUDENC_DynamicParams *params, AUDENC_Status *status)
 Execute the control() method in this instance of an audio encoder algorithm.
Void AUDENC_delete (AUDENC_Handle handle)
 Delete the instance of an audio encoder algorithm.
XDAS_Int32 AUDENC_processAsync (AUDENC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, IAUDENC_InArgs *inArgs, IAUDENC_OutArgs *outArgs)
 Perform asynchronous submission to this instance of a audio encoder algorithm.
XDAS_Int32 AUDENC_processWait (AUDENC_Handle handle, XDM_BufDesc *inBufs, XDM_BufDesc *outBufs, IAUDENC_InArgs *inArgs, IAUDENC_OutArgs *outArgs, UInt timeout)
 Wait for a return message from a previous invocation of AUDENC_processAsync() in this instance of an audio encoder algorithm.

Detailed Description

This is the AUDENC audio encoder codec interface. Several of the data types in this API are specified by the XDM interface; please see the XDM documentation for those details.


Define Documentation

#define AUDENC_EOK   IAUDENC_EOK

Success.

#define AUDENC_EFAIL   IAUDENC_EFAIL

General failure.

#define AUDENC_ERUNTIME   IAUDENC_ERUNTIME

General runtime failure.

#define AUDENC_ETIMEOUT   VISA_ETIMEOUT

Timeout occurred.

#define AUDENC_FOREVER   VISA_FOREVER

Special value for timeout parameter indicating never timeout.


Typedef Documentation

Defines instance status parameters (read-only).

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IAUDENC_Fxns::control()

Opaque handle to a AUDENC codec.

typedef struct IAUDENC_Params AUDENC_Params

This structure defines the parameters necessary to create an instance of a Audio Encoder object.

Defines the input arguments for all IAUDENC instance process function.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IAUDENC_Fxns::process()

Defines the run time output arguments for all IAUDENC instance objects.

Remarks:
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IAUDENC_Fxns::process()

Defines the control commands for the IAUDENC module.

Remarks:
This ID can be extended in IMOD interface for additional controls.
See also:
XDM_CmdId
IAUDENC_Fxns::control()

This structure defines the algorithm parameters that can be modified after creation via control() calls.

Remarks:
It is not necessary that given implementation support all dynamic parameters to be configurable at run time. If a particular algorithm does not support run-time updates to a parameter that the application is attempting to change at runtime, it may indicate this as an error.
This structure may be extended by individual codec implementations allowing customization with vendor specific parameters. The presence of vendor specific extensions will be detected by the value of the size parameter.
The size field must be correctly set by the caller. See http://tiexpressdsp.com/index.php?title=Extending_data_structures_in_xDM for more details.
See also:
IAUDENC_Fxns::control()


Function Documentation

AUDENC_Handle AUDENC_create ( Engine_Handle  e,
String  name,
AUDENC_Params params 
)

Create an instance of an audio encoder algorithm.

Instance handles must not be concurrently accessed by multiple threads; each thread must either obtain its own handle (via AUDENC_create()) or explicitly serialize access to a shared handle.

Parameters:
[in] e Handle to an opened engine.
[in] name String identifier of the type of audio encoder. to create.
[in] params Creation parameters.
Return values:
NULL An error has occurred.
non-NULL The handle to the newly created audio encoder instance.
Remarks:
params is optional. If it's not supplied, codec-specific default params will be used.
Depending on the configuration of the engine opened, this call may create a local or remote instance of the audio encoder.
In general, name is the name of the codec configured by the system integrator. However, an optional "argument string" may be appended to the codec name, to allow the codec's configured priority and/or the heaps where its memory will be allocated, to be overridden. This optional argument string is of the form ":priority", ":priority:flag", or "::flag".
priority is the new priority to create the codec with.
The flag must be either 0 or 1, and if 1, all memory allocated for the codec will be in the heap that corresponds to IALG_EXTERNAL. If flag is 0, the memory for the codec will be allocated from the heaps it has requested. For example, if a codec named "mp3" has been configured into the system, setting name to "mp3:4" would cause the codec to be created at priority 4, instead of whatever priority was configured. This feature is useful if more than one instance of the codec are to be created at different priorities.
The flag can be used to prevent the codec from using any internal memory, for example, if it is to be run at the same time as another codec that must use internal memory, and there is insufficient internal memory for both.
See also:
Engine_open()
AUDENC_delete()
Int32 AUDENC_process ( AUDENC_Handle  handle,
XDM_BufDesc inBufs,
XDM_BufDesc outBufs,
AUDENC_InArgs inArgs,
AUDENC_OutArgs outArgs 
)

Execute the process() method in this instance of an audio encoder algorithm.

Parameters:
[in] handle Handle to a created audio encoder instance.
[in] inBufs A buffer descriptor containing input buffers.
[out] outBufs A buffer descriptor containing output buffers.
[in] inArgs Input Arguments.
[out] outArgs Output Arguments.
Precondition:
handle is a valid (non-NULL) audio encoder handle and the audio encoder is in the created state.
Return values:
AUDENC_EOK Success.
AUDENC_EFAIL Failure.
AUDENC_ERUNTIME Internal Runtime Error.
Remarks:
Since the AUDENC encoder contains support for asynchronous buffer submission and retrieval, this API becomes known as synchronous in nature.
This is a blocking call, and will return after the data has been encoded.
The buffers supplied to AUDENC_process() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
If an error is returned, outArgs->extendedError may indicate further details about the error. See AUDENC_OutArgs::extendedError for details.
See also:
AUDENC_create()
AUDENC_delete()
AUDENC_control()
AUDENC_processAsync()
AUDENC_processWait()
IAUDENC_Fxns::process() - the reflected algorithm interface, which may contain further usage details.
Int32 AUDENC_control ( AUDENC_Handle  handle,
AUDENC_Cmd  id,
AUDENC_DynamicParams params,
AUDENC_Status status 
)

Execute the control() method in this instance of an audio encoder algorithm.

Parameters:
[in] handle Handle to a created audio encoder instance.
[in] id Command id for XDM control operation.
[in] params Runtime control parameters used for encoding.
[out] status Status info upon completion of encode operation.
Precondition:
handle is a valid (non-NULL) audio encoder handle and the audio encoder is in the created state.
Return values:
AUDENC_EOK Success.
AUDENC_EFAIL Failure.
AUDENC_ERUNTIME Internal Runtime Error.
Remarks:
This is a blocking call, and will return after the control command has been executed.
If an error is returned, status->extendedError may indicate further details about the error. See AUDDEC_Status::extendedError for details.
See also:
AUDENC_create()
AUDENC_delete()
IAUDENC_Fxns::control() - the reflected algorithm interface, which may contain further usage details.
Void AUDENC_delete ( AUDENC_Handle  handle  ) 

Delete the instance of an audio encoder algorithm.

Parameters:
[in] handle Handle to a created audio encoder instance.
Remarks:
Depending on the configuration of the engine opened, this call may delete a local or remote instance of the audio encoder.
Precondition:
handle is a valid (non-NULL) handle which is in the created state.
Postcondition:
All resources allocated as part of the AUDENC_create() operation (memory, DMA channels, etc.) are freed.
See also:
AUDENC_create()
XDAS_Int32 AUDENC_processAsync ( AUDENC_Handle  handle,
XDM_BufDesc inBufs,
XDM_BufDesc outBufs,
IAUDENC_InArgs inArgs,
IAUDENC_OutArgs outArgs 
)

Perform asynchronous submission to this instance of a audio encoder algorithm.

Parameters:
[in] handle Handle to a created audio encoder instance.
[in] inBufs A buffer descriptor containing input buffers.
[out] outBufs A buffer descriptor containing output buffers.
[in] inArgs Input Arguments.
[out] outArgs Output Arguments.
Precondition:
handle is a valid (non-NULL) audio encoder handle and the audio encoder is in the created state.
Return values:
AUDENC_EOK Success.
AUDENC_EFAIL Failure.
AUDENC_ERUNTIME Internal Runtime Error.
Remarks:
This API is the asynchronous counterpart to the process() method. It allows for buffer and argument submission without waiting for retrieval. A response is retrieved using the AUDENC_processWait() API.
The buffers supplied to AUDENC_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
AUDENC_create()
AUDENC_delete()
AUDENC_control()
AUDENC_process()
AUDENC_processWait()
IAUDENC_Fxns::process()
IAUDENC_Fxns::process() - the reflected algorithm interface, which may contain further usage details.
XDAS_Int32 AUDENC_processWait ( AUDENC_Handle  handle,
XDM_BufDesc inBufs,
XDM_BufDesc outBufs,
IAUDENC_InArgs inArgs,
IAUDENC_OutArgs outArgs,
UInt  timeout 
)

Wait for a return message from a previous invocation of AUDENC_processAsync() in this instance of an audio encoder algorithm.

Parameters:
[in] handle Handle to a created audio encoder instance.
[in] inBufs A buffer descriptor containing input buffers.
[out] outBufs A buffer descriptor containing output buffers.
[in] inArgs Input Arguments.
[out] outArgs Output Arguments.
[in] timeout Amount of "time" to wait (from 0 -> AUDENC_FOREVER)
Precondition:
handle is a valid (non-NULL) audio encoder handle and the audio encoder is in the created state.
Return values:
AUDENC_EOK Success.
AUDENC_EFAIL Failure.
AUDENC_ERUNTIME Internal Runtime Error.
AUDENC_ETIMEOUT Operation timed out.
Remarks:
This is a blocking call, and will return after the data has been decoded.
"Polling" is supported by using a timeout of 0. Waiting forever is supported by using a timeout of AUDENC_EFOREVER.
There must have previously been an invocation of the AUDENC_processAsync() API.
The buffers supplied to AUDENC_processAsync() may have constraints put on them. For example, in dual-processor, shared memory architectures, where the codec is running on a remote processor, the buffers may need to be physically contiguous. Additionally, the remote processor may place restrictions on buffer alignment.
See also:
AUDENC_create()
AUDENC_delete()
AUDENC_control()
AUDENC_process()
AUDENC_processAsync()
 All Data Structures Files Functions Variables Typedefs Enumerations Enumerator Defines

Copyright 2009, Texas Instruments Incorporated