module ti.sysbios.hal.SecondsClock |
|
|
|
Seconds module that uses Clock as its' time base
#include <ti/sysbios/hal/SecondsClock.h>
Functions common to all ISeconds modules |
UInt32 | |
Void | |
Functions common to all target modules |
|
|
SecondsClock_get() // module-wide |
|
Returns number of seconds since 1970 (the Unix epoch)
UInt32 SecondsClock_get();
DETAILS
The user must call Seconds_set() before making any calls to Seconds_get(),
otherwise the value returned by Seconds_get() will be meaningless.
SecondsClock_set() // module-wide |
|
Update the real time clock with number of seconds since 1970
Void SecondsClock_set(UInt32 seconds);
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool SecondsClock_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool SecondsClock_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 SecondsClock_Module_getMask();
// Returns the diagnostics mask for this module
Void SecondsClock_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
var SecondsClock = xdc.useModule('ti.sysbios.hal.SecondsClock');
module-wide config parameters
generated on Wed, 15 Apr 2015 00:18:20 GMT