Additional ARM device-specific APIs are also provided.
const Hwi_NUM_INTERRUPTS |
|
The DM6446 ARM Interrupt Controller supports 64 interrupts
#define Hwi_NUM_INTERRUPTS (Int)64
enum Hwi_MaskingOption |
|
Shorthand interrupt masking options
typedef enum Hwi_MaskingOption {
Hwi_MaskingOption_NONE,
// No interrupts are disabled
Hwi_MaskingOption_ALL,
// All interrupts are disabled
Hwi_MaskingOption_SELF,
// Only this interrupt is disabled
Hwi_MaskingOption_BITMASK,
// User supplies IER masks
Hwi_MaskingOption_LOWER
// All current and lower priority
interrupts are disabled. Only a few
targets/devices truly support this
masking option. For those that don't,
this setting is treated the same as
MaskingOption_SELF
} Hwi_MaskingOption;
typedef Hwi_FuncPtr |
|
Hwi create function type definition
typedef Void (*Hwi_FuncPtr)(UArg);
typedef Hwi_Irp |
|
Interrupt Return Pointer.
This is the address of the interrupted instruction
typedef Hwi_VectorFuncPtr |
|
Hwi vector function type definition
typedef Void (*Hwi_VectorFuncPtr)(Void);
struct Hwi_AINTC |
|
ARM Interrupt Controller
typedef struct Hwi_AINTC {
UInt32 FIQ0;
// 0x00 Interrupt Status of INT [31:0] if mapped to FIQ
UInt32 FIQ1;
// 0x04 Interrupt Status of INT [63:32] if mapped to FIQ
UInt32 IRQ0;
// 0x08 Interrupt Status of INT [31:0] if mapped to IRQ
UInt32 IRQ1;
// 0x0C Interrupt Status of INT [63:32] if mapped to IRQ
UInt32 FIQENTRY;
// 0x10 Entry Address [28:0] for valid FIQ interrupt
UInt32 IRQENTRY;
// 0x14 Entry Address [28:0] for valid IRQ interrupt
UInt32 EINT0;
// 0x18 Interrupt Enable Register 0
UInt32 EINT1;
// 0x1C Interrupt Enable Register 1
UInt32 INTCTL;
// 0x20 Interrupt Operation Control Register
UInt32 EABASE;
// 0x24 Interrupt Entry Base Address
UInt32 RES[2];
// 0x28 reserved
UInt32 INTPR[8];
// 0x30 Interrupt 0-7 Priority select
} Hwi_AINTC;
struct Hwi_HookSet |
|
Hwi hook set type definition
typedef struct Hwi_HookSet {
Void (*registerFxn)(Int);
} Hwi_HookSet;
DETAILS
The functions that make up a hookSet have certain restrictions. They
cannot call any Hwi instance functions other than Hwi_getHookContext()
and Hwi_setHookContext(). For all practical purposes, they should treat
the Hwi_Handle passed to these functions as an opaque handle.
config Hwi_E_alreadyDefined // module-wide |
|
Error raised when Hwi is already defined
extern const Error_Id Hwi_E_alreadyDefined;
config Hwi_LD_end // module-wide |
|
Issued just after return from Hwi function (with interrupts disabled)
config Hwi_LM_begin // module-wide |
|
Issued just prior to Hwi function invocation (with interrupts disabled)
config Hwi_dispatcherAutoNestingSupport // module-wide |
|
Include interrupt nesting logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherAutoNestingSupport;
DETAILS
Default is true.
This option provides the user with the ability to optimize
interrupt dispatcher performance when support for interrupt
nesting is not required.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that manipulates interrupt mask
registers and enables and disables interrupts before and
after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts
enabled during the execution of your Hwi functions.
config Hwi_dispatcherIrpTrackingSupport // module-wide |
|
Controls whether the
dispatcher retains the interrupted thread's return address
extern const Bool Hwi_dispatcherIrpTrackingSupport;
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that keeps track of the interrupt's
return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return
address using the
getIrp API.
config Hwi_dispatcherSwiSupport // module-wide |
|
Include Swi scheduling logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherSwiSupport;
DETAILS
Default is inherited from
BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that Swis
will not be posted from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Swi scheduler
prior to returning from an interrupt.
config Hwi_dispatcherTaskSupport // module-wide |
|
Include Task scheduling logic in interrupt dispatcher?
extern const Bool Hwi_dispatcherTaskSupport;
DETAILS
Default is inherited from
BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that no
Task scheduling APIs (ie
Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Task scheduler
prior to returning from an interrupt.
config Hwi_eabaseSize // module-wide |
|
EABASE Size Setting. Default is 4 bytes per entry.
Options are 4, 8, 16, 32 bytes per entry
extern const Bits32 Hwi_eabaseSize;
config Hwi_fiqStack // module-wide |
|
FIQ stack pointer. Default = null.
(Indicates that stack is to be created using
staticPlace()
extern const Ptr Hwi_fiqStack;
Hwi_clearInterrupt() // module-wide |
|
Clear a specific interrupt
Void Hwi_clearInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to clear
DETAILS
Clears a specific interrupt's pending status.
The implementation is family-specific.
Hwi_disable() // module-wide |
|
Globally disable interrupts
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_disable globally disables hardware interrupts and returns an
opaque key indicating whether interrupts were globally enabled or
disabled on entry to Hwi_disable().
The actual value of the key is target/device specific and is meant
to be passed to Hwi_restore().
Call Hwi_disable before a portion of a function that needs
to run without interruption. When critical processing is complete, call
Hwi_restore or Hwi_enable to reenable hardware interrupts.
Servicing of interrupts that occur while interrupts are disabled is
postponed until interrupts are reenabled. However, if the same type
of interrupt occurs several times while interrupts are disabled,
the interrupt's function is executed only once when interrupts are
reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if
an enabled interrupt occurred while interrupts are disabled.
Hwi_disable may be called from main(). However, since Hwi interrupts
are already disabled in main(), such a call has no effect.
CONSTRAINTS
If a Task switching API such as
Semaphore_pend(),
Semaphore_post(),
Task_sleep(), or
Task_yield()
is invoked which results in a context switch while
interrupts are disabled, an embedded call to
Hwi_enable occurs
on the way to the new thread context which unconditionally re-enables
interrupts. Interrupts will remain enabled until a subsequent
Hwi_disable
invocation.
Swis always run with interrupts enabled.
See
Swi_post() for a discussion Swis and
interrupts.
Hwi_disableEINT0() // module-wide |
|
Disable specific interrupts (0-31)
Bits32 Hwi_disableEINT0(Bits32 mask);
ARGUMENTS
mask
bitmask of interrupts to disable
RETURNS
previous EINT0 settings bitmask
DETAILS
Disables specific interrupts by clearing the bits specified by
'mask' in the EINT0.
Hwi_disableEINT1() // module-wide |
|
Disable specific interrupts (32-63)
Bits32 Hwi_disableEINT1(Bits32 mask);
ARGUMENTS
mask
bitmask of interrupts to disable
RETURNS
previous EINT1 settings bitmask
DETAILS
Disables specific interrupts by clearing the bits specified by
'mask' in the EINT1.
Hwi_disableFIQ() // module-wide |
|
Disable FIQ interrupts
RETURNS
previous FIQ interrupt enable/disable state
Hwi_disableIRQ() // module-wide |
|
Disable IRQ interrupts
RETURNS
previous IRQ interrupt enable/disable state
Hwi_disableInterrupt() // module-wide |
|
Disable a specific interrupt
UInt Hwi_disableInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to disable
RETURNS
key to restore previous enable/disable state
DETAILS
Disable a specific interrupt identified by an interrupt number.
Hwi_enable() // module-wide |
|
Globally enable interrupts
RETURNS
opaque key for use by Hwi_restore()
DETAILS
Hwi_enable globally enables hardware interrupts and returns an
opaque key indicating whether interrupts were globally enabled or
disabled on entry to Hwi_enable().
The actual value of the key is target/device specific and is meant
to be passed to Hwi_restore().
This function is
called as part of SYS/BIOS Startup_POST_APP_MAIN phase.
Hardware interrupts are enabled unless a call to Hwi_disable disables
them.
Servicing of interrupts that occur while interrupts are disabled is
postponed until interrupts are reenabled. However, if the same type
of interrupt occurs several times while interrupts are disabled,
the interrupt's function is executed only once when interrupts are
reenabled.
A context switch can occur when calling Hwi_enable or Hwi_restore if
an enabled interrupt occurred while interrupts are disabled.
Any call to Hwi_enable enables interrupts, even if Hwi_disable has
been called several times.
Hwi_enable must not be called from main().
Hwi_enableEINT0() // module-wide |
|
Enable specific interrupts (0-31)
Bits32 Hwi_enableEINT0(Bits32 mask);
ARGUMENTS
mask
bitmask of interrupts to disable
RETURNS
previous EINT0 settings bitmask
DETAILS
Enables specific interrupts by clearing the bits specified by
'mask' in the EINT0.
Hwi_enableEINT1() // module-wide |
|
Enable specific interrupts (32-63)
Bits32 Hwi_enableEINT1(Bits32 mask);
ARGUMENTS
mask
bitmask of interrupts to disable
RETURNS
previous EINT0 settings bitmask
DETAILS
Enables specific interrupts by clearing the bits specified by
'mask' in the EINT0.
Hwi_enableFIQ() // module-wide |
|
Enable FIQ interrupts
RETURNS
previous FIQ interrupt enable/disable state
Hwi_enableIRQ() // module-wide |
|
Enable IRQ interrupts
ARGUMENTS
key
enable/disable state to restore
Hwi_enableInterrupt() // module-wide |
|
Enable a specific interrupt
UInt Hwi_enableInterrupt(UInt intNum);
ARGUMENTS
intNum
interrupt number to enable
RETURNS
key to restore previous enable/disable state
DETAILS
Enables a specific interrupt identified by an interrupt number.
Hwi_getHandle() // module-wide |
|
Returns pointer to Hwi instance object
ARGUMENTS
intNum
interrupt number
Hwi_restore() // module-wide |
|
Globally restore interrupts
Void Hwi_restore(UInt key);
ARGUMENTS
key
enable/disable state to restore
DETAILS
Hwi_restore globally restores interrupts to the state determined
by the key argument provided by a previous invocation of Hwi_disable.
A context switch may occur when calling Hwi_restore if Hwi_restore
reenables interrupts and another Hwi occurred while interrupts were
disabled.
Hwi_restore may be called from main(). However, since Hwi_enable
cannot be called from main(), interrupts are always disabled in
main(), and a call to Hwi_restore has no effect.
Hwi_restoreEINT0() // module-wide |
|
Restore maskable interrupts to the state they were in
when either disableEINT0() or enableEINT0() was called
Bits32 Hwi_restoreEINT0(Bits32 mask);
ARGUMENTS
mask
bitmask of interrupts to restore
RETURNS
previous EINT0 settings bitmask
DETAILS
Simply writes mask to the EINT0 register.
Hwi_restoreEINT1() // module-wide |
|
Restore maskable interrupts to the state they were in
when either disableEINT1() or enableEINT1() was called
Bits32 Hwi_restoreEINT1(Bits32 mask);
ARGUMENTS
mask
bitmask of interrupts to restore
RETURNS
previous EINT1 settings bitmask
DETAILS
Simply writes mask to the EINT1 register.
Hwi_restoreFIQ() // module-wide |
|
Restore FIQ interrupts
Void Hwi_restoreFIQ(UInt key);
ARGUMENTS
key
enable/disable state to restore
Hwi_restoreIRQ() // module-wide |
|
Restore IRQ interrupts
Void Hwi_restoreIRQ(UInt key);
ARGUMENTS
key
enable/disable state to restore
Hwi_restoreInterrupt() // module-wide |
|
Restore a specific interrupt's enabled/disabled state
Void Hwi_restoreInterrupt(UInt intNum, UInt key);
ARGUMENTS
intNum
interrupt number to restore
key
key returned from enableInt or disableInt
DETAILS
Restores a specific interrupt identified by an interrupt number.
restoreInterrupt is generally used to restore an interrupt to its state
before
disableInterrupt or
enableInterrupt was
invoked
Hwi_setPriority() // module-wide |
|
Set an interrupt's relative priority
Void Hwi_setPriority(UInt intNum, UInt priority);
ARGUMENTS
intNum
ID of interrupt
priority
priority
DETAILS
Priority 0-1 define the interrupt as an FIQ interrupt
Priority 2-7 define the interrupt as an IRQ interrupt
Hwi_startup() // module-wide |
|
Initially enable interrupts
DETAILS
Called within BIOS_start
Module-Wide Built-Ins |
|
// Get this module's unique id
Bool Hwi_Module_startupDone();
// Test if this module has completed startup
// The heap from which this module allocates memory
Bool Hwi_Module_hasMask();
// Test whether this module has a diagnostics mask
Bits16 Hwi_Module_getMask();
// Returns the diagnostics mask for this module
Void Hwi_Module_setMask(Bits16 mask);
// Set the diagnostics mask for this module
Instance Object Types |
|
typedef struct Hwi_Object Hwi_Object;
// Opaque internal representation of an instance object
// Client reference to an instance object
typedef struct Hwi_Struct Hwi_Struct;
// Opaque client structure large enough to hold an instance object
// Convert this instance structure pointer into an instance handle
// Convert this instance handle into an instance structure pointer
Instance Config Parameters |
|
typedef struct Hwi_Params {
// Instance config-params structure
// Common per-instance configs
UArg arg;
// ISR function argument. Default is 0
Bits32 disableMask0;
// disableMask0. default is derived from MaskingOption_SELF maskSetting
Bits32 disableMask1;
// disableMask1. default is derived from MaskingOption_SELF maskSetting
Bool enableInt;
// Enable this interrupt now? Default is true
Int eventId;
// Interrupt event ID (Interrupt Selection Number)
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored
Int priority;
// Interrupt priority (0-7). Default is 7 which is the
lowest priority IRQ interrupt
Bits32 restoreMask0;
// restoreMask0. default is derived from MaskingOption_SELF maskSetting
Bits32 restoreMask1;
// restoreMask1. default is derived from MaskingOption_SELF maskSetting
} Hwi_Params;
// Initialize this config-params structure with supplier-specified defaults before instance creation
config Hwi_arg // instance |
|
ISR function argument. Default is 0
config Hwi_disableMask0 // instance |
|
disableMask0. default is derived from MaskingOption_SELF maskSetting
config Hwi_disableMask1 // instance |
|
disableMask1. default is derived from MaskingOption_SELF maskSetting
config Hwi_enableInt // instance |
|
Enable this interrupt now? Default is true
config Hwi_eventId // instance |
|
Interrupt event ID (Interrupt Selection Number)
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored
config Hwi_maskSetting // instance |
|
maskSetting. Default is Hwi_MaskingOption_SELF
config Hwi_priority // instance |
|
Interrupt priority (0-7). Default is 7 which is the
lowest priority IRQ interrupt
config Hwi_restoreMask0 // instance |
|
restoreMask0. default is derived from MaskingOption_SELF maskSetting
config Hwi_restoreMask1 // instance |
|
restoreMask1. default is derived from MaskingOption_SELF maskSetting
Instance Creation |
|
// Allocate and initialize a new instance object and return its handle
// Initialize a new instance object inside the provided structure
ARGUMENTS
intNum
interrupt number
hwiFxn
pointer to ISR function
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the
function specified by the fxn parameter and the attributes
specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a
default set of values. Otherwise, the following properties
are specified by a structure of type Hwi_Params.
- The arg element is a generic argument that is passed to the plugged
function as its only parameter. The default value is 0.
- The enableInt element determines whether the interrupt should be
enabled in the IER by create.
- The maskSetting element defines the dispatcherAutoNestingSupport
behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.
Instance Deletion |
|
// Finalize and free this previously allocated instance object, setting the referenced handle to NULL
// Finalize the instance object inside the provided structure
Hwi_getFunc() // instance |
|
Get Hwi function and arg
ARGUMENTS
handle
handle of a previously-created Hwi instance object
arg
pointer for returning hwi's ISR function argument
RETURNS
hwi's ISR function
Hwi_getHookContext() // instance |
|
Get hook instance's context for a Hwi
Ptr Hwi_getHookContext(
Hwi_Handle handle,
Int id);
ARGUMENTS
handle
handle of a previously-created Hwi instance object
RETURNS
hook instance's context for hwi
Hwi_getIrp() // instance |
|
Get address of interrupted instruction
ARGUMENTS
handle
handle of a previously-created Hwi instance object
RETURNS
most current IRP of a Hwi
Hwi_reconfig() // instance |
|
Reconfigure a dispatched interrupt
ARGUMENTS
handle
handle of a previously-created Hwi instance object
Hwi_setFunc() // instance |
|
Overwrite Hwi function and arg
ARGUMENTS
handle
handle of a previously-created Hwi instance object
fxn
pointer to ISR function
arg
argument to ISR function
DETAILS
Replaces a Hwi object's hwiFxn function originally
provided in
create.
Hwi_setHookContext() // instance |
|
Set hook instance's context for a Hwi
Void Hwi_setHookContext(
Hwi_Handle handle,
Int id,
Ptr hookContext);
ARGUMENTS
handle
handle of a previously-created Hwi instance object
id
hook instance's ID
hookContext
value to write to context
Instance Convertors |
|
// unconditionally move one level up the inheritance hierarchy
// conditionally move one level down the inheritance hierarchy; NULL upon failure
Instance Built-Ins |
|
Int Hwi_Object_count();
// The number of statically-created instance objects
// The handle of the i-th statically-created instance object (array == NULL)
// The handle of the first dynamically-created instance object, or NULL
// The handle of the next dynamically-created instance object, or NULL
// The heap used to allocate dynamically-created instance objects
// The label associated with this instance object
// The name of this instance object
const Hwi.NUM_INTERRUPTS |
|
The DM6446 ARM Interrupt Controller supports 64 interrupts
XDCscript usage |
meta-domain |
const Hwi.NUM_INTERRUPTS = 64;
C SYNOPSIS
enum Hwi.MaskingOption |
|
Shorthand interrupt masking options
XDCscript usage |
meta-domain |
values of type Hwi.MaskingOption
const Hwi.MaskingOption_NONE;
// No interrupts are disabled
const Hwi.MaskingOption_ALL;
// All interrupts are disabled
const Hwi.MaskingOption_SELF;
// Only this interrupt is disabled
const Hwi.MaskingOption_BITMASK;
// User supplies IER masks
const Hwi.MaskingOption_LOWER;
// All current and lower priority
interrupts are disabled. Only a few
targets/devices truly support this
masking option. For those that don't,
this setting is treated the same as
MaskingOption_SELF
C SYNOPSIS
struct Hwi.AINTC |
|
ARM Interrupt Controller
XDCscript usage |
meta-domain |
var obj = new Hwi.AINTC;
obj.FIQ0 = UInt32 ...
// 0x00 Interrupt Status of INT [31:0] if mapped to FIQ
obj.FIQ1 = UInt32 ...
// 0x04 Interrupt Status of INT [63:32] if mapped to FIQ
obj.IRQ0 = UInt32 ...
// 0x08 Interrupt Status of INT [31:0] if mapped to IRQ
obj.IRQ1 = UInt32 ...
// 0x0C Interrupt Status of INT [63:32] if mapped to IRQ
obj.FIQENTRY = UInt32 ...
// 0x10 Entry Address [28:0] for valid FIQ interrupt
obj.IRQENTRY = UInt32 ...
// 0x14 Entry Address [28:0] for valid IRQ interrupt
obj.EINT0 = UInt32 ...
// 0x18 Interrupt Enable Register 0
obj.EINT1 = UInt32 ...
// 0x1C Interrupt Enable Register 1
obj.INTCTL = UInt32 ...
// 0x20 Interrupt Operation Control Register
obj.EABASE = UInt32 ...
// 0x24 Interrupt Entry Base Address
obj.RES = UInt32[2] ...
// 0x28 reserved
obj.INTPR = UInt32[8] ...
// 0x30 Interrupt 0-7 Priority select
C SYNOPSIS
metaonly struct Hwi.BasicView |
|
XDCscript usage |
meta-domain |
var obj = new Hwi.BasicView;
obj.halHwiHandle = Ptr ...
obj.label = String ...
obj.intNum = Int ...
obj.priority = Int ...
obj.fxn = String ...
obj.arg = UArg ...
obj.irp = Ptr ...
obj.status = String ...
struct Hwi.HookSet |
|
Hwi hook set type definition
XDCscript usage |
meta-domain |
var obj = new Hwi.HookSet;
obj.registerFxn = Void(*)(Int) ...
DETAILS
The functions that make up a hookSet have certain restrictions. They
cannot call any Hwi instance functions other than Hwi_getHookContext()
and Hwi_setHookContext(). For all practical purposes, they should treat
the Hwi_Handle passed to these functions as an opaque handle.
C SYNOPSIS
metaonly struct Hwi.ModuleView |
|
XDCscript usage |
meta-domain |
var obj = new Hwi.ModuleView;
obj.options = String[4] ...
obj.hwiStackPeak = SizeT ...
obj.hwiStackSize = SizeT ...
obj.hwiStackBase = Ptr ...
config Hwi.E_alreadyDefined // module-wide |
|
Error raised when Hwi is already defined
XDCscript usage |
meta-domain |
msg: "E_alreadyDefined: Hwi already defined: intr# %d"
};
C SYNOPSIS
config Hwi.LD_end // module-wide |
|
Issued just after return from Hwi function (with interrupts disabled)
XDCscript usage |
meta-domain |
msg: "LD_end: hwi: 0x%x"
};
C SYNOPSIS
config Hwi.LM_begin // module-wide |
|
Issued just prior to Hwi function invocation (with interrupts disabled)
XDCscript usage |
meta-domain |
msg: "LM_begin: hwi: 0x%x, func: 0x%x, preThread: %d, intNum: %d, irp: 0x%x"
};
C SYNOPSIS
config Hwi.dispatcherAutoNestingSupport // module-wide |
|
Include interrupt nesting logic in interrupt dispatcher?
XDCscript usage |
meta-domain |
Hwi.dispatcherAutoNestingSupport = Bool true;
DETAILS
Default is true.
This option provides the user with the ability to optimize
interrupt dispatcher performance when support for interrupt
nesting is not required.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that manipulates interrupt mask
registers and enables and disables interrupts before and
after invoking the user's Hwi function.
Set this parameter to false if you don't need interrupts
enabled during the execution of your Hwi functions.
C SYNOPSIS
config Hwi.dispatcherIrpTrackingSupport // module-wide |
|
Controls whether the
dispatcher retains the interrupted thread's return address
XDCscript usage |
meta-domain |
Hwi.dispatcherIrpTrackingSupport = Bool true;
DETAILS
This option is enabled by default.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that keeps track of the interrupt's
return address and provide a small savings in interrupt latency.
The application can get an interrupt's most recent return
address using the
getIrp API.
C SYNOPSIS
config Hwi.dispatcherSwiSupport // module-wide |
|
Include Swi scheduling logic in interrupt dispatcher?
XDCscript usage |
meta-domain |
Hwi.dispatcherSwiSupport = Bool undefined;
DETAILS
Default is inherited from
BIOS.swiEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that Swis
will not be posted from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Swi scheduler
prior to returning from an interrupt.
C SYNOPSIS
config Hwi.dispatcherTaskSupport // module-wide |
|
Include Task scheduling logic in interrupt dispatcher?
XDCscript usage |
meta-domain |
Hwi.dispatcherTaskSupport = Bool undefined;
DETAILS
Default is inherited from
BIOS.taskEnabled, which is true by default.
This option provides the user with the ability to optimize
interrupt dispatcher performance when it is known that no
Task scheduling APIs (ie
Semaphore_post()) will be executed from any of their Hwi threads.
Setting this parameter to false will disable the logic in
the interrupt dispatcher that invokes the Task scheduler
prior to returning from an interrupt.
C SYNOPSIS
config Hwi.eabaseSize // module-wide |
|
EABASE Size Setting. Default is 4 bytes per entry.
Options are 4, 8, 16, 32 bytes per entry
XDCscript usage |
meta-domain |
Hwi.eabaseSize = Bits32 4;
C SYNOPSIS
config Hwi.fiqStack // module-wide |
|
FIQ stack pointer. Default = null.
(Indicates that stack is to be created using
staticPlace()
XDCscript usage |
meta-domain |
C SYNOPSIS
metaonly config Hwi.common$ // module-wide |
|
Common module configuration parameters
XDCscript usage |
meta-domain |
DETAILS
All modules have this configuration parameter. Its name
contains the '$' character to ensure it does not conflict with
configuration parameters declared by the module. This allows
new configuration parameters to be added in the future without
any chance of breaking existing modules.
metaonly config Hwi.dataAbortFunc // module-wide |
|
Data abort exception handler. Default is self loop
XDCscript usage |
meta-domain |
Hwi.dataAbortFunc = Void(*)(Void) undefined;
metaonly config Hwi.fiqFunc // module-wide |
|
FIQ interrupt handler. Default is internal FIQ dispatcher
XDCscript usage |
meta-domain |
Hwi.fiqFunc = Void(*)(Void) undefined;
metaonly config Hwi.fiqStackSection // module-wide |
|
Memory section used for FIQ stack
Default is null
XDCscript usage |
meta-domain |
Hwi.fiqStackSection = String null;
metaonly config Hwi.fiqStackSize // module-wide |
|
FIQ stack size in MAUs.
Default is 1024 bytes
XDCscript usage |
meta-domain |
Hwi.fiqStackSize = SizeT 1024;
metaonly config Hwi.irqFunc // module-wide |
|
IRQ interrupt handler. Default is internal IRQ dispatcher
XDCscript usage |
meta-domain |
Hwi.irqFunc = Void(*)(Void) undefined;
metaonly config Hwi.prefetchAbortFunc // module-wide |
|
Prefetch abort exception handler. Default is self loop
XDCscript usage |
meta-domain |
Hwi.prefetchAbortFunc = Void(*)(Void) undefined;
metaonly config Hwi.reservedFunc // module-wide |
|
Reserved exception handler. Default is self loop
XDCscript usage |
meta-domain |
Hwi.reservedFunc = Void(*)(Void) undefined;
metaonly config Hwi.resetFunc // module-wide |
|
Reset Handler. Default is c_int00
XDCscript usage |
meta-domain |
Hwi.resetFunc = Void(*)(Void) undefined;
metaonly config Hwi.rovViewInfo // module-wide |
|
XDCscript usage |
meta-domain |
metaonly config Hwi.swiFunc // module-wide |
|
SWI Handler. Default is internal SWI handler
XDCscript usage |
meta-domain |
Hwi.swiFunc = Void(*)(Void) undefined;
metaonly config Hwi.undefinedInstFunc // module-wide |
|
Undefined instruction exception handler. Default is self loop
XDCscript usage |
meta-domain |
Hwi.undefinedInstFunc = Void(*)(Void) undefined;
metaonly Hwi.addHookSet() // module-wide |
|
addHookSet is used in a config file to add a hook set (defined
by struct HookSet)
XDCscript usage |
meta-domain |
ARGUMENTS
hook
structure of type HookSet
DETAILS
HookSet structure elements may be omitted, in which case those
elements will not exist.
Instance Config Parameters |
|
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
// Instance config-params object
params.arg = UArg 0;
// ISR function argument. Default is 0
params.disableMask0 = Bits32 0;
// disableMask0. default is derived from MaskingOption_SELF maskSetting
params.disableMask1 = Bits32 0;
// disableMask1. default is derived from MaskingOption_SELF maskSetting
params.enableInt = Bool true;
// Enable this interrupt now? Default is true
params.eventId = Int -1;
// Interrupt event ID (Interrupt Selection Number)
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored
params.priority = Int 7;
// Interrupt priority (0-7). Default is 7 which is the
lowest priority IRQ interrupt
params.restoreMask0 = Bits32 0;
// restoreMask0. default is derived from MaskingOption_SELF maskSetting
params.restoreMask1 = Bits32 0;
// restoreMask1. default is derived from MaskingOption_SELF maskSetting
config Hwi.arg // instance |
|
ISR function argument. Default is 0
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.arg = UArg 0;
C SYNOPSIS
config Hwi.disableMask0 // instance |
|
disableMask0. default is derived from MaskingOption_SELF maskSetting
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.disableMask0 = Bits32 0;
C SYNOPSIS
config Hwi.disableMask1 // instance |
|
disableMask1. default is derived from MaskingOption_SELF maskSetting
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.disableMask1 = Bits32 0;
C SYNOPSIS
config Hwi.enableInt // instance |
|
Enable this interrupt now? Default is true
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.enableInt = Bool true;
C SYNOPSIS
config Hwi.eventId // instance |
|
Interrupt event ID (Interrupt Selection Number)
Default is -1.
Not all targets/devices support this instance parameter.
On those that don't, this parameter is ignored
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.eventId = Int -1;
C SYNOPSIS
config Hwi.maskSetting // instance |
|
maskSetting. Default is Hwi_MaskingOption_SELF
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
C SYNOPSIS
config Hwi.priority // instance |
|
Interrupt priority (0-7). Default is 7 which is the
lowest priority IRQ interrupt
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.priority = Int 7;
C SYNOPSIS
config Hwi.restoreMask0 // instance |
|
restoreMask0. default is derived from MaskingOption_SELF maskSetting
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.restoreMask0 = Bits32 0;
C SYNOPSIS
config Hwi.restoreMask1 // instance |
|
restoreMask1. default is derived from MaskingOption_SELF maskSetting
XDCscript usage |
meta-domain |
var params = new Hwi.Params;
...
params.restoreMask1 = Bits32 0;
C SYNOPSIS
Instance Creation |
|
XDCscript usage |
meta-domain |
// Allocate instance config-params
params.config = ...
// Assign individual configs
var inst = Hwi.create(Int intNum, Void(*)(UArg) hwiFxn, params);
// Create an instance-object
ARGUMENTS
intNum
interrupt number
hwiFxn
pointer to ISR function
params
per-instance config params, or NULL to select default values (target-domain only)
eb
active error-handling block, or NULL to select default policy (target-domain only)
DETAILS
A Hwi dispatcher table entry is created and filled with the
function specified by the fxn parameter and the attributes
specified by the params parameter.
If params is NULL, the Hwi's dispatcher properties are assigned a
default set of values. Otherwise, the following properties
are specified by a structure of type Hwi_Params.
- The arg element is a generic argument that is passed to the plugged
function as its only parameter. The default value is 0.
- The enableInt element determines whether the interrupt should be
enabled in the IER by create.
- The maskSetting element defines the dispatcherAutoNestingSupport
behavior of the interrupt.
Hwi_create returns a pointer to the created Hwi object.