Detailed Description
Defines the type system for DSP/BIOS Link.
============================================================================
- Path:
- /gpp/inc/usr/
- Version:
- 1.65.01.06 ============================================================================
- Copyright:
- Copyright (C) 2002-2009, Texas Instruments Incorporated - https://www.ti.com/
Redistribution and use in source and binary forms, with or without modification, are permitted provided that the following conditions are met:
* Redistributions of source code must retain the above copyright notice, this list of conditions and the following disclaimer.
* Redistributions in binary form must reproduce the above copyright notice, this list of conditions and the following disclaimer in the documentation and/or other materials provided with the distribution.
* Neither the name of Texas Instruments Incorporated nor the names of its contributors may be used to endorse or promote products derived from this software without specific prior written permission.
THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE. ============================================================================
Go to the source code of this file.
Defines |
#define | IN |
| Argument specification syntax ============================================================================.
|
#define | OUT |
#define | CONST const |
#define | USES(filename) |
| Empty macro to indicate header file dependency ============================================================================.
|
#define | Void void |
#define | FALSE 0u |
| Boolean constants ============================================================================.
|
#define | TRUE 1u |
#define | NULL ((void *)0) |
| Definition is language specific ============================================================================.
|
#define | NULL_CHAR '\0' |
| String terminator. ============================================================================.
|
#define | REG8(A) (*(volatile Char8 *) (A)) |
| Macros to access register fields. ============================================================================.
|
#define | REG16(A) (*(volatile Uint16 *) (A)) |
#define | REG32(A) (*(volatile Uint32 *) (A)) |
Typedefs |
typedef signed char | Int8 |
| Basic data types ============================================================================.
|
typedef signed short int | Int16 |
typedef signed long int | Int32 |
typedef unsigned char | Uint8 |
typedef unsigned short int | Uint16 |
typedef unsigned long int | Uint32 |
typedef float | Real32 |
typedef double | Real64 |
typedef short int | Bool |
typedef char | Char8 |
typedef short | Char16 |
typedef unsigned char | Uchar8 |
typedef unsigned short | Uchar16 |
typedef int | Int |
typedef void * | Pvoid |
typedef Char8 * | Pstr |
typedef Uchar8 * | Pustr |
typedef Uint32 | ProcessorId |
| These types are used across DSP/BIOS Link. ============================================================================.
|
typedef Uint32 | ChannelId |
PoolId |
This type is used for identifying the different pools used by DSPLINK. ============================================================================
============================================================================
|
#define | STATIC static |
| Free for OEMs to add their own generic stuff, if they so desire ============================================================================.
|
#define | EXTERN extern |
#define | NORMAL_API CDECL |
#define | IMPORT_API DLLIMPORT |
#define | EXPORT_API DLLEXPORT |
typedef Uint16 | PoolId |
Define Documentation
Argument specification syntax ============================================================================.
============================================================================
- Macro:
- IN/OUT/OPTIONAL/CONST
#define USES |
( |
|
filename ) |
|
Empty macro to indicate header file dependency ============================================================================.
============================================================================
- Macro:
- USES
Boolean constants ============================================================================.
============================================================================
- Constant:
- TRUE/FALSE
Definition is language specific ============================================================================.
============================================================================
- Constant:
- NULL
String terminator. ============================================================================.
============================================================================
- Constant:
- NULL_CHAR
#define REG8 |
( |
|
A ) |
(*(volatile Char8 *) (A)) |
Macros to access register fields. ============================================================================.
============================================================================
- Macro:
- REG8/REG16/REG32
#define REG16 |
( |
|
A ) |
(*(volatile Uint16 *) (A)) |
#define REG32 |
( |
|
A ) |
(*(volatile Uint32 *) (A)) |
Free for OEMs to add their own generic stuff, if they so desire ============================================================================.
============================================================================
- Macro:
- OS Specific standard definitions ============================================================================
- Macro:
- Calling convention
Definition of CDECL, DLLIMPORT, DLLEXPORT can be defined by OEM for his compiler ============================================================================
#define IMPORT_API DLLIMPORT |
#define EXPORT_API DLLEXPORT |
Typedef Documentation
Basic data types ============================================================================.
============================================================================
- Macro:
- Data types
typedef signed short int Int16 |
typedef signed long int Int32 |
typedef unsigned char Uint8 |
typedef unsigned short int Uint16 |
typedef unsigned long int Uint32 |
These types are used across DSP/BIOS Link. ============================================================================.
============================================================================
- Macro:
- DSP/BIOS Link specific types