Platform Support Package (PSP) Software Manifest
Legend
Package Name |
The name of the application or files |
Version |
Version of the application or files |
License |
Name of the license or licenses that apply to the Package. |
Location |
The directory name and path on the media (or in an archive) where the Package is located. |
Delivered As |
This field will either be “Source”, “Binary” or “Source and Binary” and is the form the content of the Package is delivered in. If the Package is delivered in an archive format, this field applies to the contents of the archive. If the word Limited is used with Source, as in “Limited Source” or “Limited Source and Binary” then only portions of the Source for the application are provided. |
Modified |
This field will either be “Yes” or “No”. A “Yes” means TI had made changes to the Package. A “No” means TI has not made any changes. |
This field specifies where TI obtained the Package from. It may be a URL to an Open Source site, a 3rd party company name or TI. If this field contains a link to an Open Source package, the date it was downloaded is also recorded. |
Manifest
Note:
Replace MM.mm.pp.bb in the
directory path
below with the PSP release version you are using. Wherever
component versions are different(as indicated by X.X.X.X)
replace
with the appropriate version from "Version" column.
Package
Name |
Version |
License |
Delivered
As |
Modified |
|
|
Open
Source Linux (based on linux-omap GIT)
|
2.6.32 |
GPLv2 |
Source
and Binary |
YES |
Location |
Source
at
AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/src/kernel/linux-MM.mm.pp.bb.tar.gz. AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/images/kernel/am3517/uImage |
Obtained
from[1] |
Kernel 2.6.32 from linux-omap pm branch (commit 3fd5969a81a9324b58a1c19cf510c0da97c99565) |
|||||
Bootstrapper (x-loader) |
1.45 | GPLv2 | Source and Binary | Yes | Location | Source
at AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/src/boot-strap/x-loader-MM.mm.pp.bb.tar.gz Binary at AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/images/boot-strap/omap3530/x-load.bin.ift AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/images/boot-strap/am3517/x-load.bin.ift |
Obtained from[1] | Derived from U-boot project. | |||||
Linux Functional Testbench(LFTB) | 01.00.00.14 | BSD | Source and Binary | Yes | Location | AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/test-suite/lftb-X.X.X.X.tar.gz |
Obtained from[1] | TI | |||||
U-Boot |
|
GPLv2 |
Source
and Binary |
YES |
Location |
Source
at AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/src/u-boot/u-boot-MM.mm.pp.bb.tar.gz AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/images/u-boot/am3517/u-boot.bin. |
Obtained
from[1] |
U-Boot 2009.11 from u-boot ( commit v2009.11 ). |
|||||
Sample
Code(video, audio) |
NA |
BSD |
Source |
NA |
Location |
AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/src/examples/examples.tar.gz |
Obtained
from[1] |
TI |
|||||
Image Signing Utility |
NA |
BSD |
Source and Binary |
NA |
Location |
Source at AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/host-tools/src/signGP.c Binary at AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/host-tools/linux/signGP |
Obtained
from[1] |
TI |
|||||
Target
Filesystem |
NA |
Various (see filesystem
Manifest)
|
Binary |
NA |
Location |
Information
on source available in filesystem
Manifest |
Obtained
from[1] |
Various (see filesystem Manifest) |
|||||
[1] Any links appearing on this manifest were verified at the time it was created. TI makes no guarantee that they will remain active in the future.