Platform Support Package (PSP) Software Manifest


Legend

Package Name

The name of the application or files

Version

Version of the application or files

License

Name of the license or licenses that apply to the Package.

Location

The directory name and path on the media (or in an archive) where the Package is located.

Delivered As

This field will either be “Source”, “Binary” or “Source and Binary” and is the form the content of the Package is delivered in.  If the Package is delivered in an archive format, this field applies to the contents of the archive. If the word Limited is used with Source, as in “Limited Source” or “Limited Source and Binary” then only portions of the Source for the application are provided.

Modified

This field will either be “Yes” or “No”. A “Yes” means TI had made changes to the Package. A “No” means TI has not made any changes.

Obtained from[1]

This field specifies where TI obtained the Package from. It may be a URL to an Open Source site, a 3rd party company name or TI. If this field contains a link to an Open Source package, the date it was downloaded is also recorded.

  

Manifest

Note: Replace MM.mm.pp.bb in the directory path below with the PSP release version you are using.  Wherever component versions are different(as indicated by  X.X.X.X) replace with the appropriate version from "Version" column.

Package Name

Version

License

Delivered As

Modified

 

Open Source Linux (based on linux-omap GIT)  

 2.6.32

 GPLv2

Source and Binary

YES

Location

Source at AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/src/kernel/linux-MM.mm.pp.bb.tar.gz.
Compiled binary at AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/images/kernel/omap3530/uImage

AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/images/kernel/am3517/uImage

Obtained from[1]

Kernel 2.6.32 from linux-omap pm branch (commit 3fd5969a81a9324b58a1c19cf510c0da97c99565)

Bootstrapper
(x-loader)
1.45 GPLv2 Source and Binary Yes Location Source at AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/src/boot-strap/x-loader-MM.mm.pp.bb.tar.gz
Binary at AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/images/boot-strap/omap3530/x-load.bin.ift
AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/images/boot-strap/am3517/x-load.bin.ift
Obtained from[1] Derived from U-boot  project.
Linux Functional Testbench(LFTB) 01.00.00.14   BSD Source and Binary Yes Location AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/test-suite/lftb-X.X.X.X.tar.gz
Obtained from[1] TI

 U-Boot  

2009.11

 GPLv2

Source and Binary

YES

Location

Source at AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/src/u-boot/u-boot-MM.mm.pp.bb.tar.gz
Binary at AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/images/u-boot/omap3530/u-boot.bin

AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/images/u-boot/am3517/u-boot.bin.

Obtained from[1]

U-Boot 2009.11  from u-boot ( commit v2009.11 ).

Sample Code(video, audio)

 NA

  BSD

Source

NA

Location

AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/src/examples/examples.tar.gz

Obtained from[1]

TI

Image Signing Utility

 NA

 BSD

Source and  Binary

NA

Location

Source at AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/host-tools/src/signGP.c    

Binary at AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/host-tools/linux/signGP

Obtained from[1]

TI

Target  Filesystem

NA

Various (see filesystem Manifest)

Binary

NA

Location

Information on source available in filesystem Manifest
Binaries at  AM35x-OMAP35x-PSP-SDK-MM.mm.pp.bb/images/fs

Obtained from[1]

Various (see filesystem Manifest)

 


[1] Any links appearing on this manifest were verified at the time it was created. TI makes no guarantee that they will remain active in the future.