Update Information
A Chip Support Package adds support for a new device to
Code Composer Studio. A Chip Support Package may
require a minimum Service Release to be installed, this will
be noted in the description. If
you are using a 3rd Party emulator please check the
company's website to obtain the appropriate drivers.
We will indicate in description below if there is a change
introduced that requires a 3rd Party driver update (remember to check
see if service release required an update).
The
release notes will provide the complete listing of the bugs
addressed in each service release. Links to previous service releases are provided, however it
is recommended that you install the latest service release.
Important Note: Some
new devices may require updates to DSP/BIOS or the Code
Generation tools in addition to the Code Composer Studio
service release. These Updates are also available from
the Update Advisor and will be indicated below.
| Chip Support
Packages |
|
F2803x
(Piccolo with Flash Plugin support) |
2-12-2010 |
This
CSP improves support for the flashing of F2803x
devices() to CCS versions that already include support
for F2803x devices. It also includes some updates for
the F2802x devices. This CSP could be applied to the Image
Update (CCS 3.3.83.19), or CCS3.3 RTM + SR-12 (CCS
3.3.82.13) + F2803x CSP.
|
|
DM365 |
11-13-2010 |
Adds support
for DM365. Service Release 12 or higher is required. Click
here to access Service Releases.
|
|
C6457 |
03-31-2009 |
Adds support
for C6457.
|
|
Jacinto
DDR |
03-25-2009 |
Adds support
for Jacinto DDR.
|
|
F2803x
(Piccolo) |
03-20-2009 |
This
CSP adds support for F2803x devices () to CCS3.3
RTM+SR-12 (CCS 3.3.82.13). It is already included in the Image Update (CCS 3.3.83.19), so no need
to apply it to this release.
|
|
Delfino |
02-24-2009 |
Adds support
for Delfino. Service Release 12 or higher is required. Click
here to access Service Releases.
|
|
DM357 |
01-23-2009 |
Adds support
for DM357 emulators. Service Release 11 or higher is required. Click
here to access Service Releases.
|
|
F2823x RevA (Updated) |
10-30-2008 |
Adds support for F2823x and F2833x Rev A silicon.
This CSP was updated to resolve install problems with
the F2823x CSP that was released on 4-22-2008.
Service Release 8 or higher is required. Click
here to access Service Releases.
F283xx users will need to download an updated C2000
compiler. |
|
C6474 |
10-14-2008 |
Adds support
for C6474. Service Release 10 or higher is required. Click
here to access Service Releases.
|
|
TCI6484 (Updated) |
10-08-2008 |
Adds support
for TCI6484. Service Release 10 or higher is required. Click
here to access Service Releases.
|
|
C674x |
10-02-2008 |
Adds support
for C6747, C6745, and OMAP-L137. Service Release 10 or higher is required. Click
here to access Service Releases.
|
|
OMAP35xx |
04-24-2008 |
Adds support for OMAP3530, OMAP3525,
OMAP3515 and OMAP3503.
Service Release 8 or higher is required. Click
here to access Service Releases. |
|
F2823x |
04-22-2008
Release Notes |
Adds support for F28232, F28234 and F28235.
Service Release 8 or higher is required. Click
here to access Service Releases.
F283xx users will need to download an updated C2000
compiler. |
|
DM6467 |
10-22-2007 |
Adds support for DM6467.
Service Release 6 or higher is required. Click
here to access Service Releases. |
|
Trace
Patches |
|
Trace Patch
v1.1.0R3.6 |
10-22-2008 |
This patch fixes big endian
trace decode issues for C64x+ and ETB receiver when
running DSP at full speed/over-clocking was generating
bad data.
Service Release 11 or higher is required. Click
here to access Service Releases. |
|
Trace Patch
v1.1.0R3.5 |
08-21-2008
Release Notes |
Trace decoder patch to fix
problem decoding compressed instructions from a big
endian .out file. This patch requires Service Release 9
or higher to be installed first. |
For additional information, contact support@ti.com
|