| XDS family | XDS100v1 | XDS100v2 | XDS100v3 | XDS110 | XDS200 | XDS510 | XDS560 | XDS560 Rev D cable | XDS560T | XDS560v2 System Trace | XDS560v2 Pro Trace | |
|---|---|---|---|---|---|---|---|---|---|---|---|---|
| Feature1 | ||||||||||||
| Header Type / Pins | 14-pin TI 20-pin TI |
14-pin TI 20-pin TI 20-pin ARM |
14-pin TI 20-pin TI 20-pin ARM |
20-pin TI | 20-pin TI | 14-pin TI 20-pin TI |
14-pin TI 20-pin TI |
20-pin TI | 60-pin TI | 60-pin MIPI HPST | 60-pin MIPI HPST | |
| Adaptive JTAG Clocking2 | N/A | Y | Y | N/A | Y | Y5 | Y5 | Y | Y | Y | Y | |
| Core Pin Trace3 | N/A | N/A | N/A | N/A | N/A | N/A | N/A | Y (DSP Only) | N/A | N/A | Y | |
| System Pin Trace3 | N/A | N/A | N/A | N/A | N/A | N/A | N/A | N/A | N/A | Y | Y | |
| SWD debug with SWO Trace | N/A | N/A | N/A | Y | Y | N/A | N/A | N/A | N/A | N/A | N/A | |
| IEEE1149.7 (cJTAG) | N/A | N/A | Y | Y | Y | N/A | N/A | N/A | N/A | Y | Y | |
| Target Voltage Reference (TVRef) | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | |
| System Reset (nReset) | Y4 | Y4 | N/A | Y | Y | Y4 | Y4 | Y | N/A | Y | Y | |
| Emulation Boot Modes | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | Y | |
| HS-RTDX | N/A | N/A | N/A | N/A | N/A | N/A | Y | Y | N/A | N/A | N/A | |
| PIN | XDS Signal Type(1) | Target Signal Type | Name | Description |
|---|---|---|---|---|
| nTRST | O | I | Test Logic Reset | When asserted (low active) causes all test and debug logic in the device to be reset along with the IEEE 1149.1 TAP. |
| TCK | O | I | Test Clock | This is the test clock used to drive an IEEE 1149.1 TAP state machine and logic. Depending on the XDS attached, this is either a free running clock or a gated clock that requires RTCK monitoring.(2) |
| TMS | O | I | Test Mode Select | Directs the next state of the IEEE 1149.1 TAP state machine |
| TDI | O | I | Test Data Input | IEEE 1149.1 Scan data input to the device |
| TDO | I | O | Test Data Output | IEEE 1149.1 Scan data output of the device |
| RTCK(5) | I | O(4) | TCK Return | Depending on the XDS attached the JTAG signals are clocked out with RTCK(3). An XDS that supports adaptive clocking monitors RTCK to determine when to gate TCK. |
| PIN | XDS Signal Type | Target Signal Type | NAME | DESCRIPTION |
|---|---|---|---|---|
| TVRef(2) | I | O | Target Voltage Reference | Should be tied to the I/O voltage of the target device. Used to detect if power is active and to set JTAG signal voltage level translators if supported by the XDS(1). |
| TDIS | I | O | Target Disconnect | XDS that support this signal can detect the difference between a powered-down target and when the target cable is not physically connected. |
| | I/O(1) | | I/O | Emulation Port | Depending on your device and XDS, EMU pins support boot modes, cross triggers, HS-RTDX, Core Trace and System Trace. See your XDS user's guide and device data sheet for supported features. | |
| nRESET(3) | O | I | Target Reset | This is an optional signal that if integrated into your applications power-up-reset circuit may be used to remotely reset the target board from a debugger. |