Tests
TI Zephyr test suites live under tests/ and are run with
Twister,
Zephyr’s standard test runner. Only the tests that apply to AM13 are
listed.
Test Structure
Tests follow the same structure as upstream Zephyr tests:
tests/
└── <subsystem>/
└── <test_name>/
├── src/
│ └── main.c
├── CMakeLists.txt
├── prj.conf
└── testcase.yaml
The testcase.yaml file defines one or more test scenarios, board filters,
and harness configuration. See the
Zephyr testcase.yaml reference
for the full schema. Samples use sample.yaml instead; Twister in this
Zephyr version only discovers tests by those two file names.
Running Tests with Twister
Zephyr’s west twister picks up the tests, samples and applications of this
repository when -T points at it: twister scans the given path recursively
for testcase.yaml and sample.yaml files. Run the commands below from the
zephyr directory of the west workspace, where ../ti-zephyr is the
path to this repository.
Run all TI Zephyr tests, samples and applications on a specific board (see the AM13 board support page for the board IDs):
west twister -T ../ti-zephyr -p <board>
Build only, without flashing or running on hardware:
west twister -T ../ti-zephyr -p <board> --build-only
Run a single test or sample by its directory:
west twister -T ../ti-zephyr/tests/<subsystem>/<test_name> -p <board>
west twister -T ../ti-zephyr/samples/<subsystem>/<sample_name> -p <board>
A test can also be selected by scenario name instead of path
(west twister -T ../ti-zephyr --list-tests shows the names):
west twister -T ../ti-zephyr -s <scenario> -p <board>
Filter by tag:
west twister -T ../ti-zephyr --tag drivers -p <board>
Save the selected tests as a test plan and run it later:
west twister -T ../ti-zephyr -p <board> --save-tests plan.json
west twister --load-tests plan.json
Building and Running Applications
The reference applications under applications/ are fully operational and
are handled by twister like any other sample. Each application has a
sample.yaml that defines an application.<name> scenario, so the
commands above already include them.
Build and run all applications for a board:
west twister -T ../ti-zephyr/applications -p <board>
Build and run a single application:
west twister -T ../ti-zephyr/applications/<application> -p <board>
Add --build-only to build without flashing or running on hardware. To
flash and run on a connected board, use twister’s device testing options
(--device-testing with a hardware map), or build the application and flash
it directly with west flash.
The applications set harness: none in their sample.yaml, so they have
no console output check. Verify their behavior on the board itself, for
example the display and touch response.
Applications that need a shield, which supplies the display and touch
devicetree nodes, set it in the extra_args of their sample.yaml, for
example extra_args: SHIELD=<shield>. Twister has no command-line option
for shields. The build output is written to the twister-out directory,
or to the directory given with --outdir. See the README.rst of each
application for the supported board, wiring and how to flash it.