OTP Keywriter TISCI Description¶
This chapter provides information on TISCI message for programming customer keys into eFuse array on K3 devices.
| TISCI Message ID | Message Name |
|---|---|
| 0x9031 | TISCI_MSG_KEY_WRITER |
This document must be read alongside Key Writer
API Description¶
TISCI_MSG_KEY_WRITER - Key writer¶
Usage¶
| Message Type | Secure |
| Secure Queue Only? | Yes |
TISCI Message ID¶
TISCI_MSG_KEY_WRITER (0x9031U)
struct tisci_msg_keywriter_req
Request message for keywriter
| Parameter | Type | Description |
|---|---|---|
| hdr | struct tisci_header | standard TISCI header |
| image_addr_lo | u32 | Lower 32 bit address (in LE format) of the certificate |
| image_addr_hi | u32 | Higher 32 bit address (in LE format) of the certificate |
| key_prog_mask | u32 | Reserved for future use |
Address of the certificate containing customer key information is given as input to the API.
struct tisci_msg_keywriter_resp
Response message for keywriter
| Parameter | Type | Description |
|---|---|---|
| hdr | struct tisci_header | standard TISCI header |
| debug_response | u32 | debug code for success/failure |
A debug_response of 0x0 means the key programming was successful, other
response codes indicate the point of failure, which can be referred from PDK documentation
for OTP Keywriter.