Security X509 Certificate Documentation¶
Introduction¶
This document describes the X509 extensions supported by the X509 parser in System Firmware.
Note
This document is only applicable to HS devices. System Firmware does not include a X509 parser on GP devices.
References¶
- ISO 8824-1 | ITU-T X.680 (08/2015): Information technology - Abstract Syntax Notation One (ASN.1): Specification of basic notation, http://handle.itu.int/11.1002/1000/12479
- ISO 8825-1 | ITU-T X.690 (09/2015): Information technology - ASN.1 encoding rules: Specification of Basic Encoding Rules (BER), Canonical Encoding Rules (CER) and Distinguished Encoding Rules (DER) http://handle.itu.int/11.1002/1000/12483
- ISO/IEC 9594-8 | ITU-T X.509 (10/2016): Information technology - Open Systems Interconnection - The Directory: Public-key and attribute certificate frameworks http://handle.itu.int/11.1002/1000/13031
- Processor Boot Management TISCI Description
Extensions¶
The following X509 extensions are supported by System Firmware.
| Extension Name | Purpose |
|---|---|
| System Firmware Boot Extension | Provide boot information |
| System Firmware Image Integrity Extension | Image hash and length |
| System Firmware Software Revision Extension | revision of binary for anti-rollback |
| System Firmware Load Extension | Provide load information |
| System Firmware Debug Extension | To unlock debug port |
| System Firmware Encryption Extension | Encryption extension |
| System Firmware HS Board Configuration Extension | HS Boardcfg extension |
System Firmware Boot Extension¶
This extension adds support for booting various cores on a K3 SOC. It is identified by the OID 1.3.6.1.4.1.294.1.33. The structure of the field is shown below in ASN.1 notation.
SYSFW-Boot := SEQUENCE
{
bootCore INTEGER, -- indicates the core in the device that needs to be booted
-- with the image accompanying this certificate.
configFlags_set INTEGER, -- Configuration options for the core being booted.
-- flags to set
configFlags_clr INTEGER, -- Configuration options for the core being booted
-- flags to clear
resetVec OCTET STRING, -- Location of reset vector for the core.
fieldValid INTEGER -- indicates which of the reserved fields in the extension are
-- valid
rsvd1 INTEGER, -- reserved field for future use
rsvd2 INTEGER, -- reserved field for future use
rsvd3 INTEGER, -- reserved field for future use
}
The boot extension is decoded into the below structure.
struct sec_boot_ctrl {
u32 bootCore;
u32 configFlags_set;
u32 configFlags_clr;
u64 resetVec;
}
The reserved fields are for future use and are not decoded currently.
Populating the certificate fields¶
For an example, please refer to the section [ sysfw_boot_seq ] in Sample x509 template.
bootCoreshould be initialized to the Core ID of the targeted core. Core ID should be obtained from the SOC data. e.g. For booting a core with ID0x20, the relevant line in the X509 template is[ boot_seq ] bootCore = INTEGER:0x20
configFlags_set
- This is a 32 bit field that indicates core specific flags that need to be set before booting the core. The representation is big endian.
configFlags_clr
- This is a 32 bit field that indicates core specific flags that need to be cleared before booting core. The representation is big endian.
Please refer to the SOC and core specific documentation on the supported flags. The flags are passed to set_processor_config API as is. Please ensure that the flags set or cleared are valid according to the API.
resetVec
- This is a 64 bit field indicating the address of the reset vector that needs to be programmed. The representation is big endian.
System Firmware Image Integrity Extension¶
This extension adds support for specifying a hash and size of the accompanying payload. It is identified by the OID 1.3.6.1.4.1.294.1.34. The structure of the field is shown below in ASN.1 notation.
SYSFW-INTEGRITY := SEQUENCE
{
shaType OID, -- indicates OID of the hash used. Must always be set to SHA2-512
-- OID:2.16.840.1.101.3.4.2.3
shaValue OCTET STRING, -- SHA2-512 value of the payload
imageSize INTEGER, -- Size of the image in bytes. This will be amount of data
-- used when checking the image integrity, copying the image
-- to its destination or when decrypting the image.
}
System Firmware Software Revision Extension¶
System Firmware reuses the Software Revision extension/OID as defined by ROM as no additional information is required. This is identified by OID 1.3.6.1.4.1.294.1.3.
SYSFW-SWREV:= SEQUENCE
{
swrev INTEGER -- 32 bit value indicating the revision of the binary
}
System Firmware Load Extension¶
System Firmware uses the Load extension to determine where the image is loaded as part of authentication. The load extension is identified by OID 1.3.6.1.4.1.294.1.35. This is a new extension defined by System Firmware.
SYSFW-LOAD := SEQUENCE
{
destAddr OCTET STRING, -- Address to which the image accompanying this certificate
-- needs to be copied.
auth_in_place INTEGER -- Controls if/how the authenticated binary is copied to a different
-- location. See below for more information.
}
The load extension is decoded into the below structure.
struct ti_load_info {
u64 destAddr;
u8 auth_in_place;
};
Populating the certificate fields¶
destAddr- This is a 64 bit field indicating the address to which the data needs to be copied. The representation is big endian.
auth_in_placeThis is an integer field used to indicate whether the binary should be copied to the specified load address during authentication. The valid values for this field and their interpretation are described below.
Value Action 0 Normal operation. Binary is copied to load address. 1 In place operation. Binary is not moved. 2 In place operation variant. Binary is moved to the beginning of the buffer i.e. binary now starts at the location where the certificate started Any other value invalid operation
System Firmware Encryption Extension¶
System Firmware reuses the Encryption extension/OID as defined by ROM as no additional information is required. This is identified by OID 1.3.6.1.4.1.294.1.4.
SYSFW-ENCRYPT := SEQUENCE
{
initalVector OCTET STRING,
randomString OCTET STRING,
iterationCnt INTEGER,
salt OCTET STRING
}
The encryption extension is decoded into the following data structure.
struct ti_enc_info {
u8 initialVector[16];
u8 randomString[32];
u8 iterationCnt;
u8 salt[32];
};
Populating the certificate fields¶
initialVector- This is the 16 byte initialization vector to be used in AES-CBC decryption.
randomString- This field indicates the random 32 byte string that was appended to the
binary before encrypting the combined binary. System Firmware will compare the last
32 bytes of the decryption output against the
randomStringfield from the X509 certificate to verify the success of decryption operation.
- This field indicates the random 32 byte string that was appended to the
binary before encrypting the combined binary. System Firmware will compare the last
32 bytes of the decryption output against the
iterationCnt- This field is reserved and must be initialized to zero.
salt- This field is 32 bytes long. It is reserved and must be initialized to zero.
Note
System Firmware always loads the binary to the location specified by System Firmware Load Extension before performing in-place decryption at the loaded location.
System Firmware Debug Extension¶
Note
This extension is not yet finalized.
The custom extension field used for debug control is identified by the OID 1.3.6.1.4.1.294.1.8. The structure of the field is shown below in ASN.1 notation.
UID-Debug ::= SEQUENCE
{
uid OCTET STRING, -- unique ID of the device for which this certificate applies
debugCtrl INTEGER, -- debug control information
coreDbgEn INTEGER, -- Core IDs for which debug must be enabled
coreDbgSecEn INTEGER, -- Core IDs for which secure debug must be enabled
}
The debug control data is decoded as a structure below:
struct sdbg_debug_ctrl {
u16 debug_priv_level;
u16 reserved;
u8 debug_core_sel[MAX_CPU_CORES];
u8 sec_debug_core_sel[MAX_CPU_CORES];
}
The table below shows the way UID-Debug fields are decoded into struct sdbg_debug_ctrl.
| sdbg_debug_ctrl member | X.509 certificate debug extension field |
|---|---|
| debug_priv_level | debugCtrl field is decoded as a u32 value and the lower 16 bit value is picked up |
| reserved | debugCtrl field is decoded as a u32 value and the upper 16 bit value is picked up |
| debug_core_sel | coreDbgEn field is decoded as an array of u8 values of processor IDs for which non-secure debug should be enabled |
| sec_debug_core_sel | coreDbgSecEn field is decoded as an array of u8 values of processor IDs for which secure debug should be enabled |
The following table shows the enumeration of values for debug_priv_level:
| Enumeration name | Value | Meaning |
|---|---|---|
| DEBUG_DISABLE | 0 | Disable debug |
| DEBUG_PRESERVE | 1 | Preserve current setting by locking registers |
| DEBUG_PUBLIC | 2 | Enable debug at public (non-secure) user and privileged level |
| DEBUG_PUBLIC_USER | 3 | Enable debug at public (non-secure) user level only |
| DEBUG_FULL | 4 | Enable full debug (both secure and non-secure privileged and user levels) |
| DEBUG_SECURE_USER | 5 | Enable debug for both secure and non-secure at user level only |
For an example, please refer to the section [ debug ] in Sample x509 template.
System Firmware HS Board Configuration Extension¶
System Firmware extends the Encryption extension/OID as defined by ROM for the purpose of authenticating the board configurations on HS devices. The hashes of the 4 board configuration blobs
- Core board configuration
- PM board configurations
- RM board configuration
- Encrypted Security board configuration
and the encryption parameters of the security board configuration are encoded in the board configuration extension of the System Firmware outer certificate . This extension is identified by OID 1.3.6.1.4.1.294.1.36.
SYSFW-HS-BCFG:= SEQUENCE
{
initalVector OCTET STRING,
randomString OCTET STRING,
iterationCnt INTEGER,
salt OCTET STRING,
secBoardCfgHash OCTET STRING,
secBoardCfgVer INTEGER,
pmBoardCfgHash OCTET STRING,
rmBoardCfgHash OCTET STRING
boardCfgHash OCTET STRING
}
The extension is decoded into the following data structure.
struct ti_bcfg_info {
u8 initialVector[16];
u8 randomString[32];
u8 iterationCnt;
u8 salt[32];
u8 secBoardCfgHash[64];
u8 secBoardCfgVer;
u8 pmBoardCfgHash[64];
u8 rmBoardCfgHash[64];
u8 boardCfgHash[64];
};
Populating the certificate fields¶
initialVector- This is the 16 byte initialization vector to be used in AES-CBC decryption.
randomString- This field indicates the random 32 byte string that was appended to the
board configuration binary before encrypting the combined binary. System Firmware
will compare the last 32 bytes of the decryption output against the
randomStringfield from the X509 certificate to verify the success of decryption operation.
- This field indicates the random 32 byte string that was appended to the
board configuration binary before encrypting the combined binary. System Firmware
will compare the last 32 bytes of the decryption output against the
iterationCnt- This field is reserved and must be initialized to zero.
salt- This field is 32 bytes long. It is reserved and must be initialized to zero.
secBoardCfgHash- This is a 64 byte field containing the SHA2-512 hash of the encrypted security board configuration.
secBoardCfgVer- This field indicates the version of security board configuration and must be initialized to zero.
pmBoardCfgHash- This is a 64 byte field containing the SHA2-512 hash of the PM board configuration.
rmBoardCfgHash- This is a 64 byte field containing the SHA2-512 hash of the RM board configuration.
boardCfgHash- This is a 64 byte field containing the SHA2-512 hash of the main board configuration structure.
Sample x509 template¶
Note
The template below shows all the X509 extensions supported by the System Firmware ASN1 parser. Depending on the usecase, the certificate may contain only a few of these extensions.
- For performing JTAG unlock, only Software revision (
swrv) and Debug(debug) extensions are required. - For authenticating a binary, only the Load (
sysfw_image_load) and Image integrity (sysfw_image_integrity) extensions are required.
Note
The data in the req_distinguished_name section is random to indicates
- System Firmware does not process the information in the section.
- This needs to be updated by the user to reflect his information.
[ req ]
distinguished_name = req_distinguished_name
x509_extensions = v3_ca
prompt = no
dirstring_type = nobmp
# This information will be filled by the end user.
# The current data is only a place holder.
# System firmware does not make decisions based
# on the contents of this distinguished name block.
[ req_distinguished_name ]
C = oR
ST = rx
L = gQE843yQV0sag
O = dqhGYAQ2Y4gFfCq0t1yABCYxex9eAxt71f
OU = a87RB35W
CN = x0FSqGTPWbGpuiV
emailAddress = kFp5uGcgWXxcfxi@vsHs9C9qQWGrBs.com
[ v3_ca ]
basicConstraints = CA:true
1.3.6.1.4.1.294.1.3=ASN1:SEQUENCE:swrv
1.3.6.1.4.1.294.1.4=ASN1:SEQUENCE:encryption
1.3.6.1.4.1.294.1.8=ASN1:SEQUENCE:debug
1.3.6.1.4.1.294.1.36=ASN1:SEQUENCE:sysfw_hs_boardcfg
1.3.6.1.4.1.294.1.33=ASN1:SEQUENCE:sysfw_boot_seq
1.3.6.1.4.1.294.1.34=ASN1:SEQUENCE:sysfw_image_integrity
1.3.6.1.4.1.294.1.35=ASN1:SEQUENCE:sysfw_image_load
1.3.6.1.4.1.294.1.36=ASN1:SEQUENCE:sysfw_hs_boardcfg
[ sysfw_boot_seq ]
bootCore = INTEGER:0x20
bootCoreOpts_set = INTEGER:0x00000000
bootCoreOpts_clr = INTEGER:0x00000000
resetVec = FORMAT:HEX,OCT:41c02100
flagsValid = INTEGER:0x00
rsvd1 = INTEGER:0x00
rsdv2 = INTEGER:0x00
rsdv3 = INTEGER:0x00
[ sysfw_image_integrity ]
shaType = OID:2.16.840.1.101.3.4.2.3
shaValue = FORMAT:HEX,OCT:TEST_IMAGE_SHA512
# Replace TEST_IMAGE_LENGTH with actual image length
imageSize = INTEGER:TEST_IMAGE_LENGTH
[ sysfw_image_load ]
destAddr = FORMAT:HEX,OCT:41c02100
authInPlace = INTEGER:0
[ swrv ]
swrv = INTEGER:0
[ debug ]
debugUID = FORMAT:HEX,OCT:0000000000000000000000000000000000000000000000000000000000000000
debugType = INTEGER:0x00000004
coreDbgEn = INTEGER:0x20210102
coreDbgSecEn = INTEGER:0x2223
[ encryption ]
initalVector = FORMAT:HEX,OCT:TEST_IMAGE_ENC_IV
randomString = FORMAT:HEX,OCT:TEST_IMAGE_ENC_RS
iterationCnt = INTEGER:TEST_IMAGE_KEY_DERIVE_INDEX
salt = FORMAT:HEX,OCT:TEST_IMAGE_KEY_DERIVE_SALT
[ sysfw_hs_boardcfg ]
initalVector = FORMAT:HEX,OCT:SEC_BCFG_ENC_IV
randomString = FORMAT:HEX,OCT:SEC_BCFG_ENC_RS
iterationCnt = INTEGER:SEC_BCFG_KEY_DERIVE_INDEX
salt = FORMAT:HEX,OCT:SEC_BCFG_KEY_DERIVE_SALT
secBoardcfgHash = FORMAT:HEX,OCT:SEC_BCFG_HASH
secBoardcfgVer = INTEGER:SEC_BCFG_VER
pmBoardcfgHash = FORMAT:HEX,OCT:PM_BCFG_HASH
rmBoardcfgHash = FORMAT:HEX,OCT:RM_BCFG_HASH
boardcfgHash = FORMAT:HEX,OCT:BCFG_HASH