Resource Management Proxy TISCI Message Description¶
Introduction¶
This chapter provides information on usage of the RM Proxy management TISCI message API parameters.
| TISCI Message ID | Message Name | 
|---|---|
| 0x1300 | TISCI_MSG_RM_PROXY_CFG | 
| N/A | TISCI_MSG_RM_PROXY_CFG Response | 
Proxy Valid Parameters Field Usage¶
Some proxy TISCI message APIs make use of a valid_params bit field. Bits within the valid_params field define whether or not individual TISCI message parameters are valid. When a bit corresponding to a parameter is set (to 1) the parameter is considered valid and will be programmed into its corresponding register field, assuming validation of the parameter passes. When a valid_params bit is not set, i.e. a value of 0, the corresponding register field is read and used within the validation process of the request. The register field for a parameter is not programmed if the corresponding valid_params bit is not set.
TISCI_MSG_RM_PROXY_CFG - Proxy Configuration¶
Proxy Configuration Request¶
The proxy_cfg TISCI message API is used to configure the channelized firewalls of a Navigator Subsystem proxy. The proxy index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list. The channelized firewalls covering the proxy error events are configured to only give DMSC write access. The proxy target data control region channelized firewalls are configured to give the assigned host read and write access.
Usage¶
| Message Type | Normal | 
| Secure Queue Only? | No | 
TISCI Message ID¶
TISCI_MSG_RM_PROXY_CFG          (0x1300U)
RM TISCI message to setup a Navigator Subsystem proxy for configuration
Proxy Configuration Message Parameters¶
struct tisci_msg_rm_proxy_cfg_req
Configures a Navigator Subsystem proxy
| Parameter | Type | Description | 
|---|---|---|
| hdr | struct tisci_header | Standard TISCI header | 
| valid_params | u32 | Bitfield defining validity of proxy configuration parameters. This field is unused at the moment but exists if expansion of the API is needed in the future. | 
| nav_id | u16 | SoC device ID of Navigator Subsystem where proxy is located | 
| index | u16 | Proxy index. | 
Configures the channelized firewalls of a Navigator Subsystem proxy. The firewalls are configured to all the header host access to the backing RAM and target data configuration registers. The proxy index must be assigned to the host defined in the TISCI header via the RM board configuration resource assignment range list.
Proxy Configuration Response¶
The proxy_cfg_response message returns the result status of the processed proxy_cfg message.
Proxy Configuration Response Message Parameters¶
struct tisci_msg_rm_proxy_cfg_resp
Response to configuring a proxy.
| Parameter | Type | Description | 
|---|---|---|
| hdr | struct tisci_header | Standard TISCI header |