Security Board Configuration

Security Configuration in System Firmware

The security portion of system firmware has options that can be configured independently of the main Board Configuration. These options are controlled through the security board configuration. In addition, initialization of the secure portion of the system firmware is deferred until the secure board configuration is sent to allow tuning of the system boot time.

Warning

This message MUST be sent in order to initialize the security capabilities of system firmware. Until it is received no security functionality is available.

A standalone board configuration message contains the security data within a flat-typed array. The security data is provided separately to reduce DMSC boot time. The security board cfg message is sent any time after the boot notification message is sent and has no dependence upon receipt of the standard board configuration message.

Note

Security Board configuration requires to be signed and encrypted on HS devices to ensure authenticity and protect secrets. Please refer to Signing Board Configuration on HS devices on how to sign and encrypt board configuration on HS devices.

TISCI API for Security Board Config

The following are the parameters required in the TI-SCI message to pass security board configuration data to DMSC after DMSC sends boot notification complete. The security board configuration message is not dependent on receipt of the standard board configuration message.

Usage

Message Type Normal
Secure Queue Only? Yes

TISCI Message ID

TISCI_MSG_BOARD_CONFIG_SECURITY          (0x000DU)

Message Data Structures

struct tisci_msg_board_config_security_req

TISCI_MSG_BOARD_CONFIG_SECURITY request to provide the location and size of the boardcfg security configuration structure.

Parameter Type Description
hdr struct tisci_header TISCI header
boardcfg_securityp_low u32 Low 32-bits of physical pointer to boardcfg security configuration struct.
boardcfg_securityp_high u32 High 32-bits of physical pointer to boardcfg security configuration struct.
boardcfg_security_size u16 Size of security configuration data.
boardcfg_security_devgrp devgrp_t Device group for the security board configuration.

Note

Even though the security board configuration structure contains the boardcfg_security_devgrp member, it is ignored. Initialization of firewalls is performed for a devgrp when it is enabled via the core board configuration message. This is necessary to ensure isolation. See Board Configuration.

The reamining security services are initialized when the security board configuration is received for the first time. Subsequent security board configuration messages do not have any effect on operation of System Firmware.

struct tisci_msg_board_config_security_resp

Empty response for TISCI_MSG_BOARD_CONFIG_SECURITY.

Parameter Type Description
hdr struct tisci_header TISCI header.

Although this message is essentially empty and contains only a header a full data structure is created for consistency in implementation.

Warning

The boardcfg data structures described below must be placed in MCU OCMC SRAM. The address used in the TISCI message will be in MCU OCMC SRAM.

Configuration substructure enumeration

This is a fixed size c-structure which both defines the format of the configuration as well as reserves DMSC memory to store the configuration. The boardcfg_sec data structure makes use of the same ABI revision structure structure for the top level and boardcfg substructure header for each member structure as the top level boardcfg structure does..

Element Type Description
boardcfg_abi_rev ABI revision structure Board Config ABI version (separate from DMSC ABI version)
processor_acl_list Processor Access List Processor access control list configuration
host_hierarchy Host Hierarchy Host hierarchy configuration
otp_config Extended OTP array configuration Extended OTP access configuration
dkek_config Derived KEK Management DKEK access configuration
reserved_cfg_entry Reserved Entry Reserved configuration entry

Processor Access List

Access Control List for various Processors in the SoC.

boardcfg_proc

Element Type Description
subhdr boardcfg substructure header Magic and size for integrity check
proc_access_list processor_access_list [32] Processor access description

The magic number to be populated in the subhdr is 0xF1EA.

Processor access list entry

Element Type Description
processor_id u8 Processor ID (mandatory) - Use 0 to mark unused
proc_access_master u16 Recovery Host ID or Primary control master host ID (mandatory)
proc_access_secondary[0-2] u16 Other Host IDs that can control this processor(set to DMSC host ID if unused)

Host Hierarchy

Host Hierarchy for various processing entities in the SoC. Host hierarchy defines the supervisory tree for all processing entities in the SoC.

boardcfg_host_hierarchy

Element Type Description
subhdr boardcfg substructure header Magic and size for integrity check
host_hierarchy_entries host_hierarchy_entries [32] Host hierarchy description

The magic number to be populated in the subhdr is 0x8D27.

Host hierarchy entry

Element Type Description
host_id u8 Processing entity Host ID (mandatory) - Use 0 to mark unused
supervisor_host_id u8 Supervisor Host ID

Extended OTP array configuration

The below structure defines which hosts read the OTP area and which host has permissions to write to the OTP area. Please also refer to the below documents to understand the usage of the board configuration structure.

  1. Using Extended OTP on HS devices and
  2. Extended OTP TISCI Description and
Element Type Description
subhdr boardcfg substructure header Magic and size for integrity check
otp_entry otp_entry [32] OTP MMR access control per row
write_host u8 ID of the host who can perform writes to OTP rows

The magic number to be populated in the subhdr is 0x4081.

Note

Wildcard host ID (128U/0x80) cannot be used in the write_host field. The host ID used here must map to a secure proxy thread.

Warning

Even though OTP functionality is not available on GP devices, the boardcfg structure for OTP must be present. The header must be populated with the size and magic number correctly.

Extended OTP Row Entry

Element Type Description
host_id u8

Host ID

  • Set to 128 if the MMR must be accesible to all hosts
  • Set to 0 if the MMR must not be accesible to any host
host_perms u8

2 bit wide fields specifying permissions

  • bit 1:0 - 10b - non-secure, any other value secure
  • bit 7:2 - Reserved for future use.

Derived KEK Management

The below structure controls access to DKEK on the SOC. Please also refer to the below documents to understand the usage of the board configuration structure.

  1. Using Derived KEK on HS devices and
  2. Derived KEK TISCI Description and
Element Type Description
subhdr boardcfg substructure header Magic and size for integrity check
dkek_allowed_hosts u8[4]

Hosts allowed access to DKEK

Set one of the entries to 128 if DKEK must accessible to all hosts.

allow_dkek_export_tisci u8

Flag indicating whether DKEK can be exported via TISCI API

Set to 0x5A if TISCI export is allowed.

rsvd u8[3] Reserved field. Currently unused. Set to 0.

The magic number to be populated in the subhdr is 0x5170.

Reserved Entry

The below entry is reserved for future use.

Element Type Description
subhdr boardcfg substructure header Magic and size for integrity check
rsvd u8[4] Reserved for future use. Set to 0

The magic number to be populated in the subhdr is 0x23BE.