Asymmetric Key Services¶
This document describes the asymmetric key services available in System Firmware.
Introduction¶
Asymmetric key services refer to the foundational operations on which all public key cryptography schemes are built:
- Encrypt a message with a public key
- Decrypt a message with a private key
- Sign (encrypt) a message with a private key
- Verify (decrypt) a signature with a public key
System Firmware provides APIs to perform these operations through a Public Key Accelerator (PKA) module. The remainder of the document describes the details of these operations for RSA and Elliptic Curve algorithms.
For all of the operations, we assume that the required keys are already present in the keystore.
Data Format¶
All key parameters, input, and output vectors use the BIGINT format supported by PKA. The host is responsible for supplying the input data in this format and must extract output data accordingly.
BIGINT data format¶
Asymmetric key operations are performed by a Public Key Accelerator (PKA) hardware module which expects key parameters and input/output data blocks to be in a particular format in order to generalize the operations across all key types and sizes. System Firmware enforces the data format referred to as BIGINT in order to facilitate translation of these parameters to the PKA module.
BIGINT is a series of 32-bit words used to represent a little-endian byte stream and the size of the stream. The first word will contain the size of the byte stream in words, i.e.:
ceil(number_of_bytes_in_stream / 4)
Following the size word will be an array of words holding the LE byte array. An example below shows a 10-byte data block in bytes and again in BIGINT format. Note that the byte array is padded with extra zeros in the MSBs if it is too small to completely fill the last BIGINT array slot.
/* Data block shown as a byte stream */
u8 data_block[] = {0x00, 0x11, 0x22, 0x33, 0x44, 0x55, 0x66, 0x77, 0x88, 0x99};
/* Same data in BIGINT format:
* First word is the size = ceil(10/4) = 3
* Next 3 words contain the byte data (little endian)
* Last word padded with zeros to fill unused data
*/
u32 data_block_bigint[] = {0x3, 0x33221100, 0x77665544, 0x00009988};
In general, for a given byte array, the BIGINT array size will be
/**
* Length of a biginteger array in words, the +1 is for the size
*/
#define BIGINT_LEN(bytelen) (((bytelen + 3) / 4U) + 1U)
With RSA Keys¶
System Firmware provides API’s directly corresponding to the Cryptographic Primitives specified in Section 5 of RFC8017 [1]. This allows user to implement the encryption and signature schemes specified in RFC8017 while maintaining key secrecy using System Firmware.
Note that the cryptographic primitives provide fundamental operations on which higher-level encryption and signature schemes may be implemented. There is no assumption made on format or padding of the data nor on what the contents of the data represent.
RSA Encryption Primitive (RSAEP)¶
To use RSAEP, the user invokes System Firmware API with the following arguments.
- Index in the keystore containing the public key to be used for encryption.
- Memory location containing the plaintext data.
- Memory location to which the encrypted output ciphertext data must be copied.
System Firmware copies the plaintext data into DMSC internal memory, encrypts it with the specified public key, and copies the ciphertext into the specified output location.
RSA Decryption Primitive (RSADP)¶
To use RSADP, the user invokes System Firmware API with the following arguments.
- Index in the keystore containing the private key to be used for decryption.
- Memory location containing the ciphertext data.
- Memory location to which the decrypted plaintext data must be copied.
System Firmware copies the ciphertext into DMSC internal memory, decrypts it with the specified private key, and copies the decrypted plaintext data into the specified output location.
RSA Signature Primitive (RSASP1)¶
To use RSASP1, the user invokes System Firmware API with the following arguments.
- Index in the keystore containing the private key to be used for signing.
- Memory location containing the plaintext data.
- Memory location to which the generated ciphertext data (signature) must be copied.
System Firmware copies the message hash into DMSC internal memory, performs the signing operation with the private key, and copies the signature into the specified output location.
RSA Verification Primitive (RSAVP1)¶
To use RSAVP1, the user invokes System Firmware API with the following arguments.
- Index in the keystore containing the public key to be used for the verify operation.
- Memory location containing the signature.
- Memory location to which the plaintext data must be copied.
System Firmware copies the signature into DMSC internal memory and performs the verify operation using the specified public key. It copies the generated message hash to the specified output location.
With EC Keys¶
System Firmware supports API’s necessary to implement ECDSA sign and verify operations as per [2] below. In both the operations, calculation of the hash of the message is required to be performed before invoking the API. This allows the System Firmware API’s to be independent of the hash algorithm chosen.
Note
According to [3] below, it is recommended to choose a hash with bit length equal to the security strength associated with the bit length of the curve’s group order n. If the length of the hash is greater than the bit length of n then the user must truncate to select only the leftmost n bits (that is, the n MSBs of the BIGINT representation of the hash) or else System Firmware operation will fail. A hash with bit length less than n will effectively reduce the strength of the security of the digital signature to the strength of the hash function, at best.
ECDSA Sign¶
For creating a ECDSA signature of a message, the user
- Calculates the hash of the message with a desired algorithm.
- Invokes the ECDSA sign API with the below arguments.
- the hash of the message,
- the slot number of the private key to be used for signing in the keystore and
- the memory location where the signature of the message must be placed.
- System Firmware copies the hash of the message into DMSC internal memory, calculates the signature of the message using the specified private key and copies the signature to the specified memory location.
ECDSA Verify¶
For verifying a message with ECDSA signature, the user
- Calculates the hash of the message using the algorithm specified by the sender of the message.
- Invokes the System Firmware ECDSA verify API with the below arguments
- the hash of the message,
- the slot number of the senders public key in the keystore and
- the signature of the message.
- System Firmware copies the hash and signature into DMSC internal memory, verifies the signature and hash against the public key. The pass/fail status is returned in the response message.
Return failures¶
For all of the above functions, System Firmware will only return an ACK when successful or a NACK if unsuccessful. Possible reasons for a NACK can be one or more of the following:
- ID of the host requesting access to the key to be used by the primitive operation does not match the Host ID specified for that key slot
- Key slot requested does not hold a valid key
- Type of operation requested does not have the corresponding usage flag set for the specified key slot
- Host is requesting operation on a data in memory which they do not own (UDMA transfer to/from DMSC internal memory will fail)
- Key parameters are not valid and cause PKA operation to fail (System Firmware does not enforce that the user provides valid key parameters otherwise)
- Input data is too large
- For RSA - size of the input data is larger than the modulus
- For ECDSA - length of the hash data is larger than the group order
References¶
- PKCS #1: RSA Cryptography Specifications Version 2.2, https://tools.ietf.org/html/rfc8017
- Standards for Efficient Cryptography Group, “Elliptic Curve Cryptography”, SEC 1, Version 2.0, May 2009 https://www.secg.org/sec1-v2.pdf
- Digital Signature Standard (DSS), FIPS PUB 186-4 https://nvlpubs.nist.gov/nistpubs/FIPS/NIST.FIPS.186-4.pdf